Why is Lighting Important in Interior Design?

Being a homeowner is not just about owning a property or a house that you can call your own. Other than being responsible for the maintenance and development of the property, being a homeowner is also a great opportunity to be creative with your household, especially when it comes to the various functionalities and interior design. If done properly, interior design can significantly raise the market value of your house, and help create a safe, welcoming space for you and your family. Furthermore, interior design is an amazing way of displaying your individuality, tastes, and preferences, and can add a new dimension to the house.

And when it comes to interior design, lighting is one of the most vital aspects you should be attentive to. Not only does lighting help create a comfortable arena that appears spacious, but the right lighting also contributes to adding a sense of depth to the house, and breathe in life to your impressive home.

Hence, if you are a new homeowner or are thinking of sprucing up your home by overhauling the interior design, this article is a quick guide on the importance of lighting in interior design, and how you can choose the best electrical solutions and home automation systems that complement your house to create a space that spells luxury and comfort.

Importance of Lighting Systems in Interior Design

Designing the interiors of a home is undoubtedly a challenging task and requires a lot of management and organisational skills. But as long as you are able to strike the balance with the perfect lighting, your job is half done! Creating the perfect lighting is not just an essential part of interior design, but also helps your house stand out, adding the wow factor that goes perfectly with your decor and preferences. Modern houses often rely on a blend of natural light in artificial design and artificial lighting that creates a mindful and welcoming ambience for all its residents.

When it comes to interior design, lighting cannot be ignored. From the porchlight to the accent lighting on your kitchen island, lighting can be a game-changer for your interiors. Interior lighting has a crucial role to play when it comes to establishing the general ambience of your home, and therefore, must be considered with careful attention. In addition to making sure that your house is well-lit, lighting systems also help complement the architectural and decorative style of the house, influence your moods, and can boost every little detail of your space. With a flexible lighting system, you can help create the perfect balance. An appealing interior lighting system also helps you show off your imagination by setting the perfect ambience and aesthetic.

Read Also: Reasons for Using a Dimmer for Your Home's Lighting

Read on to know about some of the few popular lighting systems that can transform your house.

Types of Lighting Popular in Interior Design

If you are looking to smarten up your home with some interior design lighting, it is beneficial to be aware of the different types that can be used to brighten up all the important areas of your home. So, mentioned below are the most popular types of household lighting that are used by interior designers:

  • Overall Lighting

    As the most commonly used lighting type, overall lighting is a heavy-duty lighting system that is present in almost all households for utility purposes. In interior design, overall lighting systems are the most obvious lighting types that are used as the primary source of light in households and can efficiently light up entire rooms. Since overall lighting is considered the most basic lighting system, it is responsible for illuminating all walls and surfaces. Overall lighting has come a long way in terms of its utility and design over the past decade and is presently available as decorative recessed ceiling lights and feature pendants. Contemporary overall lighting systems are also available as a part of the home automation network where they can be conveniently operated and adjusted by the user remotely.

  • Ambience Lighting

    While overall lighting is tasked with the sole purpose of illuminating every surface and wall of a room, ambient lighting is responsible for creating the atmosphere of the room depending on the situation. as and when needed. So, it is no surprise that after overall lighting, ambient lighting is most sought after by customers when it comes to interior design lighting. In addition to the general illumination of the room, ambient lighting is extremely popular as it helps add a sense of warmth and depth to a room, creating a welcoming atmosphere. Ambient lighting is popularly available as decorative lighting such as overhead feature pendants and chandeliers, which, in addition to creating a welcoming environment, significantly enhances the aesthetic appeal of a room.

  • Task Lighting

    Task lighting, although somewhat less popular, is an equally integral part of the lighting design in interior decoration. While overall lighting and ambience lighting is responsible for illuminating a larger space inside the room, task lighting, on the contrary, is applicable only for lighting up strategic areas within the room for specific purposes. Mostly available as lamps, under cabinet lights, and ceiling pendants, task lighting can be installed in particular areas, such as the study area in the home office, or the prep area of the kitchen for better visibility while working, and so on. Task lighting is also often installed across the household with the sole purpose of illuminating a limited area for conveniences, such as the stairway or the porch area. Comparatively cheaper and available in a wide variety of colour options, task lighting is slowly gaining popularity in contemporary homes. While the task lighting systems are mostly used for added functionality, they are also available as decorative items that can positively contribute to the elegance of your room.

  • Accent Lighting

    Accent lighting in interior design might not serve a purpose as important as that of the overall lighting or the ambience lighting systems, but with the growing popularity of home automation systems, accent lighting has slowly gathered a larger audience. With overall lighting and ambience lighting serving the fundamental lighting design, accent lighting is definitely an exciting bonus for your futuristic home. In addition to accent lighting being capable of effectively lighting up limited areas of the house, it serves its true purpose by adding a defined sense of style to a room. Furthermore, while regular overall lighting systems offer a limited colour palette, accent lighting can be easily personalised to complement the homeowner’s tastes.

    Accent lighting also stands out from other lighting systems because of its effortless installation and maintenance. Accent lighting can be conveniently installed on any surface, such as a cabinet or a shelf. The use of accent lighting is more prominent in modern homes, where it can be used as a part of the general decor, as well as to draw attention to areas of interest. Accent lighting can be easily connected with the home automation module, where it can be conveniently personalised to be easily operated.

Read More: 5 Trending Light Fixtures for Your Home and Office

Lighting Systems Available at the Schneider Electric eShop

The Schneider Electric eShop has long remained one of the most trusted manufacturers and distributors of lighting solutions across the country, with their most popular products being:

  • Lighting and Power Sockets

    Schneider Electric eShop offers a wide range of artificial light in interior design to choose from, especially when it comes to ambience and accent lighting. Schneider Electric eShop’s range of lighting solutions is exceptionally long-lasting with uncompromised performance, making them some of the best options available commercially. In addition to lighting systems and LEDs, you can also choose the best power sockets, light switches, and electrical protection devices from Schneider Electric eShop’s expansive range, which will make your house secure and ready for home automation.

  • Lighting Control

    With a great lighting system must also come great lighting control! And with Schneider Electric eShop’s proprietary Wiser Home Automation system, you can never go wrong when it comes to lighting control. Wiser, the best home automation solution from Schneider Electric eShop offers a one-of-a-kind intuitive control module that can effortlessly connect with all lighting systems and smart devices around the house, offering you complete control over them. In addition to great personalisation options, Wiser Smart Home Automation can be securely connected to your smartphone, allowing you remote access to all connected systems.