Thermal Overload Relays

43 results

arrow-down
MLTIFUNC PH CNTRL 220 480VA PHFAIL ROT
RM35TF30
OVERVOLTAGE CONTROL RELAY RM22-UA - RANG
RM22UA33MR
3 PHASE UNDERVOLTAGE CONTROL RELAY RM22-re
RM22TU23
PH FAILURE ROTATN 208-480VAC 1C/O
RM17TG00
On Delay Timer
RE22R2AMR
ON DELAY TIMER 24 240 VAC
RE17LAMW
TeSys THERMAL OVERLOAD 0.16-0.25A CL10A
LRD02
TESYS K OVERLOAD RELAY CL10 0.36 - 0.54A
LR2K0304
TeSys MAGNETIC CIRCUIT BREAKER
GV2L04
TeSys MOTOR CIRCUIT BREAKER
GV2P01
TeSys MAGNETIC CIRCUIT BREAKER
GV2L06
Thermal overload relay LR9G 225A push-in
LR9G225

Thermal overload relays are essential components in protecting electrical circuits. They protect the components from overheating and damage due to excessive current flow. These relays automatically cut off power when the load exceeds a preset limit. Hence, they safeguard equipment and ensure smooth operations. These relays are designed to provide accurate and reliable protection.

Thermal Overload Relay Working Principle

Thermal overload relays use the heat generated from excessive electrical current to trigger a protective mechanism. There are bi-metallic strips inside the relays. These strips bend when exposed to high temperatures caused by an overcurrent. As the current increases, the temperature rises. This causes the metal strips to bend and eventually break the circuit. It results in cutting off power to the motor or connected device. The relay resets automatically or manually once the circuit is interrupted. However, this depends on the configuration to restore normal operation. This simple yet effective mechanism helps prevent equipment damage and ensures operational efficiency.

1. Thermal Protection

MPCBs utilize a bimetallic strip for thermal protection. When a motor experiences an overload, the current passing through the MPCB increases, causing the bimetallic strip to heat up. As it heats, the strip bends due to the differing expansion rates of the two metals. Once the bending reaches a certain threshold, it triggers the trip mechanism, breaking the circuit and stopping the current flow to prevent motor damage.

2. Magnetic Protection

For short circuit protection, MPCBs employ an electromagnet. When a short circuit occurs, the sudden surge in current creates a strong magnetic field in the electromagnet, which rapidly pulls a lever or plunger that triggers the trip mechanism. This action is almost instantaneous, protecting the motor from the severe damage that high fault currents can cause.

3. Phase Failure Protection

MPCBs can also detect phase imbalances or failures. If one phase drops out or has a significantly lower current than the others, the MPCB will trip to protect the motor from the adverse effects of single-phasing.

Overall, MPCBs provide comprehensive motor protection by combining these mechanisms to ensure safe and reliable motor operation. You can check Schneider MPCB on our eShop. We also have a single-phase MPCB.

What are the main types of overload protection?

Overload protection comes in two primary types. These two types are thermal overload and magnetic overload. Thermal overload protection is ideal for guarding against gradual current increases caused by overload conditions. On the other hand, magnetic overload protection responds to sudden spikes in current like short circuits. Both types of protection work together to ensure the safety and longevity of electrical systems and motors.

FAQs: Common Questions to Ask

Q. Where are thermal overload relays used?

Thermal overload relays are commonly used in motor control circuits. They are particularly used in industrial applications to protect motors from overheating due to overload conditions.

Q. Can a thermal overload relay be reset?

Yes, thermal overload relays can typically be reset manually once the overload condition is resolved. Some models may also reset automatically after cooling down.

Q. What is the difference between a thermal overload relay and a fuse?

A fuse offers one-time protection by breaking the circuit during excessive current flow. On the other hand, a thermal overload relay can reset and be reused. It offers continuous protection against overload conditions.

Q. How do I select the right thermal overload relay for my motor?

Consider factors such as motor rating, current requirements, and the specific operating conditions of the application to select the right thermal overload relay. It’s crucial to match the relay to the motor’s characteristics to ensure proper protection.

Q. How do I test a thermal overload relay?

You can test a thermal overload relay by applying a controlled overload to the motor. You must also check if the relay trips as expected. Regular maintenance and testing are essential for ensuring optimal relay performance.



Similar Category

Automation Relay Control Relay Harmony Electromechanical Relays Residual Current Relays Variable Speed Drives PFC Controller