Electrical Reactors

12 Items

arrow-down
EasyLogic PFC  DR CU 25kVAr 440V 7%50Hz
LVR07250A44CU
EasyLogic PFC  DR CU 10kVAr 440V 7%50Hz
LVR07100A44CU
VarPlus MAX 20 kVAr 440V 7% 50Hz
LVR07200A44LO
VarPlus MAX 5 kVAr 440V 7% 50Hz
LVR07050A44LO
VarPlus MAX 10 kVAr 440V 7% 50Hz
LVR07100A44LO
VarPlus MAX 50 kVAr 440V 14 % 50Hz
LVR14500A44LO
DetunedReactor CU 50kVAr 440V 7%50Hz
LVR07500A44CU
VarPlus MAX 25 kVAr 440V 7% 50Hz
LVR07250A44LO
VarPlus MAX 50 kVAr 440V 7% 50Hz
LVR07500A44LO
VarPlus MAX 100 kVAr 440V 7% 50Hz
LVR07X00A44LO
VarPlus MAX 75 kVAr 440V 7% 50Hz
LVR07750A44LO
VarPlus MAX 15 kVAr 440V 7% 50Hz
LVR07150A44LO

An electrical reactor is a key part of every power system. It limits sudden current changes and helps keep voltage stable during irregular loads or short circuits. The electrical reactor's working depends on magnetic induction, where the current passes through coils, reducing electrical stress in the system. Many industries and substations use it for stable operations and safety. The electrical reactor function is also to reduce harmonics and improve the overall performance of electrical equipment.


Buy Electrical Reactors 

Electrical reactors are essential components in various electrical systems, primarily used to manage and limit the flow of current. Whether you're dealing with power factor reactors for compensating reactive power or detuned reactors Schneider for harmonic filtering, these devices play a vital role in stabilizing electrical networks. When integrated into an APFC panel with a reactor, they ensure optimal performance by improving power quality and minimizing losses. Investing in high-quality electrical reactors enhances the safety and efficiency of your power systems, making them a crucial part of industrial applications.


Working Principle of Power Factor Reactors 

Power factor reactors are designed to regulate and enhance power quality in electrical networks. They operate by compensating for reactive power, which improves the overall efficiency of the system. Installed in conjunction with APFC panels with reactors, these devices help maintain a stable voltage by controlling excessive currents and harmonics. By including a detuned reactor Schneider in the setup, harmonic distortions are minimized, ensuring smoother operation of the electrical grid. The working principle revolves around managing current flow, reducing losses, and enhancing the system's lifespan.


Types of Electrical or Line Reactors 

A reactor in an electrical system is used in several applications, each serving different electrical demands. Depending on design and use, line reactors are divided into a few core types. These types protect equipment, manage harmonics, and help maintain power factor efficiently. Understanding what a reactor is in electrical helps to reduce failures and extend system life.


1. Shunt Reactor 

Used in transmission networks to balance voltage during light load conditions. This type of electric reactor absorbs reactive power, ensuring the voltage stays within safe levels. It is often used in an electrical substation for system stability.


2. Series Reactor 

The series type of electrical reactor limits the short circuit current in circuits. It helps maintain constant current flow and provides protection to cables and transformers from high faults in a network.


3. Line Reactor 

This electronic reactor is installed between the inverter and motor to reduce harmonics and surge voltage. It controls current spikes and improves the overall operation of drives and connected motors.


4. Power Factor Reactor 

The power factor reactor is used with capacitor banks to correct the power factor and restrict harmonic distortion. It ensures balanced load and protects electrical components from resonance effects.


5. Tuning Reactor 

A tuning type of reactor in an electrical substation is paired with filters to control unwanted frequency components. It maintains a clean power supply and enhances system efficiency under varying loads.


Frequently Asked Questions 


Q1. What does a reactor do in electronics? 

Ans. In electronics, a reactor is used to limit or control current flow, particularly in AC circuits. Electrical reactors help manage power factor, filter harmonics, and stabilize voltage in complex systems. 


Q2. Why do we use reactors in the power system? 

Ans. Reactors are used in power systems to improve power quality by managing reactive power and reducing harmonic distortions. They play a key role in maintaining stable voltage levels and protecting equipment from damage.


Q3. What is the difference between a reactor and a transformer? 

Ans. While both reactors and transformers are used in electrical systems, a reactor limits current flow and filters harmonics, while a transformer is designed to change voltage levels. Electrical reactors are primarily used for stabilizing power quality, whereas transformers are used for voltage regulation.


Q4. What is a reactor in electrical engineering? 

Ans. A reactor in an electrical setup is a coil-based device that manages the flow of current in circuits. It protects other components from sudden voltage jumps or faults during switching. The device captures energy in its magnetic field and releases it gradually to maintain balance. It is mostly used across power systems to keep operations steady and to lower the level of short-circuit currents in the network.


Q5. How do electrical reactors work? 

Ans. An electrical reactor limits sudden current changes and balances voltage across circuits. When electricity passes through its coils, a magnetic field forms and slows violent current surges. This protects connected machines during overloads and power changes. The whole process helps keep the electrical network stable, avoids damage, and ensures that every part continues to operate smoothly without heavy shocks or sudden drops.


Q6. What is the difference between 3% and 5% reactor? 

Ans. The contrast between 3% and 5% reactors in the electrical system is about impedance strength. A 5% reactor holds higher impedance and gives deeper current control than a 3%. On the other hand, 3% gives less voltage drop. The figure shows how much voltage is held to limit the current. The choice depends on what level of power quality and safety is most suitable for the setup being used.


Q7. What is the difference between a nuclear battery and a reactor? 

Ans. A nuclear battery changes radiation energy straight into electricity, while a reactor in an electrical substation builds energy through fission that turns water into steam for turbine use. The nuclear battery is compact, often used in remote or small-scale operations, whereas a reactor generates large energy for public grids. Both work on nuclear effects but serve very different power goals and system functions.


Q8. What is the difference between a transformer and a reactor? 

Ans. A transformer changes voltage from one level to another, but an electronic reactor blocks high current with inductance. Transformers move power efficiently with a small loss, while reactors hold back dynamic current that may damage systems. A reactor has open magnetic fields and higher inductance compared to a closed-core transformer. Both are often used together to ensure reliable and balanced power distribution.



Best-Selling Schneider Electric India - Others - Electrical Reactors Price List (2026-2027)

Updated Date: 22 November, 2026

Top Popular Best-Selling Schneider Electric India - Others - Electrical Reactors Price List (2026-2027) Latest Price
VarPlus MAX 15 kVAr 440V 7% 50Hz ₹ 27,558.00
VarPlus MAX 75 kVAr 440V 7% 50Hz ₹ 70,481.00
VarPlus MAX 100 kVAr 440V 7% 50Hz ₹ 91,293.00
VarPlus MAX 50 kVAr 440V 7% 50Hz ₹ 45,189.00
VarPlus MAX 25 kVAr 440V 7% 50Hz ₹ 29,262.00
DetunedReactor CU 50kVAr 440V 7%50Hz ₹ 78,980.00
VarPlus MAX 50 kVAr 440V 14 % 50Hz ₹ 74,637.00
VarPlus MAX 10 kVAr 440V 7% 50Hz ₹ 22,728.00
VarPlus MAX 5 kVAr 440V 7% 50Hz ₹ 15,727.00
VarPlus MAX 20 kVAr 440V 7% 50Hz ₹ 29,252.00