Blog
What is a Timer Relay? Working Principle, Functions and Types
Certain machines have to wait before carrying out an action. It is not advisable for a compressor to restart immediately after it has stopped. A fan should continue to run after a heater has switched ...
What is a Lighting Control System? Types, Smart Lighting and Benefits
A practical home lighting control plan starts with the rooms, routines and lighting needs of the household. Go into a house at night and see how many lights are still on. In most homes there are at le...
Difference Between Inverter and UPS: Which One Do You Need?
A power failure will eventually affect all households, causing the lights to go out, the fans to slow down and the Wi-Fi router to lose connection. Two devices offer a solution and appear very similar...
Difference Between Latch and Flip-Flop: Working, Types and Comparison
Digital systems need to store information; for example, a counter has to keep its count, a processor must retain an address, and a controller has to maintain its state between steps.
What is Watt’s Law? Formula, Calculation, Examples and Applications
Whenever you check the label on any kettle, fan or charger you will notice a number followed by the letter W. That number shows how rapidly the device consumes electrical energy.
What is a Clamper Circuit? Working, Types, Uses and Advantages
Signals frequently reach the wrong DC level. For example, a sine wave might vary between -5 V and +5 V, even though the following stage requires a voltage range from 0 V to +10 V.
What is an Encoder and Decoder? Working, Differences and Applications?
Keypads, switches and sensors generate a large number of individual signals. The processor selects a short code; there must be something in between the two, and this is the role of the encoder.
What is a Varactor Diode? Working, Characteristics and Applications
Previously, adjusting a radio involved turning a knob that was connected to a large air-gap capacitor. Now, the same thing is achieved using a small semiconductor chip and a control voltage.
What is Hydroelectric Power? Working, Types, Uses and Benefits
For over two thousand years people have used water to carry out work. For instance, early mills made use of a wheel and a stream to grind grain. Nowadays the same principle is used to light entire cit...