Blog
Understand the Difference between Servo Motor and Stepper Motor
In many electrical systems, movement is not about spinning fast. It is about stopping exactly where needed. Whether it is a robotic arm, a medical device, or a small automation setup, controlled motio...
What Are HRC Fuses? Types, Uses & Working Principle
Electrical systems do not fail politely. When something goes wrong, it often happens fast and with force. In larger installations, that force can be destructive. This is where devices like the HRC fus...
What is Stepper Motor? Working Principle, Types & Applications
Motors are everywhere, but not all motors are meant to behave the same way. Some are built to run nonstop. Others are built to stop exactly where they should. A stepper motor belongs to the second gro...
Why Modular Switchboards are the Future of Modern Indian Homes?
There was a time when electrical switchboards were an afterthought. They were installed once, usually in whatever style was available, and rarely questioned again. As long as the light turned on, the ...
Understand the Difference Between Relay & Contactor: Full Explanation
People who deal with electrical systems, even casually, often hear terms like relay and contactor, and at first, everything feels similar. They both click, both switch circuits, both sit inside panels...
What Is an Isolator Switch? Types, Uses & Benefits Explained
In any electrical system, whether it’s a home setup, a small workshop, or a huge substation, there is always one thing that quietly ensures safety before anyone touches a wire: the isolator switch. ...
Understand the Difference Between Fuse and Circuit Breaker
It’s surprising how most people never even think about electrical protection until the moment something stops working, like a room suddenly going dark, a device refusing to turn on, or maybe a buzzi...
What Is a Relay? Working, Types & Applications
It’s interesting how relays show up everywhere, yet most people never think twice about them. Someone might have used a washing machine, switched on a car headlight, or seen a building’s lights tu...
Oil Circuit Breaker: Construction, Working, Types & Applications
Electrical systems rely on many forms of protection, and one device that has served power networks for generations is the oil circuit breaker. Even though new technologies like vacuum and SF6 breakers...