Wires & Cables
What Is the Difference Between Wire and Cable?
When it comes to electrical work, you’ve probably heard people talk about wires and cables. Sometimes, it feels like they’re using both words to mean the same thing. It’s common.
Types of Electrical Wires and How to Choose the Best One for Your Home!
When it comes to electrical wiring, one should be very attentive while choosing the type of wire as it is a matter of safety, reliability and efficiency of future power supply. Electrical wires are th...
Types of Wireless Technologies in Industrial Automation
The application of automatic control has been an important factor in transforming modern manufacturing and industrial processes.
Stranded vs. Solid Wire: Optimal Choice and Reasons
Wires are vital channels in electrical systems, allowing electric current to flow effortlessly. Stranded and solid wires are two distinct kinds and the choice between them is crucial for guaranteeing ...
What do the different colours mean on electrical wires?
Improper handling of electric wires can cause serious accidents. They can be a threat not only for laymen but for trained electricians as well.
How to Find the Suitable Size of Cable & Wire for Electrical Wiring Installation?
In the realm of electrical installations, one crucial element often dictates the success of an entire project: the selection of the right cable and wire size. Whether you are working on residential wi...
Electrical Cable Size Calculator & Cable Size Chart Amps
Electrical cables are the lifelines of any electrical system, transmitting power from one point to another. Keeping in mind the very crucial job they conduct, choosing the right cable size in electric...
Type of Electric Cables & Conductors with Application
In layman's terms, cables and wires are sometimes used interchangeably and might mean the same thing, but technically the two are not the same. While a wire comprises a single electrical conductor, a ...