Types of Wireless Technologies in Industrial Automation
The application of automatic control has been an important factor in transforming modern manufacturing and industrial processes. Following the introduction of control systems, all the production routes have been advanced in terms of safety, efficiency, and productivity. Wireless technologies have gradually become solutions in industry automation because of their several benefits over traditional wired-based networks. The article aims to conduct a detailed analysis of different wireless technologies for industrial automation, their advantages, problems, and compatibility with various applications.
Industrial Wireless Networks: Revolutionising Industrial Automation
Industrial automation has opened up an exciting wireless sensor networks (WSNs) research area. The main advantages of these networks include their usage in places where traditional wiring could be less viable and cost-prohibitive. Let’s focus on the practical yields of WSNs in industrial processes nowadays.
Increase in Accessibility and Flexibility
One of the significant advantages of WSNs is that they will remove the necessity of the long wiring that is the enabling factor for their service provision in remote areas or even locations which cannot be accessed easily. This is not only the step towards lowering the installation costs but also provides the ability to monitor the applications where wiring is not feasible. Additionally, in the cases of temporary installations and areas with unreliable power sources, WSNs fulfil this function.
Optimising Plant Asset Management
Wireless networks are the critical technology used for modernising industrial facilities that are already in use. By releasing cable resources usually reserved for lower-priority measurements, intelligent sensor networks can manage plant assets more efficiently. Traditional instruments, including pressure gauges and temperature dials, can be substituted with wireless sensors, which confirm better accuracy and reliability. Besides, WSNs enable the measurements on equipment that is rotating or on the go and the ones at remote locations, thereby increasing locations for sensing.
Scalability and Cost-Effectiveness
The scalability of WSNs is another significant advantage of these networks. New modules can be added to the existing networks anywhere at low cost, and constant expansion and adaptation to the new necessities can also be achieved. Further, temporary measurements also serve a purpose for process diagnostics and optimisation, permitting the full utilisation of WSN options.
Read More - UNDERSTANDING THE BASICS OF HOME AUTOMATION AND ENERGY EFFICIENCY
Wireless Sensor Networks: Challenges and Standards
The quest for global acceptance of WSNs in industrial automation has met many challenges. One of the major concerns is the need for a single universal standard in the wireless communication network. The fact that multiple protocols can be working within the same bandwidth and not be compatible with each other can lead to reliability, latency issues, and potential security vulnerabilities. Implementing a universal benchmark that promotes security, interoperability, and cost-effectiveness is extremely difficult for the industry.
Read Also - WHAT IS A SENSOR, HOW DOES IT WORK, AND WHAT ARE THE VARIOUS TYPES OF SENSORS?
Different Types of Wireless Communication
The different types of wireless communication used in industries are as follows:
1. Wi-Fi
Wi-Fi communication, adopting the standard of IEEE 802.11, has become popular in industrial automation because of its fast data transfer rates, reliability, and flexibility to interact with existing network infrastructures. The Wi-Fi networks specify wireless connection within a limited area. They usually cover areas of a factory floor or warehouse. Wi-Fi in the industrial sector includes wireless control of machines, inventory tracking, quality control, and worker mobility. IoT devices like tablets and smartphones use Wi-Fi to exchange data with the control systems, servers, and cloud storage in real-time so workers can quickly make quick decisions and fail the process.
2. Bluetooth
Bluetooth technology has transformed more than its original consumer-centric applications to provide utility in industrial automation environments. Bluetooth offers lower power consumption for short-range wireless connections, suitable for connecting devices nearby. The BLE variants take the effectiveness further regarding power efficiency and are the favourite choice for industrial battery sensors and actuators. Industrial usage of Bluetooth is maintained by asset tracking, equipment monitoring, and personnel safety. Devices equipped with Bluetooth-like gadgets can communicate among themselves and with direct control systems without any hiccups.
3. Zigbee
This networking protocol is the low-power wireless technology used in the automation and IoT domains. Zigbee operates on the IEEE 802.15.4 standard and possesses low data rates but short to medium distances. Zigbee's mesh networking abilities are capable of uninterrupted and secure communication in industrial environments that may contain barriers and interference. Industrial uses of Zigbee include electronic control of industrial lighting, building automation, and intelligent metering. Zigbee's autonomously connecting mesh networks assure continuous operation and fault tolerance, resulting in more reliable automation ecosystems.
4. 6LoWPAN
The technology of 6LoWPAN is based on the IEEE 802.15.4 standard, a low-power personal area wireless network. IPv6 technology, which is more advanced and offers a higher bit data capacity than IPv4, is utilised, making an IOT network of vast devices available. The technology is best suited for the small, low-power devices typically encountered in industrial automation systems because of its low-power characteristics. It is suitable for sensor networks that need to function for extended periods on limited power supplies. Despite having lower speeds than other wireless networks, 6LoWPAN stands out in low-power device connection, the leading technology in energy-efficient industry applications.
5. Wireless HART
Wireless HART complies with IEEE 802.15.4 standards and falls under the approved HART protocol in industrial automation. HART allows analogue and digital signals to be transmitted simultaneously via the same cable on the same frequency. HART wireless utilises mesh topology, meaning broadcasts are not sent to a router; instead, multiple nodes in an operational area communicate with each other. This architecture improves the network resilience and reliability by allowing data to be directly transmitted between the devices. Wireless HART is one of the most robust and widely adopted wireless communication technologies in industrial settings. It is easy to achieve seamless integration with existing HART infrastructure.
Conclusion
Wireless technologies are significantly triggering a revolution in automated manufacturing, which facilitates the creation of intelligent industrial networks. Industries can utilise these technologies to discover new frontiers of innovation, performance and sustainability. With the latest developments in wireless technologies, their integration into industrial automation ecosystems will contribute to the digital transformation pace acceleration and reshape the manufacturing and production of the future.
Explore Schneider eShop’s wide range of wireless transmitters and sensors and the batteryless Harmony XB5R buttons, which have a long service life for industrial automation applications. By giving customers a choice of colours and markings, these transmitters are very flexible and easy to use. Boost your automation setup purchase by adding these transmitters. Discover Schneider eShop today and find these products, among others, to add wireless technologies to your industrial automation projects.
Comments