Smart Keypads: A Must for Home Automation

Over the past decade, there have been unprecedented levels of change when it comes to information technology and its use in our everyday lives. This has also allowed companies to look for creative solutions that allow homeowners to take the next step towards energy conservation and enjoy the amazing conveniences and comforts that technology can provide. One of the many perks of technology is home automation and smart homes. Keeping up with the pace towards using smart technology, Schneider Electric eShop has emerged as one of the most reputed distributors of home automation systems across the country.

Type of home automation systems available at the Schneider Electric eShop

With the wide-scale popularity of home automation, Schneider Electric eShop has yet again established itself as one of the premiering choices for industrial, as well as domestic electrical solutions. With its proprietary Wiser Home Automation, here is how Schneider Electric eShop is ushering in the era of futuristic smart homes in India:

  • Wiser Home Automation

    Wiser as Schneider Electric eShop’s flagship home automation solution has been extremely popular among homeowners since it was launched. As a home automation system that can be directly installed and integrated with all compatible devices around the household, Schneider Electric eShop’s Wiser Home Automation system can be used to effectively keep track of all connected devices and control them even when you are away from home.

    Furthermore, Wiser Home Automation also contributes to a cleaner, more sustainable future as it can help you to monitor all kinds of energy consumption around the household and send automatic alerts to streamline your energy usage. Additionally, the Wiser Home Automation can be easily accessed using a smartphone as well as Google-assistant devices.

  • Wiser Energy Home Power Monitor

    The Wiser Energy Home Power Monitor from Schneider Electric eShop can effectively read the energy usage for all connected devices and use machine learning to process the data collected and suggest energy-saving alternatives. Its intuitive programming can also learn about the user’s preferences and automate energy consumption accordingly. The Wiser Home automation system can also be connected to the Wiser Energy Home Power Monitor, allowing you to set custom alerts for your connected household devices. Users can also opt for automated responses such as operating the lighting and switching off the dryer when done.

  • Wiser Energy Current Sensors

    Schneider Electric eShop’s Wiser Energy Current Sensors have also grabbed the attention of homeowners, as they offer excellent preventive measures against electrical accidents, such as electrical surges and short circuits. Other than real-time monitoring of energy consumption around the house, the Wiser Energy Current Sensors can be connected to electrical protection devices such as circuit breakers switches and fuses.

Furthermore, Schneider Electric eShop is also one of the most reputed distributors of home appliances such as household and electrical security devices, smart appliances, and lighting that can be seamlessly connected with the Wiser Home Automation network and turn your household into the smart home of the future.

What is a Smart Home Keypad?

With home automation made widely accessible across the globe, more homeowners are opting for smart home automation devices that can be effortlessly integrated with their home automation systems, adding to their comfort and convenience. One of the common smart home devices that have made home automation significantly more accessible is the smart home keypad, which is currently the top choice for customers of smart home appliances around the world.

Read Also: Things You Need to Know About Smart Home Automation Systems

Simply put, a smart keypad serves as a module connecting all smart appliances around the household and provides the user with complete control over all connected devices. Currently, smart home keypads are available as small units that are easy to install and maintain and are extremely convenient to use. Equipped with a touch-sensitive interface, the smart home keypads not only look futuristic and elegant, but they are also easily compatible with old and new technology alike. In addition to the standard functions that allow users to operate all lighting within the household, these smart keypads let users control appliances in groups and personalize all settings based on individual tastes and preferences. The minimalist and intuitive nature of smart home keypads sets them apart from conventional switches and can help you to get your house ready for futuristic home automation.

Why should you use Schneider Electric eShop’s smart home keypad?

Given its immense popularity, Schneider Electric eShop’s smart home keypads have remained relevant over the past years. In addition to the functionality and convenience it brings to a household, Schneider Electric eShop’s smart home keypad is also highly coveted among customers for several other reasons. Mentioned below are some of the exclusive advantages of home automation that make the sleek, ergonomic smart home keypads from Schneider Electric eShop a must-have:

  1. Superior user experience

    A smooth and convenient user experience is perhaps the leading motive behind the development and wide-scale use of home automation. And if a superior user experience is what you are looking for, Schneider Electric eShop’s smart home keypad will not disappoint you. Schneider Electric has designed this popular brand of smart home keypads to emphasise simplicity and comfort, with keypad buttons and interfaces that allow intuitive navigation and can even carry out complex functions like altering the audio volume, shifting the window shades, and changing the ambience lighting to accommodate any atmosphere. From easy, intuitive on/off commands, the smart home keypad from Schneider Electric eShop offers access to personalised lighting and audio, as well as home climate settings, making it one of the reasons why we need home automation.

  2. Smartphone support

    One of the primary reasons that make home automation worth its price is the easy, seamless connectivity with smartphones. Being able to supervise and control your household appliances directly from your smartphone is an incredibly attractive and convenient feature, to begin with, and it also significantly reduces any breach of personal safety, even when you are away from home. Presently, all home automation keypads from Schneider Electric eShop can be connected to your smartphone network, maintaining a secure connection between all compatible appliances.

    With the proprietary Schneider Electric eShop’s smartphone app, you can connect, supervise and operate all smart home keypads, offering you complete access to lighting and automation, and extensive control options. The secure smartphone connectivity has made the smart home keypad systems from Schneider Electric eShop exceptionally ergonomic, easy to implement, and regulate around the household. With the latest updates, the smart home keypads from Schneider Electric eShop have been turned future-ready with additional functionalities such as voice command, and more.

  3. Wireless keypad options

    Who likes tangled messes? With the latest smart home keypad models, you can bid farewell to wires for good. Designed with the finest technology, the wireless smart keypad options for home automation have grown immensely popular, especially for the convenience they bring to projects like home remodelling and renovation. Easy to install and maintain, these untethered smart keypads from Schneider Electric eShop are known to substantially reduce energy consumption and improve connectivity. These amazing smart home keypads come with secure wireless connectivity, which is easy to install and highly adaptable.

  4. Touchscreen compatibility

    With almost all smart devices being adapted for touchscreen functionality, the smart home keypads from Schneider Electric eShop have also been designed for complete touchscreen compatibility. Forget the days of old junky switches, the latest smart keypads for home automation offer a completely digital interface that can be efficiently operated with gestures.

    The latest smart keypads from Schneider Electric eShop can easily read gentle taps, swipes, and flicks, and allows you to comfortably adjust the lighting and temperature around the household as well as control all connected devices. The multi-screen layer and intuitive UI also contribute to a smooth experience.

  5. Elegant design and theme

    If you have a keen sense of interior decor and accessories, Schneider Electric eShop’s smart keypads for home automation will definitely catch your eye! In addition to offering amazing functionality and comfort, these smart keypads feature a sleek, minimalistic design, that goes well irrespective of the user’s tastes and preferences.

    Intuitive and easy-to-use, the user interface on the smart home automation keypads from Schneider Electric eShop comes with programming options that allow you to customise your smart keypad, create automated lighting presets, and more. In addition to a sophisticated, chiselled look these keypads are highly resistant to physical damage and easy to maintain.

Read Also: Know About the Basics of Home Automation System and Its Use in Modern Homes