On Delay Timer vs Off Delay Timer: Key Differences, Working Principle & Selection Guide

On Delay Timer vs Off Delay Timer: Key Differences, Working Principle & Selection Guide

Summary

Timers control when things switch on or off. But which type fits the job? The difference between on delay timer and off delay timer comes down to timing. One delays the start. The other delays the stop. This guide covers what is an on delay timer, what is an off delay timer, basic wiring for both, and how to pick the right one for a panel using a Control Relay. Simple idea, once it clicks.

Key Takeaways

• An on delay timer waits before turning an output on.

• An off delay timer waits before turning an output off.

• Wiring differs slightly, though both use similar contact types.

• Pick based on whether the delay is needed at startup or shutdown.

• Both work closely with a standard Control Relay in most panels.

Introduction

Timing matters more than most people think. A motor that starts too soon can get damaged. A fan that stops too early can leave a machine overheating. That's where delay timers step in. Two types dominate this space. Mixing them up causes real wiring headaches. This guide covers on delay timer vs off delay timer clearly. It looks at how each works, where the wiring differs, and which suits which job. No jargon overload. Just the basics that matter.

What is an On Delay Timer

An on delay timer, sometimes called a delay-on timer, waits before turning its output on. Flip the input signal on, and nothing happens right away. A countdown starts instead. Once that countdown ends, the output finally switches on.

So what is an on delay timer used for? Picture a conveyor system that needs a short pause before the next stage kicks in. Or a compressor that shouldn't restart the second power comes back after a trip. The timer builds in a gap between one event and the next. That gap protects equipment and keeps a process running in the right order. Technicians can usually set the exact delay a job needs, whether that's two seconds or two minutes.

How Does an On Delay Timer Work

The idea is simple once broken down. Energising the coil starts a countdown, not an instant switch. That one detail defines the whole device.

The Basic Timing Sequence

Power reaches the coil, and the timer starts counting. The output contact stays put during this countdown. Only once the set delay runs out does the contact change state. Cut power mid count, and everything resets back to zero.

Understanding On Delay Timer Working Principle

The on delay timer working principle comes down to one simple rule. Input first, delay second, output last. Nothing skips ahead. That order is what makes the timer predictable. Predictability is exactly what engineers need when coordinating several stages in a row.

On Delay Timer Wiring Diagram Basics

A typical on delay timer wiring diagram shows the coil wired to the control voltage supply. Normally open and normally closed contacts connect to whatever needs the delayed start. Getting the contact type right matters a lot. A normally open, timed closed contact acts nothing like a normally closed, timed open one.

Common Contact Configurations

On delay timers usually offer NOTC and NCTO contact types. NOTC stays open until the delay ends, then closes. NCTO does the opposite. It stays closed until the delay ends, then opens. The right choice depends on whether the connected device needs to switch on or off once the delay finishes.

What is an Off Delay Timer

An off delay timer works the other way round. The output turns on right away with the input signal. No waiting there. The delay only kicks in once that input signal drops.

So what is an off delay timer good for? Picture a cooling fan on a motor. The fan needs to run the moment the motor starts. But it also needs to keep running a bit after the motor shuts off, to clear residual heat. An off delay timer handles that exact job. The output stays on for a set time after the input drops. That gives equipment time to wind down safely instead of stopping instantly.

How Does an Off Delay Timer Work

This timer flips the order around. Output responds right away to input. Removing that input starts a countdown before anything actually switches off.

The Basic Timing Sequence

The moment input power arrives, the output turns on with no delay at all. It stays on as long as input remains present. Once input power drops, a countdown starts. The output stays active through that countdown, only switching off once time runs out.

Contrasting With On Delay Behaviour

An on delay timer makes something wait to start. An off delay timer makes something wait to stop. Both use the same basic timing parts, just triggered at opposite ends of the cycle. Spotting this difference quickly helps when reading a wiring plan under pressure on site.

Off Delay Timer Wiring Diagram Basics

An off delay timer wiring diagram looks much like its on delay cousin, though contact behaviour differs. The coil still connects to control voltage. Contacts still switch a load. But the timing happens on shutdown, not startup, which changes how the circuit gets planned.

Common Contact Configurations

Off delay timers usually use NOTO and NCTC setups. NOTO closes instantly when energised, then opens after a delay once de-energised. NCTC does the reverse. It opens instantly, then closes again only after the delay ends. Matching the right contact type to the load matters for reliable results.

Difference Between On Delay Timer and Off Delay Timer

At a glance, these two timers look almost identical. Same housing. Same terminals. Similar wiring layout. The real difference between on delay timer and off delay timer sits entirely in when the countdown happens.

Timing Direction

An on delay timer counts after the input turns on. An off delay timer counts after the input turns off. That one difference shapes everything about how each device behaves once wired into a working circuit.

Output Behaviour at Startup

On delay timers keep the output off right when power first arrives. It only turns on once the delay ends. Off delay timers do the opposite. Output turns on the instant power shows up, no waiting involved at all.

Output Behaviour at Shutdown

On delay timers switch output off right away once input power disappears. No lingering delay there. Off delay timers hold output active for a set time after input drops. That is the entire reason they exist in cooling and ventilation jobs.

Typical Use Case Framing

On delay timer vs off delay timer selection often comes down to one question. Does the delay need to happen before something starts, or after it stops? Answer that, and the right timer type becomes obvious pretty fast.

Feature On Delay Timer Off Delay Timer
Delay Occurs After input turns on After input turns off
Output at Startup Delayed Immediate
Output at Shutdown Immediate Delayed
Common Contacts NOTC, NCTO NOTO, NCTC
Typical Use Sequencing, startup protection Cooldown, ventilation delay

Applications of On Delay Timer

These timers show up wherever a startup needs protecting or staging. Industrial panels, motor controls, and automation systems all use them to coordinate what happens first.

Motor Restart Protection

After a power trip, restarting a motor right away can cause damage or trip protection again. An on delay timer holds the restart back for a set time, letting voltage settle first. This small pause protects costly equipment from repeated stress during unstable power on a factory floor.

Conveyor Sequencing

Multi-stage conveyors often need each section to start slightly after the last one. On delay timers create that staggered start, stopping product pileup or strain from every section starting at once. This keeps material flow smooth across the whole line, no sudden jolts.

Compressor Cycling Control

Compressors often need a pause before restarting to avoid pressure stress on internal parts. An on delay timer builds in that pause automatically, protecting the unit from short cycling. This stretches equipment life quite a bit in HVAC and refrigeration systems running long duty cycles.

Alarm and Indicator Delays

Sometimes an alarm shouldn't fire the second a fault appears, since brief blips happen normally. An on delay timer filters these out. It only triggers the alarm if the fault sticks around past the set delay. That cuts down false alarms in sensitive monitoring setups.

Applications of Off Delay Timer

Off delay timers solve a different problem. They keep something running briefly after the trigger disappears. Cooling, safety, and ventilation systems lean on this heavily.

Cooling Fan Control

Motors and electronic enclosures often need airflow after shutdown to clear heat. An off delay timer keeps the fan running for a set time after the main system powers down. This stops heat damage that could shorten component life over repeated cycles.

Security Lighting Delays

Motion lighting benefits from an off delay timer, keeping lights on briefly after motion stops. This avoids the annoying flicker of lights cutting off the instant someone pauses. It still saves energy compared to lights left running all night.

Ventilation Systems

Bathroom or industrial extractor fans often need to keep clearing air after the trigger switch turns off. An off delay timer extends fan run time for a set period. That way odours or fumes clear properly instead of lingering because the fan stopped too soon.

Safety Interlocks

Some machine guarding systems need a short delay before fully releasing safety measures after a stop command. Off delay timers help manage that transition. They give moving parts time to fully stop before related safety circuits change state, cutting risk during shutdown.

Conclusion

Choosing between an on delay timer and an off delay timer comes down to one question. Does the delay belong at the start or the end of the cycle? Once that's clear, wiring and contact choice tend to fall into place. Anyone building or upgrading a control panel, whether pairing a timer with a Control Relay or sourcing new parts, can find a reliable range through the Schneider Electric eShop.

FAQs

Q1. Can one timer be switched between on delay and off delay functions?

Some multifunction timers allow this. Basic mechanical timers are usually fixed to one function and can't be changed on site.

Q2. How precise are typical delay timer settings?

Most timers stay accurate to within a fraction of a second, though this varies with build quality and price.

Q3. Do delay timers need a separate power supply from the load they control?

Often yes. In industrial panels, the timer coil usually runs on control voltage, separate from the higher power load circuit.

Q4. What happens if a delay timer fails while in service?

Failure varies, but many timers fail in a way that leaves the contact stuck open or closed. Regular testing helps catch this early.

Q5. Are delay timers compatible with PLC based control systems?

Yes. Many industrial delay timers work easily with PLC logic, either as standalone hardware or built into the PLC's own timing functions.

Older posts Newer posts