Electric Switches

267 results

arrow-down
ZENcelo India - 16AX/20A 2 Way Full Flat Switch - Dark Grey
IN8402/16(BZ)
IN8402/16
IN8402/16
ZENcelo India - 6A 2 Way Full Flat Switch - Dark Grey
IN8402(BZ)
ZENcelo India - 6A 2 Way Full Flat Switch -White
IN8402
ZENcelo India - 16AX/20A 1 Way Full Flat Switch with Indicator - Dark Grey
IN8401/16(BZ)
ZENcelo India - 16AX/20A 1 Way Full Flat Switch with Indicator - White
IN8401/16
6AX 1 Way Full-Flat Switch Module with On indicator - bronze
IN8401(BZ)
ZENcelo India - 6A 1 Way Full Flat Switch with Indicator-White
IN8401
Opale - 6A 1 Way Switch
X1001WH
Opale - 6A 2 Way Switch
X1002WH
Opale - 16A 1 Way Switch
X1101WH
Opale-16A 1 Way Switch, With Indicator
X1181WH

Electric Switches for Residential, Commercial & Industrial Applications

Most people don’t really notice electric switches until one stops working. Yet they are part of almost every moment in a space. From switching on bedroom lights to controlling heavy equipment in factories, switches work everywhere. Electric switches are used across different places- homes, workplaces, and industrial setups. Each of these places have slightly different expectations from switches.

Electrical switches for home mainly aim for daily comfort. They operate lights, fans, and small appliances. Commercial electric switches usually face more frequent use as they are placed in offices, cafes or showrooms. Hence, steady performance becomes important.

Industrial spaces are a different story altogether. Industrial electric switches are built for higher loads. They are suitable for tougher working environments where machines run for long hours.

Across these environments, properly selected electrical control switches support dependable functioning while aligning with safety and installation guidelines followed by professionals.


How to Choose the Right Electric Switch for Your Requirement

Choosing the right electric switch often starts with simple questions rather than technical terms. Where will it be used? How often? And under what conditions? Thinking through everyday usage, surroundings, and basic safety needs helps narrow down options and avoids issues later on.


Start with Load and Voltage Details

When planning to choose electric switch, it’s helpful to first understand how much electrical load the circuit carries. Checking the voltage rating and current rating can prevent long-term issues and helps match required electrical safety standards.


Think About Control Points

Proper electric switch selection also depends on how you want to control lighting or appliances. Some spaces only need single-point control. On the other hand, places like staircases or hallways may need two or more control points.


Consider Where the Switch Will Be Installed

The best electric switch for home or commercial areas often depends on surroundings. Switches placed in damp, dusty, or outdoor spaces may need additional protective design.


Check Compatibility with Wiring Systems

Modern wiring layouts often follow modular patterns. Making sure the switch works well with these systems usually helps with maintenance and long-term reliability.


Switch Categories Available in This Section

You must understand different switch categories. It helps in selecting products suited to specific installation and usage needs. Each type is designed for a particular environment, control preference, or wiring layout. Exploring these categories makes it easier to identify switches that match operational requirements while supporting organised installation and smooth electrical performance


Modular Electric Switches

Modular electric switches are commonly used in modern interiors. They are frequently installed in homes, offices, and renovated spaces where design and organised wiring both matter. Modular switches for home and office offer neat installation and flexible wiring arrangements.


Touch & Smart Switches

Touch and smart electric switches are increasingly seen in homes and workplaces that use automation or connected devices. They allow easier operation. Touch switches fit well into modern lifestyle setups where convenience is a priority.


Control & Selector Switches

Control and selector switches are typically used inside panels or machinery systems. Control switches help operators manage different functions and settings. They are especially useful for industrial switch control where equipment control needs to be precise and reliable.


Why Choose Schneider Electric Switches

Schneider Electric switches are widely recognised. They get appreciated for their consistent manufacturing standards and dependable performance. These switches are designed to handle repeated use without affecting functionality. They are also developed to follow recognised electrical safety practices commonly used in professional installations. Their build quality supports long service life, which makes them suitable for residential, commercial, and industrial environments.

Because of this reputation for steady performance and electrical safety compliance, these reliable electric switches are often preferred by electricians and project planners.


Frequently Asked Questions


Q1: Which electric switch is suitable for home use?

Ans. Most people simply want switches that work smoothly for their homes. They don’t want them to create problems later. An electric switch for home used for lights, fans, and common appliances is enough for regular household needs. Residential electric switches must offer comfort, durability, and proper fitting with existing wiring.


Q2: What is the difference between one-way and two-way electric switches?

Ans. A one-way switch offers light or appliance control from a single point. On the other hand, a two-way switch lets you control the same light from two different locations. Staircases commonly use it. They are also used in long hallways.


Q3: Are these electric switches suitable for industrial applications?

Ans. Some switches are designed specifically for industrial environments. The industrial electric switches are built stronger. Hence, they can handle repeated operation and heavier electrical loads. They are often installed in machinery areas and control panels. This is because these spaces need dependable performance.


Q4: What load capacity should I check before selecting an electric switch?

Ans. You must know how much electric switch load rating is required before election. Every switch handles a different level of current and voltage. Select the one that matches your requirement. This helps prevent heating issues and supports safe, long-term operation.


Q5: Do electric switches comply with Indian electrical standards?

Ans. Most switches available in India are manufactured following recognised safety guidelines. The electrical safety standards India are created to ensure switches can be installed safely. Also, this ensures their proper functionality. These standards help maintain safety across homes, offices, and industrial spaces.


Q6: Can electric switches be used with modular wiring systems?

Ans. Yes, many modular electric switches are designed to work easily with modular wiring systems. These switches are commonly preferred because they provide a cleaner installation and are simpler to replace if needed. Modular wiring has become quite popular in both residential and commercial spaces.


Q7: Are smart and touch switches compatible with standard electrical fittings?

Ans. In many cases, smart and touch switches can be installed with standard electrical fittings. However, compatibility may depend on wiring setup and automation requirements. It is usually better to confirm installation details of the smart electric switches or consult a professional before making the change.


Q8: How do I choose the right electric switch for commercial spaces?

Ans. Commercial electric switches usually need to handle frequent usage throughout the day. Offices, stores, and public areas often require switches that remain reliable even after repeated operation. Considering load demand and usage pattern usually helps in choosing the right switch.



Similar Searches

Power Switch Power Socket Modular Switch Electric Switches Electric Switch Boards Electric Sockets DP Switch Small Switches Fan Regulator TV Socket Switch Board Cover Power Plug Modular Electric Board Modular Switch Board Modular Plate Isolator Switch

Popular Searches

3 Phase Motor Starter 3 Pin AC Plug 16 Amp Switch Board 6A Socket 3 Pin Socket 6 Amp Switch 10 Amp Switch 20 Amp Switch 32 Amp Switch

Top Schneider Brands

Miluz Zeta AvatarOn Unica Pure Livia Zencelo Miluz Lara Opale

Best-Selling Schneider Electric India Electric Switches - Price List (2026-2027)

Updated Date: 08 November, 2026

Top Popular Best-Selling Schneider Electric India Electric Switches - Price List (2026-2027) Latest Price
Unica Pure-6Ax 1 Way Switch, Grey ₹ 261.00
10A 1 way Switch ₹ 162.00
Switch, Miluz Zeta, 10A, 1 Way, 1 Module, Warm Grey ₹ 174.00
Switch, Miluz Zeta, 10A, 1 Way, 1 Module, Anthracite ₹ 174.00
16AX 1 way switch ₹ 258.00
Switch, Miluz Zeta, 10A, 1 Way, 1 Module, White ₹ 145.00
Unica Pure-32A Dp Switch With Indicator, Grey ₹ 1,623.00
Opale - 6A 2 Way Switch ₹ 345.00
Unica Pure-16Ax 2 Way Switch, Grey ₹ 585.00
16A 1-way switch 2 module ,PG ₹ 590.00