Difference Between Latch and Flip-Flop: Working, Types and Comparison

Summary
Both latches and flip-flops store one bit of data. They differ in how they react to a control signal. This guide explains the difference between latch and flip flop circuits. It shows how does a flip flop work with a clock edge and how a latch responds to a level. It compares the D latch and D flip flop difference in a table. It also lists the advantages of flip flop over latch in timing, noise and design safety.
Key Takeaways
- Latches are level-sensitive storage circuits, while flip-flops capture and store input data only at a clock edge.
- Both circuits are sequential elements that store one bit of data using two stable output states.
- D latches follow input changes while enabled, whereas D flip-flops sample the input at defined clock transitions.
- Flip-flops offer predictable timing, improved noise immunity, and reduced race-through risks in synchronous digital system designs.
- Latches provide faster data paths and lower power consumption, making them useful in specific low-power storage applications.
- Choosing between latches and flip-flops depends on timing requirements, clocking methods, power limits, and design complexity.
Introduction
Digital systems need to store information; for example, a counter has to keep its count, a processor must retain an address, and a controller has to maintain its state between steps. There are two simple types of circuit that enable this: one is the latch and the other is the flip-flop. Although they appear identical on a block diagram, they behave in a completely different way over time. Many designers face the question of latches versus flip-flops at an early stage and the answer has a major impact on the whole timing plan. Consider a door: a latch is similar to a door which remains open as long as the handle is held; a flip-flop is like a camera that takes one picture at a particular moment. The sections that follow explain each circuit and the main points of difference between latch and flip-flop.
What is a Latch
A latch is a type of bistable storage element with two stable output states and has a data input, an enable input, and an output pair consisting of Q and Q-bar. So long as the enable signal is active, the output matches the input; this is the reason why the device is referred to as transparent, and after the enable signal has become inactive, the output remains at the value it had at that instant. The simplest form of latch is the SR latch, which is constructed using two NOR gates or two NAND gates connected in a cross-coupled configuration. There is a forbidden state in which both inputs are active at the same time and this results in an undefined output. In practice, however, the D latch is used more frequently since it eliminates that forbidden state and requires only a single data input.
What is a Flip-Flop
A flip-flop is actually a bistable device too, but it only responds to a specific clock edge; between edges the output remains unchanged no matter what the input does. The various types are SR, JK, D and T. Each of these has a different set of inputs and a different truth table. The D type merely copies the input to the output at the clock edge. The JK type has the property of toggling when both inputs are high. It is not generally known that most flip-flops include latches within them; a typical edge-triggered design makes use of two latches which operate on opposite clock levels, and it is this combination of the two latches that produces the edge response.
How Does a Flip-Flop Work
Understanding how does a flip flop work means following the clock. The circuit ignores the input for most of the cycle and reads it for only a tiny window. Three ideas explain the behaviour.
Edge Triggering
A flip-flop takes in data at the moment the clock signal changes. In the case of a positively edge-triggered device, the input is accepted as the signal rises from 0 to 1; with a negatively edge-triggered device, the input is sampled when the signal falls. During the time period between these two events, any changes to the input have no effect on the output. It therefore occurs only once for each clock cycle. For instance, with a 100 MHz clock one update can happen every 10 ns.
Master-Slave Structure
A typical D flip-flop consists of two D latches connected in series, the master latch being transparent when the clock signal is low and the slave latch being transparent when the clock is high. On rising of the clock the master latch changes to a closed state and takes in the input value, at the same time the slave latch opens and forwards the value it has acquired to the output. Since only one of the latches is open at any given time, the data does not pass directly through.
Setup and Hold Times
The input has to remain stable for a short period both before and after the active edge; these times are known as the setup time and the hold time. Typical values range from a fraction of a nanosecond to a few nanoseconds, the exact figure depending on the logic family. A violation may cause the output to end up in an unpredictable state referred to as metastability, which is why timing checks are included in all synchronous designs.
How Does a Latch Work
The latch reacts to a level rather than to an edge and the way it operates depends on whether the enable input is active; this one rule is what accounts for its speed, simplicity, and the risks it involves.
SR Latch Operation
An SR latch constructed using NOR gates has set and reset inputs: if S is made high, then Q is set to 1, and when R is made high, Q is taken to 0. Whenever both inputs are low, the latch keeps its previous state. The condition in which both inputs are high is not permitted since both outputs go to 0 and the subsequent state depends on which input becomes low first. A gated version includes an enable input which prevents any changes when the device is inactive.
D Latch Operation
A complementary inverter is included in the D latch to ensure that S and R are not both at a high level at the same time. If the enable signal is high, then Q will take on the value of D; but if the enable signal is low, Q remains unchanged. This property, which is called transparency, has a dual effect in that the data is transmitted quickly, with a delay equivalent to that of a few gate stages. At the same time, any noise or glitch on D while the enable signal is high is also passed on to the output.
Timing and Transparency Issues
During the entire enable period the latch remains open, which allows signals to pass through more than one latch in a single phase; this situation is known as a race-through problem. In order to avoid it, designers use two-phase clocks so that the adjacent latches open on different phases. A thorough timing analysis is required, and the tools employed must take into account time borrowing, which occurs when a slow path uses up the spare time from the following stage.
Difference Between Latch and Flip-Flop
A clear latch vs flip flop difference is that a latch responds while its enable signal is active, whereas a flip-flop responds at a clock edge.
The way in which latch circuits and flip flop circuits are triggered differs from one another in their timing control and in the number of gates required. The table given below sets out the main points side by side and answers the usual question about the difference between latch and flip flop from one point of view.
| Feature | Latch | Flip-Flop |
|---|---|---|
| Trigger type | Level-sensitive | Edge-triggered |
| Control signal | Enable or gate | Clock |
| Output changes | Any time enable is active | Only at the clock edge |
| Transparency | Transparent when enabled | Never transparent |
| Gate count | Fewer gates, usually 4 to 6 | More gates, usually 8 to 12 |
| Speed | Faster data path | Slightly slower due to two stages |
| Power use | Lower | Higher |
| Noise sensitivity | Passes glitches while enabled | Ignores glitches between edges |
| Typical use | Registers, small buffers, low-power designs | Counters, shift registers, state machines |
| Timing analysis | Complex, needs time borrowing | Simple and well supported by tools |
D Latch and D Flip-Flop Difference
When reviewing the d latch and d flip flop difference, the key point is whether data is followed during an enable level or sampled at a clock edge. This distinction is central to the broader latch vs flip flop difference in digital circuit design.
As both devices deal with the same data input, they can be readily confused with each other. The only distinction between the D latch and the D flip-flop is the moment at which the data is copied; in one case the input is copied during a particular time interval while in the other it is taken at a specific instant. The table illustrates the D latch and D flip-flop difference.
| Feature | D Latch | D Flip-Flop |
|---|---|---|
| Inputs | D and enable | D and clock |
| Capture moment | Whole enable period | Clock edge only |
| Output behaviour | Follows D while enabled | Copies D once per clock edge |
| Internal structure | Single stage | Two latches in master-slave form |
| Transistor count (CMOS) | About 8 to 12 | About 16 to 24 |
| Glitch on D | Passes to Q during enable | Ignored between edges |
| Best fit | Pipelines with two-phase clocks | Synchronous registers and counters |
Advantages of Flip-Flop Over Latch
The advantages of flip flop over latch include more predictable timing and reduced sensitivity to input glitches between clock edges. These benefits often guide the choice in synchronous systems.
There is a reason why flip-flops are used in synchronous design: they provide predictable timing and guard the stored data against noise. The advantages of flip-flops over latches can be divided into three practical areas.
Predictable Timing
The fact that a flip-flop only changes state at the clock edge means that all the registers in a design are updated simultaneously. Timing analysis therefore becomes simple since the engineers have only got to check that each path meets the setup and hold requirements and no further conditions. Timing tools can easily perform this function, which is the reason why flip-flops are the standard component in standard cell libraries as well as in FPGA fabrics.
Better Noise Immunity
The input is looked at for a very short period of time and any glitches that occur outside of this period have no effect. Unlike a latch, a latch will accept any change as long as the enable signal is active. This difference is significant in noisy factory environments with long signal lines. For instance, a timer relay circuit using a clocked register will not respond to a short spike that occurs between clock edges.
No Race-Through
A flip-flop is never transparent, so data cannot pass through two stages in one cycle. This removes the race condition that affects latch chains. Shift registers, counters and state machines depend on this property. Each stage moves data by exactly one position per clock pulse, and the design behaves the same way at every speed within its rated limits.
Conclusion
Timing, power, and noise requirements should also be considered; a Timer relay is a separate timing-control component used in many electrical applications.
Latches respond to a level whereas flip-flops react to an edge; this one difference has an impact on timing, noise characteristics and the amount of design effort needed. Because they are predictable and easy to check, flip-flops are appropriate for use in most synchronous systems. Latches are still used in situations where area, speed and power are most critical. The choice depends on the clocking style, the speed requirements and the degree of noise exposure. For control relays, timers, protection devices and panel components used in automation, Schneider Electric eShop offers a wide range of electrical products.
FAQs
1. What is a JK flip-flop and why is it useful?
A JK flip-flop has no forbidden state. When both inputs are high, the output toggles on each clock edge, which suits counters and frequency dividers.
2. What are preset and clear inputs?
The asynchronous preset and clear pins cause the output to be set to 1 or 0 all at once, rather than waiting for a clock edge, and they establish a certain state when the power is turned on.
3. What is a T flip-flop used for?
A T flip-flop changes state when its input is at a high level. When stages are connected in a chain, the clock frequency is divided by two at each stage, which results in a basic binary counter.
4. What is clock skew?
Clock skew is the difference in clock arrival time at two flip-flops. Excess skew can cause hold violations and wrong data capture.
5. Are flip-flops used in memory?
Flip-flops form registers and the cells of fast SRAM-style storage in small arrays. Large memories use denser latch-like cells to save area.
Comments