Current Divider Rule: Formula, Derivation & Solved Examples

Current Divider Rule: Formula, Derivation & Solved Examples

Summary

Current never splits evenly. Not unless resistances match exactly. The current divider rule solves this instantly. This guide covers the current divider formula. It explains the derivation. It also covers a general n-resistor version. A worked current divider rule example walks through the maths, step by step, including a three-resistor case. Applications in ammeter shunts and low voltage switchgear round things out. This guide shows how to find current through a resistor in any parallel network.

Key Takeaways

  • Current divides between parallel branches according to their conductance, or inverse resistance.
  • The lower-resistance branch carries more current than the higher-resistance branch.
  • The two-resistor current divider formula uses the opposite resistance in the numerator.
  • For three or more branches, the conductance-based formula should be used.
  • Kirchhoff's Current Law verifies that the sum of branch currents equals the total current.
  • The principle is useful in resistor networks, current shunts and parallel conductors.

Introduction

Current entering a parallel network rarely splits evenly. One branch often carries far more than another. Why does that happen? And how can branch currents be found quickly, without solving for node voltages first? So what is current divider rule, exactly? It answers this question directly. Current divider rule in parallel circuit analysis applies Ohm's Law (I=V/R). It also applies Kirchhoff's Current Law (∑Iin=∑Iout). Together, these two principles predict branch currents instantly. This matters well beyond textbook problems. Sizing parallel branch components depends on it. So does sizing current-sensing shunts and multi-conductor cables. Commercial panels and low voltage switchgear both rely on getting this calculation right.

Deriving the Current Divider Formula

Deriving the current divider formula starts from a simple picture. Total current ITI_T IT​ enters a node. It then splits between two parallel resistors, R1​ and R2​. Both resistors sit across the exact same two nodes. That means both experience the identical voltage drop, V. This single fact makes the whole derivation possible. Ohm's Law links voltage, current, and resistance at each resistor. Combining that with the parallel resistance formula produces a clean result. The end formula calculates a branch current directly. It uses only the total current and the two resistor values. No need to solve for node voltage separately.

Circuit Layout & Assumptions

Picture total current IT​ flowing into a node. From there, it splits between R1​ and R2​. Both are connected in parallel. Both resistors share the exact same node-to-node voltage drop, VV V. This shared voltage is the starting assumption. Without it, the formula could never be built. Every parallel resistor combination follows this same rule. That holds true no matter how many branches exist within the network.

Step-by-Step Mathematical Derivation

Start by finding the equivalent parallel resistance:

REQ = R1×R2 / R1+R2

Next, express the node voltage using Ohm's Law:

V = IT×(R1×R2 / R1+R2)

Substitute V back into the branch current equation (I1=V/R1​):

I1 = IT×(R1×R2 / R1+R2)/ R1 ⇒ I1 = IT×(R2 / R1+R2)

Current through R1​ is proportional to R2​. Not R1​. It divides by the sum of both resistances.

General Current Divider Formula (N-Resistor Parallel Network)

The simple two-resistor swap trick breaks down fast. Add a third branch, and it fails. A different approach handles any number of branches reliably. It uses conductance instead of resistance.

Why the Simple 2-Resistor Swap Rule Fails for 3+ Parallel Branches

Many learners assume the pattern continues. They expect:

I1 ≠ IT×[R2/ R1+R2+R3]

That assumption is wrong. The two-resistor formula only works because of how two parallel resistances specifically combine. Add a third branch, and that relationship breaks. A different method becomes necessary. It is built on conductance, not the resistor-swap shortcut.

The Conductance Approach

Conductance, G, equals 1/R. It is measured in Siemens. Branch current follows a cleaner pattern:

Ix​ = IT​×(Gx/ ​GT) = IT × (1/ Rx/ 1/ R1 + 1/ R2 + …..+ 1/ Rn)

This formula works for any number of branches. Two, three, or many more. No exceptions.

Alternative Parallel Equivalent Method

A second approach uses the equivalent parallel resistance directly:

Ix ​= IT ​× (Red/ Rx​​)

This method needs the overall equivalent resistance first. Then it applies to each branch. Both approaches, conductance-based or resistance-based, give identical results. The choice often comes down to which values are already known.

How to Use Current Divider Rule: Worked Numerical Examples

Seeing the formula in action helps far more than reading equations alone. This section works through two examples. One simple, two-resistor case. One three-resistor network. Each result gets checked against Kirchhoff's Current Law.

Example 1: Standard 2-Resistor Current Division

A total current IT=12 A enters a parallel circuit. It has R1=10 Ω and R2=30 Ω. The task is finding branch currents, I1 and I2. 

Apply the formula for I1:

I1 = 12 x (30/ 10 + 30) = 12 x (30/ 40)= 9 A

Apply the formula for I2:

I2 = 12 x (10/ 30 + 10) = 12 x (10/ 40)= 3 A

Example 2: Three-Resistor Current Division 

A total current imageenters a parallel circuit containing three resistors: image, image, and image. The task is to find the branch currents image, image, and image.

Apply the formula for I1:

I1 =  12 x (1/6) / (1/6 + 1/3 + 1/2) = 12 x (1/6) / 1 = 2 A

Apply the formula for I2::

 I2 =12 x (1/3) / (1/6 + 1/3 + 1/2) = 12 x (1/3) / 1 = 4 A

Apply the formula for I3:

 I3  = 12 x (1/2) / (1/6 + 1/3 + 1/2) = 12 x (1/2) / 1 = 6 A

Practical Applications in Electrical Systems & Low Voltage Switchgear

The current divider rule extends well beyond textbook exercises. Real systems rely on it constantly. From precision instruments to heavy industrial switchgear. Three applications show this range clearly.

Current Ammeter Shunts

A sensitive ammeter can only handle limited current. A low-resistance shunt resistor extends that range. It connects in parallel. Most circuit current bypasses the meter through the shunt. Only a small, predictable fraction flows through the meter itself. The current divider formula calculates exactly how much. This allows accurate scaling for far larger measurement ranges.

Parallel Cable Sizing in Low Voltage Switchgear

Heavy switchgear assemblies often use multiple parallel conductors. They carry large currents together. The current divider rule predicts how load distributes across them. Uneven contact resistance disrupts that distribution. So does unequal conductor length. One conductor ends up carrying more current than its neighbours. Hot spots form. Left unaddressed, this leads to thermal insulation breakdown and equipment failure.

Current-Steering Transistor Networks

Integrated circuits use parallel resistor paths often. So do amplifier bias stages. These mirror or split signal currents precisely. The same divider principle applies here too. Designers calculate exact branch currents during design. Each parallel path then carries precisely the intended fraction of total current. This precision matters enormously in sensitive analog circuits.

Conclusion

The current divider rule turns a complex parallel circuit problem into a quick calculation. Understanding the derivation matters. So does the general n-resistor version. Knowing how it applies across simple and complex networks removes guesswork entirely. From ammeter shunts to heavy low voltage switchgear design, this rule appears constantly in real engineering work. Components and technical resources for these applications, from shunt resistors to switchgear assemblies, are available through the Schneider Electric eShop.

FAQs

What is the main rule of the Current Divider Rule?

Incoming current splits across parallel branches in inverse proportion to resistance. The lowest resistance branch carries the largest share. The highest resistance branch carries the smallest.

How is the Current Divider Rule applied in low voltage switchgear design?

It evaluates how fault and load currents divide across parallel busbars, breaker contacts, or power cables. Equal resistance across parallel paths prevents one conductor from carrying excessive current. That prevents overheating and equipment failure.

Can the current divider rule be used with capacitors or inductors instead of resistors?

Yes, with modification. For AC circuits, resistance is replaced with impedance. Impedance accounts for both resistance and reactance. The same inverse relationship applies. A branch with lower impedance still carries more current, though the maths involves complex numbers.

What is the difference between the current divider rule and the voltage divider rule?

The current divider rule applies to parallel circuits. It finds branch current from total current. The voltage divider rule applies to series circuits instead. It finds voltage across a component from total voltage. Both stem from Ohm's Law and Kirchhoff's Laws.

What are the main factors that affect current distribution in a parallel circuit?

Current distribution depends mainly on the resistance of each parallel branch. A lower-resistance path carries more current, while a higher-resistance path carries less. In practical circuits, conductor length, connection resistance, temperature and component characteristics can also influence how evenly current is shared.

Older posts Newer posts