Capacitor Color Code: How to Read Color Bands, Number Codes & Tolerance

Summary
Small capacitor bodies leave little room for printed text. A decimal point like 0.0047 μF often gets lost entirely. This guide explains the capacitor color code system clearly. It covers how to read capacitor color code bands, alphanumeric printed codes, and tolerance letters. A capacitor value chart and a capacitor code chart are both included. Whether the task is ceramic capacitor color code identification or general capacitor value identification, this guide makes the process simple and reliable.
Key Takeaways
- A capacitor color code chart replaces tiny decimal points with clear bands.
- Each band carries specific meaning. Two bands give significant digits. One gives the multiplier. Others give tolerance and voltage rating.
- Modern capacitors often use printed digits instead, following a simple 3-digit rule.
- The letter R stands in for a decimal point on small values.
- Tolerance letters, from B to Z, cover a wide range of precision classes.
- Getting this reading right prevents costly component mismatches in any circuit.
Introduction
Printing a decimal point on a capacitor barely bigger than a grain of rice creates problems. A value like 0.0047 μF can smudge, fade, or simply vanish under poor lighting. Manufacturing errors follow close behind. So engineers found a better way. Scientific prefixes replaced awkward decimals. P stands for pico. N stands for nano. R stands in for the decimal point itself. Standardised multi-band capacitor color code systems solved the legibility problem too, encoding value, tolerance, and voltage into simple coloured stripes. Four parameters matter most when reading any capacitor. Nominal capacitance in pF, nF, or μF. Tolerance as a percentage. Maximum working voltage before dielectric breakdown. And temperature coefficient, which affects long-term stability under heat.
Standard Capacitor Color Code Chart & Band Meanings
Colour bands follow a fixed sequence across most capacitor types. Each colour maps to a specific digit, from zero through nine. The same colour also carries a multiplier value and often a tolerance rating too. This dual meaning can confuse beginners at first glance. Reading the table below carefully removes that confusion, since every colour's full meaning sits laid out clearly, band by band, digit by digit.
| Color | 1st Digit | 2nd Digit | Multiplier (pF) | Tolerance (>10 pF) | Tolerance (<10 pF) | Working Voltage Rating |
|---|---|---|---|---|---|---|
| Black | 0 | 0 | ×1 (10⁰) | ±20% | ±2.0 pF | — |
| Brown | 1 | 1 | ×10 (10¹) | ±1% | ±0.1 pF | 100V |
| Red | 2 | 2 | ×100 (10²) | ±2% | ±0.25 pF | 250V |
| Orange | 3 | 3 | ×1,000 (10³) | ±3% | — | — |
| Yellow | 4 | 4 | ×10,000 (10⁴) | ±4% | — | 400V |
| Green | 5 | 5 | ×100,000 (10⁵) | ±5% | ±0.5 pF | — |
| Blue | 6 | 6 | ×1,000,000 (10⁶) | — | — | 630V |
| Violet | 7 | 7 | — | — | — | — |
| Grey | 8 | 8 | ×0.01 | — | — | — |
| White | 9 | 9 | ×0.1 | ±10% | ±1.0 pF | — |
How to Read a 5-Band Color-Coded Capacitor (Step-by-Step)
A five-band capacitor packs a surprising amount of data into a small space. Each band answers one specific question, in a fixed order from top to bottom. Reading them in sequence turns five simple colours into a complete, usable specification.
Band 1 (Top / Outermost)
The first band gives the first significant figure of the capacitance value. This is always the outermost, or topmost, band on the component body. Reading direction matters here. Starting from the wrong end reverses every digit that follows, producing a completely wrong value. Orientation should always be confirmed before reading any further bands on the capacitor.
Band 2
The second band gives the second significant figure. Combined with band one, these two digits form the base number for the final calculation. For example, brown followed by black gives the digits 1 and 0, forming the base number 10. This base number then gets multiplied by whatever the third band specifies next.
Band 3
The third band is the decimal multiplier. It tells how many trailing zeros to add, expressed in picofarads. A base number of 10, multiplied by a factor of 100, gives 1000 pF, or 1 nF. This step is where most reading errors happen, since a single misread colour changes the result by a full order of magnitude.
Band 4
The fourth band gives the tolerance class. This tells how far the actual capacitance might vary from its printed nominal value. A tight tolerance, such as ±1 percent, suits precision timing circuits well. A looser tolerance, such as ±20 percent, suits general filtering applications where exact value matters far less to overall circuit performance.
Band 5
The fifth band, when present, gives the maximum DC working voltage. Exceeding this voltage risks dielectric breakdown inside the capacitor. Not every capacitor includes this fifth band, since some smaller components rely on printed text instead for voltage rating. Where present, though, this band completes the full specification picture in one glance.
Reading Alphanumeric Printed Codes
Many modern capacitors skip colour bands entirely. Printed digits take their place instead, stamped or laser-marked directly onto the component body. This shift reflects changes in how capacitors get manufactured and inspected today, rather than any change in the underlying values being communicated.
Why Modern Capacitors Use Printed Digits Instead of Color Bands
Printed digits suit high-speed manufacturing far better than painted colour bands. Automated optical inspection, or AOI, reads printed text more reliably than it reads subtle colour variations under factory lighting. Throughput improves as a result, since machines verify markings faster and with fewer false readings. This shift explains why many surface-mount capacitors now rely entirely on printed capacitor marking code systems rather than traditional bands.
The 3-Digit Rule
Most printed codes follow a simple three-digit pattern. The first two digits form the significant numerical base value. The third digit acts as a multiplier index, expressed as 10 raised to that power, in picofarads. For example, 103 means 10 multiplied by 10 to the third power, giving 10,000 pF, or 10 nF. This compact system fits easily onto even the smallest component bodies.
The 'R' Decimal System
For capacitance values under 10 pF, the letter R replaces the decimal point directly. This avoids printing a tiny, easily smudged dot on a very small surface. For example, 4R7 represents 4.7 pF exactly. The R simply sits where the decimal point would otherwise go, making the value unmistakable even under poor lighting or magnification.
Capacitor Tolerance Letter Code Lookup Table
Tolerance letters appear frequently alongside numerical capacitor codes. Each letter maps to one specific precision class, spanning a wide range from extremely tight to fairly loose. This lookup table covers the nine most common letter codes used across the industry today.
| Letter Code | Tolerance Rating | Letter Code | Tolerance Rating |
|---|---|---|---|
| B | ±0.1 pF | J | ±5% |
| C | ±0.25 pF | K | ±10% |
| D | ±0.5 pF | M | ±20% |
| F | ±1% | Z | +80%, -20% |
| G | ±2% | — | — |
Conclusion
Reading a capacitor accurately comes down to recognising the system in use. Colour bands, printed digits, or letter codes each encode the same essential information in a different format. Mastering how to read capacitor color code bands, along with the 3-digit printed system and tolerance letters, removes guesswork from component selection and circuit repair alike. This skill matters across general electronics work and within broader Industrial Automation settings, where a single wrong capacitor can cause a costly failure down the line. Reliable components for these applications, along with accurate technical documentation, are available through the Schneider Electric eShop for engineers and technicians building or maintaining precision circuits.
FAQs
What does '4R7' mean on a capacitor?
The letter R acts as a decimal point for capacitance values under 10 pF. Therefore, 4R7 represents a capacitance value of 4.7 pF.
What is the unit base for capacitor color codes and 3-digit codes?
The base unit for all capacitor color code multipliers and 3-digit printed codes is always picofarads. To convert to nanofarads, divide by 1,000. To convert to microfarads, divide by 1,000,000.
What happens if a capacitor's working voltage rating is exceeded?
Exceeding the maximum working voltage rating causes dielectric breakdown. This results in short-circuit failure, internal arcing, leakage current spikes, and potential physical destruction or explosion of the capacitor.
Do all capacitors use the same color code system?
No. Ceramic capacitor color code conventions can differ slightly from those used on film or tantalum types, particularly around voltage band placement. Checking the manufacturer's datasheet remains the safest approach whenever a colour band's meaning seems uncertain for a specific component family.
How can a capacitor value be verified without relying on markings?
A digital multimeter with a capacitance function, or a dedicated LCR meter, measures actual capacitance directly. This method works well when markings have faded, smudged, or become otherwise unreadable, and it also catches components that have drifted outside their rated tolerance over time.
Comments