What is a variable speed drive?

A variable speed drive is an electronic device used to control the speed and torque of an electric motor by varying the frequency and voltage of the power supplied to it. It is also known as a (VFD) variable frequency drive or adjustable speed drive (ASD). They are widely used in industrial and commercial applications to achieve energy savings, improve process control, and extend equipment lifespan. By adjusting the frequency and voltage output to the motor, VSDs enable smooth acceleration and deceleration, precise speed control, and efficient operation over a wide range of operating conditions. This allows for significant energy savings by matching motor speed to the required load, reducing mechanical stress on the motor and associated equipment, and minimizing energy wastage during partial load conditions.

Variable Speed Drives & Soft Starters

169 results

Sort By arrow-down
ATV12 2.2KW 240V 1PH HEAT SINK TB
ATV12HU22M2
Price starting from
₹ 46,518.00
₹ 21,630.87

The components of a VSD are:

Variable speed drives (VSDs) offer several benefits:

Types of Variable Speed Drives

VSD comes in several types, each suited to specific applications and requirements:

FAQs