Home / Glossary / AC Motor
An AC Motor (Alternating Current Motor) is an electrical machine that converts alternating current (AC) electrical energy into mechanical rotational energy. Operating on the principle of electromagnetic induction, AC motors are the most widely used type of electric motor globally — found in household appliances, industrial pumps, compressors, HVAC systems, and conveyor equipment.
How Does an AC Motor Work?

The working principle is based on electromagnetic induction and the creation of a Rotating Magnetic Field (RMF):

  • 1
    AC Supply to Stator: Alternating current is supplied to the stator windings, generating a continuously rotating magnetic field.
  • 2
    Electromagnetic Induction: The rotating field cuts through rotor conductors, inducing a current in the rotor by Faraday's Law.
  • 3
    Torque Generation: The induced rotor current creates its own magnetic field, interacting with the stator field to produce electromagnetic torque.
  • 4
    Mechanical Output: The torque causes the rotor to spin, driving the shaft and delivering mechanical energy to the connected load.
Key Components

Stator

The stationary outer part containing three-phase windings placed 120° apart. Produces the rotating magnetic field when energised by AC supply.

Rotor

The inner rotating part mounted on the shaft. Follows the stator's rotating magnetic field and converts electromagnetic torque into mechanical rotation.

Air Gap

A small physical gap between stator and rotor that allows magnetic flux to efficiently link both components without mechanical contact.

Shaft and Bearings

The shaft transmits rotational mechanical energy to the load. Bearings support the shaft and enable smooth, low-friction rotation.

Types of AC Motors

Induction Motor (Asynchronous)

The most common type. Rotor speed is slightly less than the stator's rotating field speed (slip). Available in single-phase and three-phase. Simple, robust, low maintenance.

Synchronous Motor

Runs at exactly the same speed as the rotating magnetic field with no slip. Requires external rotor excitation. Used where constant speed is critical.

Single-Phase Induction Motor

Powered by single-phase AC supply. Common in household appliances — fans, refrigerators, washing machines. Requires starting mechanisms such as capacitors.

Three-Phase Induction Motor

Powered by three-phase AC supply. Self-starting, highly efficient, and used in heavy industrial applications — compressors, conveyors, cranes, and HVAC systems.

Common Applications
  • Industrial pumps and water treatment plants
  • HVAC and air conditioning systems
  • Conveyor belts and material handling
  • Compressors and blowers
  • Household appliances — washing machines, fans, refrigerators
  • Electric vehicles and elevators
  • Power tools — drills, grinders, saws
  • Food and beverage processing equipment
AC Motor vs DC Motor
Parameter AC Motor DC Motor
Power Source Alternating Current (AC) Direct Current (DC)
Construction Simple, fewer parts More complex (brushes, commutator)
Maintenance Low — no brushes Higher — brushes wear out
Speed Control Via Variable Frequency Drive (VFD) Easier direct control
Cost Lower initial cost Higher initial cost
Best For Industrial and commercial use Precise speed and torque control

Shop Related Products
AC Drives and VFDs

AC Drives and VFDs

Control and optimise AC motor speed and torque with our range of variable frequency drives.

Shop Now
Motor Starters

Motor Starters

Direct-on-line and soft starters for safe and controlled starting of AC motors.

Shop Now
Contactors

Contactors

Electrically controlled switches for starting and stopping AC motors safely in circuits.

Shop Now
Overload Relays

Overload Relays

Protect AC motors from overheating and overload conditions with thermal and electronic relays.

Shop Now
Motor Protection

Motor Protection

Circuit breakers and protection devices designed specifically for motor applications.

Shop Now
Circuit Breakers

Circuit Breakers

MCBs and MCCBs for overcurrent and short-circuit protection in motor circuits.

Shop Now
Back to Glossary

Browse all electrical terms A to Z