calcPageSize())"
/>
Further offers for this product
Excl. Tax
In Stock
No sellers found for this product.
Excl. Tax
Motor Management, TeSys T, motor controller, operator control unit with fast device replacement service
TESYS T CONTROL DISPLAY UNIT FDR
- Description
- Specifications
- Reviews
Description
TeSys T is a motor management system that provides full motor monitoring, control, and protection when used with short circuit protection and a contactor. It manages most critical processes while reducing downtime and increasing productivity as well as predicts what will happen in the process, as it accurately monitors current, voltage, and power over a wide range. This motor management system is also a flexible system that supports six communication protocols which are Modbus™, CANopen, DeviceNet™, Profibus™, Ethernet/IP, and Modbus/TCP. TeSys T motor management system consist of several components which include the LTMR controller, the expansion module, HMI and software along with several accessories. The LTMR controller is the main component of the system that manages the basic functions. This includes the measurement of the ground current, motor temperature, three phase current of the motor, the controller also includes logic inputs and outputs which is used in fault management. The expansion module is directly connected to the controller and provides additional inputs as well as measure the voltage between the phases which allow the controller the monitor additional functions. TeSys T is highly reliable and has a very long product life thanks to a state-of-the-art component selection, to the all in one design and to the advanced electronic protection. TeSys T can be integrated in many different types of harsh environment such as dusty atmospheres, marine applications, high vibration applications and corrosive atmospheres and is used in Metal/Mining/Mineral, Oil & Gas, Water Wastewater. This is a TeSys operator control unit that is used in conjuction with LTMR controller to configure the parameters, display the information about the controller, display detected faults and control the motor locally. This operator unit has Fast Device Replacement Service (FDR). This operator unit has LCD screen to display the information along with 5 control keys and 4 LED indicators and has 2 ports for RJ45 connectors that are used to connect to the PC and controller.
Overview
| Product Name | TESYS T CONTROL DISPLAY UNIT FDR |
|---|---|
| Range Name | TeSys |
| Tax Class | GST-18 |
| Short Description | Motor Management, TeSys T, motor controller, operator control unit with fast device replacement service |
Reviews
Description
TeSys T is a motor management system that provides full motor monitoring, control, and protection when used with short circuit protection and a contactor. It manages most critical processes while reducing downtime and increasing productivity as well as predicts what will happen in the process, as it accurately monitors current, voltage, and power over a wide range. This motor management system is also a flexible system that supports six communication protocols which are Modbus™, CANopen, DeviceNet™, Profibus™, Ethernet/IP, and Modbus/TCP. TeSys T motor management system consist of several components which include the LTMR controller, the expansion module, HMI and software along with several accessories. The LTMR controller is the main component of the system that manages the basic functions. This includes the measurement of the ground current, motor temperature, three phase current of the motor, the controller also includes logic inputs and outputs which is used in fault management. The expansion module is directly connected to the controller and provides additional inputs as well as measure the voltage between the phases which allow the controller the monitor additional functions. TeSys T is highly reliable and has a very long product life thanks to a state-of-the-art component selection, to the all in one design and to the advanced electronic protection. TeSys T can be integrated in many different types of harsh environment such as dusty atmospheres, marine applications, high vibration applications and corrosive atmospheres and is used in Metal/Mining/Mineral, Oil & Gas, Water Wastewater. This is a TeSys operator control unit that is used in conjuction with LTMR controller to configure the parameters, display the information about the controller, display detected faults and control the motor locally. This operator unit has Fast Device Replacement Service (FDR). This operator unit has LCD screen to display the information along with 5 control keys and 4 LED indicators and has 2 ports for RJ45 connectors that are used to connect to the PC and controller.
Overview
| Product Name | TESYS T CONTROL DISPLAY UNIT FDR |
|---|---|
| Range Name | TeSys |
| Tax Class | GST-18 |
| Short Description | Motor Management, TeSys T, motor controller, operator control unit with fast device replacement service |