MCB Tripping: Reasons and How to Avoid it

Table of Content

Electrical faults due to overloading or shirt circuits are not uncommon. Generally, most homes as well as commercial setups have devices installed, which protect from short circuits or overloading. One such protective device is MCB, which stands for miniature circuit breakers. These are electromechanical devices that protect a circuit from electrical overloading and burnout. 

Popularly known as time delay tripping devices, MCBs trip and shut down the system whenever there is an overflow of current. This protects the entire circuit from damage and burnout. In the case of short circuits, the MCB trips and stops the power supply within just milliseconds. 

Companies manufacturing various kinds of electrical devices often make MCBs as well. Among the various brands, Acti 9 MCB is a popular one from the house of Schneider Electric. A great choice, Acti9 Schneider is highly energy-efficient for power distribution and extremely simple to install. 

In this article, we will discuss the importance of using good quality MCBs such as Acti 9 from Schneider Electric and how to choose one for your requirement. 

What is MCB?

An MCB (Miniature Circuit Breaker) is a safety device. It is designed to protect electrical circuits from overloads and short circuits. This device trips automatically to interrupt the power supply when the current exceeds a safe limit. MCBs are widely used in residential and commercial settings. They ensure electrical safety.

How MCBs Work

MCBs function by continuously monitoring the current flowing through a circuit. When an overload or short circuit occurs, the MCB trips and cuts off the power supply. This prevents overheating or potential fires. The tripping mechanism consists of a bimetallic strip for overload protection and an electromagnet for short circuit protection. This ensures quick response times to electrical faults.

MCB Tripping Reasons

Why MCB trips? There are several MCB tripping reasons as follows.

Overload

MCB trips to prevent overheating and potential fire hazards when the connected appliances draw more current than its rated capacity.

Short Circuit

A short circuit occurs when two conductors touch. This creates a surge of current that triggers the MCB to trip instantly.

Earth Faults

Does MCB trip on earth fault? Yes, MCBs can trip if there's an unintended connection between the live wire and the earth. They do so to ensure safety.

Faulty Appliances

Defective devices or loose connections can cause current fluctuations. This leads to frequent tripping.

Inverter Issues

MCB trips in inverters can occur due to incorrect wiring or voltage mismatches. This disrupts the electrical flow.

How to Avoid MCB Tripping?

You can avoid the MCB trip problem by following the below given tips.

Use Correct Load Capacity

Ensure that the MCB is rated for the total current drawn by connected devices to prevent overload.

Regular Maintenance

Inspect wiring and appliances periodically. This will help you identify potential issues like loose connections or worn-out components.

Separate Circuits for Heavy Appliances

Distribute high-load appliances across separate circuits to prevent overloading a single MCB.

Check for Faulty Devices

Regularly test appliances for defects that may cause power surges or excessive current draw.

How to fix MCB Tripping?

Now the question comes- How to fix MCB tripping? Below are the steps to be followed.

Identify the Cause

Diagnose the issue by isolating faulty appliances or pinpointing wiring problems.

Reset the MCB

Reset the MCB by turning it off and on after resolving the issue. Investigate further if it keeps tripping.

Upgrade MCB Capacity

Replace it with one of higher capacity if the load frequently exceeds the MCB’s rating.

Consult an Electrician

Seek professional assistance to ensure the issue is addressed safely if you face persistent problems.

Why MCB Trips Frequently?

Below are the reasons explaining why MCB trips frequently.

Overloaded Circuits

When multiple appliances run simultaneously on a single circuit, it can cause frequent tripping.

Wiring Issues

Faulty or old wiring can result in current leakages, leading to repeated MCB tripping.

Undersized MCB

Using an undersized MCB that doesn’t match the circuit’s load can lead to frequent trips.

Environmental Factors

High humidity or extreme temperatures can impact electrical circuits and cause the MCB to trip.

Why should you choose good quality MCB?

If you notice that your MCB is tripping frequently, understand that it needs your immediate attention. Along with overloaded circuits and short circuits, a ground fault is another one of the main reasons for MCB tripping. A good quality MCB will trip at the slightest fault ensuring protection for the connected devices. This is the reason you must ensure that you use the best quality MCB like Acti 9 MCB for your home or commercial establishment. 

Here are some other reasons why you must always choose a good quality MCB for your requirements:

  • The rivet material and the enclosure of a good quality MCB will be able to withstand the arc energy which is produced by the circuit breaker when the current passing through it gets hampered. With a good quality MCB, there are no chances of hazards or MCB damage. 
  • A good quality MCB will have an MCB coil with a large diameter. As a result, there will be no risks of temperature surge and there will also be no problem in closing the circuit. 
  • A standard high-quality MCB like Acti9 Schneider always use superior contact material, which kicks into action on time when required. The breaking process is much better in such MCBs, causing minimal equipment damage. 
  • A good quality MCB will trip immediately in case of an overload. This protects the circuit and the various appliances and equipment in line. 
  • A high-quality bimetal sheet is used in good-quality MCBs. As a result, the MCB responds to short circuits immediately and breaks the circuit at once. And once things get back to normal, the MCB starts to function normally again. 

Which type of MCB is best for your home?

MCB installation is done in different places depending on the requirements and the range of protection that is needed. Therefore, different kinds of MCBs are available in the market catering to a wide range of purposes. Some of the most common kinds of MCBs include A, B, C, D, K, and Z. This categorisation is done depending on the tripping capacity or trip curve. 

Among all the MCBs available in the market, the two most common kinds of MCBs include:

  • Type B – These MCBs are extensively used in industrial units with small-scale operations or residential properties. These MCBs trip when the power supply exceeds five times or more than the suggested limit. These are highly sensitive MCBs as they have an extremely low tolerance for voltage fluctuations. In the majority of residential spaces, current surges and voltage fluctuations are not that intense and therefore type B MCBs are highly preferred here. 
  • Type C – These MCBs are suitable for devices and appliances which require high power consumption. Many household appliances like mixers, grinders, motor pumps for drawing water, geyser, instant water heaters, irons, etc. have high power consumption. Along with the residential use for the above-mentioned devices, type C MCBs are also high in demand in industrial and commercial units. 

Type C MCBs trip when the electric flow surges to more than 10 times the suggested limit. You will commonly see these MCBs used with fluorescent lights and electric motors. When compared to type B MCBs, type C offers a higher range of protection. Not only this, type C MCBs can handle electrical surges as they have higher capacity. 

Also Read: MCB: Guide - Types, Sizes, And Uses

Purchase MCBs for your requirements from a trusted place

If you are looking for high-quality electrical devices including MCBs, there is no better place than the Schneider Electric e-shop. You will find the most suitable MCBs for your home including Acti 9 MCB from the Schneider Electric e-shop. Along with this above-mentioned model, you will get other MCBs, which are great for use in commercial, residential, and industrial setups. Check the product details of the MCB to understand if it syncs well with your requirements before making the final purchase. Apart from MCBs, the Schneider Electric e-shop houses other electrical products as well. Visit https://eshop.se.com/in/ to know more.

How to Identify the Cause of Circuit Breaker Tripping?

Identifying the cause of MCB tripping is crucial to ensure electrical safety. Here are the key reasons for MCB tripping and how to diagnose them:

  • Overloaded Circuit- If multiple devices are connected to a single circuit, it may exceed the load capacity, leading to tripping. Unplug some appliances and check if the issue persists.
  • Short Circuit- A sudden surge in current due to damaged wiring or faulty devices can cause MCB tripping. Look for burnt smells, sparks, or discolored outlets.
  • Ground Faults- An unintended connection between live and ground wires can trigger a ground fault circuit interrupter (GFCI). Use a tester to check for ground faults.
  • Faulty MCB- Sometimes, an old or defective MCB itself may be the problem. Consider replacing it if tripping continues despite troubleshooting.
  • Environmental Factors- High humidity, dust, or temperature variations can impact the MCB’s performance, leading to frequent trips. Ensure the electrical panel is clean and dry.

FAQs

Q1. What is the role of a bimetal sheet in an MCB?

Ans: The bimetal sheet in an MCB acts as a thermal sensor. It bends when excessive current flows. This triggers the MCB to trip and prevent electrical overload.

Q2. How often should I replace my MCB?

Ans: MCBs typically last for years, but they should be replaced if they frequently trip, show signs of damage, or fail to function correctly.

Q3. Can environmental factors affect my MCB's performance?

Ans: High humidity, dust accumulation, and extreme temperatures can impact MCB efficiency and lead to unwanted tripping.

Q4. Is it safe to use multiple devices on one circuit protected by an MCB?

Ans: It depends on the circuit’s capacity. Overloading a circuit with too many devices can cause MCB tripping. Distribute the load across multiple circuits for safety.

Q5. What should I look for when purchasing an MCB?

Ans: Consider factors like the types of MCBs (B, C, D curve), rated capacity, short circuit protection, and brand reliability to ensure optimal performance and safety.



Older posts Newer posts