How to Find the Suitable Size of Cable & Wire for Electrical Wiring Installation?

In the realm of electrical installations, one crucial element often dictates the success of an entire project: the selection of the right cable and wire size. Whether you are working on residential wiring or overseeing a complex industrial setup, the size of cables and wires used can profoundly impact the efficiency, safety, and longevity of the electrical system.

The task of determining the suitable cable and wire size, however, can be a confusing and difficult technical journey. Undersized wires can lead to overheating and potential hazards, while oversized cables might result in wastage and inefficiency. Striking the delicate balance requires a blend of mathematical precision, knowledge of electrical standards, and an understanding of the unique demands posed by each application.

Table of Content

In this article, we shall learn all about how to calculate cable size and wire size for your electrical wiring installations.

Why Cable Size Matters in Electrical Wiring?

Selection of the correct cable size is essential for electrical safety and efficiency. This is because inappropriate size can result in overheating and cause potential hazards like electrical fires. Hence, you must know how to select cable size and cable size calculation formula. A proper-sized cable ensures optimal power distribution and energy efficiency. It also prevents damage to electrical systems. Proper selection of cable size also improves system performance and reduces energy losses.

Prevent Overheating and Fire Hazards

An undersized cable may not be able to carry the required load. Hence, it may result in overheating and possibly lead to electrical fires. Correctly sizing cables prevents these dangers and ensures electrical safety.

Improve Energy Efficiency

An appropriate cable size helps minimize energy losses. A correctly sized cable ensures that the current flows efficiently. This results in reducing energy wastage and maintaining overall system efficiency.

Reduce Voltage Drop

Voltage drop occurs when electrical energy is lost due to the resistance of cables. The voltage drop can be minimized by selecting the right cable size. It ensures that appliances and systems function optimally.

Compliance with Electrical Standards

Proper cable sizing ensures that your installation complies with electrical codes and safety standards. Compliance is essential for both residential and commercial electrical systems.

Why is Correct Wire Size Important?

Choosing the correct wire size is crucial in electrical wiring installation. This is because it directly impacts the efficiency, reliability, and safety of the system. An undersized wire can lead to excessive heat generation. This results in increasing the risk of fire hazards and reducing the lifespan of electrical components. On the other hand, an oversized cable results in unnecessary costs and inefficient energy transmission. The proper selection ensures minimal voltage drop, compliance with electrical installation guidelines, and optimal performance of electrical devices.

Key Factors that Influence Cable Size Selection

Selection of the right  cable size depends on various factors. It includes the load requirement, distance, ambient temperature, and type of installation. Properly understanding these factors ensures the safe and efficient operation of electrical systems. Read below to understand how to choose cable size.

Load Requirement

The amount of current that the cable will carry determines its size. Higher loads require cables with a larger cross-sectional area to avoid overheating and ensure the system operates safely.

Length of the Cable Run

Longer cable runs result in higher resistance. This leads to voltage drops. Larger cables are required to maintain efficiency and prevent performance loss for longer distances.

Ambient Temperature

The surrounding temperature can affect the cable’s ability to carry current. Higher temperatures require larger cables to avoid overheating. This factor should always be considered when choosing cable sizes.

Type of Insulation Material

Different insulation materials have varying temperature and current-carrying capacities. The type of insulation used in the cable influences its size and suitability for specific applications.

All these factors are crucial for the cable selection formula. So, you must understand them for the right selection.

Electrical Cable Sizing Chart

Selection of the right cable size for electrical wiring installation requires an understanding of the current carrying capacity, voltage drop considerations, and environmental factors. Below is a general guide for cable size selection based on common electrical loads:

Load (Amps)

Cable Size (sq. mm)

Voltage Drop (V/m)

10 A

1.5 sq. mm

3.3

16 A

2.5 sq. mm

2.0

25 A

4.0 sq. mm

1.2

32 A

6.0 sq. mm

0.8

40 A

10 sq. mm

0.6

Electrical Cables Size & Current Rating Chart

You must understand the relationship between cable size and current rating for ensuring safe electrical wiring installations. Below is a reference table for common cable sizes and their current ratings:

Cable Size (sq. mm)

Approx. Current Rating (A)

1.5

10

2.5

16

4.0

25

6.0

32

10.0

40

Cables and how they can impact voltage drop

It is common knowledge that all conductors (other than some superconductors), cables, and wires are characterised by some resistance. It is important to note that resistance is inversely proportional to the conductor’s diameter and directly proportional to its length.

Therefore, R ∝ L/a … [Laws of resistance R = ρ (L/a)]

The conductor experiences a voltage drop whenever an electrical current passes through it. This drop may be negligible for conductors that are of smaller length. But in the case of longer conductors and conductors with a narrow diameter, considering voltage drops is important if correct installation and safety are to be ascertained.

The IEEE rule B-23 mandates that voltage drop should never be larger than 2.5% of the supply voltage at any place between installation and power supply.

Let us take a look at an example:

If supply voltage is 160V AC, then voltage drop can be allowed up to:

Permissible Voltage Drop = 160 x (2.5/100) = 4V

Voltage drops in cables can be measured using two systems of measurement.

The FPS (foot pound system) utilizes a length-based (100 ft) system to calculate voltage drop.

The SI (system international and metric system) calculates voltage drop in amperes per meter (A/m).

Nowadays, you can search for cable current carrying capacity calculator on the web to access several such free tools.

How do I calculate the voltage drop in a cable?

The steps for calculating voltage drop in the cable are as follows:

First, measure the highest permissible voltage drop.

Second, calculate the load current.

Third, you must know that the most appropriate cable will be one that has a current rating closest to the load current calculated. Several charts with cable sizes and corresponding current ratings are easily available online. Use such a chart to select a suitable cable.

Fourth, use the chart to also locate voltage drop in meters or 100ft, according to your system of preference.

Fourth, use the chart to also locate voltage drop in meters or 100ft, according to your system of preference.

Fifth, use the following cable size and current rating formula for calculating voltage drop along the actual length of the wiring circuit.

  1. 1. If you want to calculate the drop in voltage per meter, (Actual length of circuit x volt drop for 1m) /100
  2. 2. If you want to find the drop in voltage in 100ft (Actual length of circuit x volt drop for 100ft) /100

After calculating the above, you have to multiply the value you get with the load factor -

Load factor = Load Current to be taken by Cable/ Rated Current of Cable (which should be given in the chart you are referring to).

Now, you have arrived at the voltage drop value of the cable when the load current passes through it.

If this value is less than the maximum permissible voltage drop, then the size of the cable selected should be okay.

However, if the value is higher than the value of the maximum permissible voltage drop, then the voltage drop for the next greater-sized cable according to the referred chart has to be calculated. This process has to be continued until the value of the voltage drop becomes less than the maximum permissible voltage drop value.

Common Cable Sizes for Residential and Commercial Use

Cable sizes vary depending on the application and electrical load. You must understand the standard sizes to choose the correct one for your specific needs.

Residential Wiring

Cables such as 2.5mm² for lighting circuits and 4mm² for power circuits are commonly used for home wiring. These sizes ensure safe and efficient power distribution in household applications.

Commercial Wiring

Commercial buildings typically require larger cables, such as 6mm² or 10mm². It depends on the electrical load and distance. These sizes help in efficiently managing the increased power demand in commercial setups.

Industrial Use

Cable sizes may range from 10mm² to 50mm² or more for industrial applications. Their size depends on the machinery and equipment that need to be powered.

Specialty Applications

Larger cables like 16mm² and 25mm² are chosen for certain specialized installations, such as high-power equipment or outdoor applications. They handle higher electrical demands and external factors.

How can I determine precise wire and cable size for a certain load?

First, you need to keep in mind that cable sizes corresponding to given loads can be ascertained with the help of standardized tables and charts available online but certain rules regarding voltage drop must be heeded.

There must be a 20% additional scope of current for emergency or future requirements for a given load other than the known current value.

Voltage drop must be limited to 1.25% from the energy meter to the distribution board while it should not be more than 2.5% of the supply voltage for the final sub-circuit.

Temperature variations have to be considered as per needs. Temperature factor charts are also easily available online and can be referred to.

You also need to keep in mind the load factor when trying to estimate cable size.

Two other factors that need to be considered in the determination of cable size are the type of wiring system and the diversity factor in installation.

Let us now look at a solved example using a wire size calculation formula to better understand this.

Example of wiring size calculation:

The total load for the installation of electrical wiring in a building is 5.5kW and the total length of cable from the meter to the distribution board is 40 feet. Supply voltage is 220V and temperature is recorded at 35°C. Calculate the most appropriate cable size from meter to sub-circuit for wiring to be installed in conduits.

Solution:

Total Load = 5.5kW =5.5 x 1000W = 5500W

20% additional load = 5500 x (20/100) = 1100W

Total Load = 5500W + 1100W = 6600W

Total Current = I = P/V = 6600W /220V =30A

Now select the size of cable for a load current of 30A from your referred chart or table. This should be around (7/0.044) (34 Amperes). Accordingly, we can use (7/0.044) cable.

Thereafter, you need to match the (7/0.044) cable with the charted temperature factor. This value should be around 0.97 at 35°C and the current carrying capacity of (7/0.044) is 34A. Therefore, the current carrying capacity of this cable at 35°C could be calculated as:

Current rating for 35°C = 34 x 0.97 = 32.98 A

As the calculated value (32.98 A) at 35°C is less than that of the current carrying capacity of (7/0.044) cable which is 34A, this cable size (7/0.044) is also appropriate with the given temperature.

Next, you need to calculate the voltage drop for 100 feet for this (7/0.044) cable from cable size charts with corresponding current ratings and voltage drops available online. This value should be around 5.7V. Since in this case, the length of the cable is 40 feet, the voltage drop for 40 feet cable would be calculated as:

Actual Voltage drop for 40 feet = (5.7 x 40/100) x (30/34) = 2.01V

And Allowable voltage drop = (2.5 x 220)/100 = 5.5V

Therefore, we can see that the actual voltage drop (2.01V) is less than that of the maximum permissible voltage drop of 5.5V. Hence, the most suitable cable size is (7/0.044) for the given load.

Also Read: Type of Electric Cables & Conductors with Application

Get your cables at the Schneider Electric eShop!

Schneider Electric has been a trusted name in the market for electric cables and wires for over two decades. For those who want to avoid the hassles of complicated calculations, visit the Schneider Electric eShop for expert consultation on cable sizes best suited to your exact requirements.

FAQs

Q1. How do temperature variations affect cable selection?

Ans: Temperature variations impact the current-carrying capacity of cables. Higher ambient temperatures reduce cable efficiency, necessitating a larger cable size to compensate for increased resistance. Usage of temperature factor charts helps in determining the appropriate size adjustments.

Q2. What is a load factor?

Ans: The load factor represents the ratio of the actual electrical load used over a specific period to the maximum possible load. It helps with cable size calculation by ensuring a buffer for peak demands.

Q3. Can I use online calculators for cable sizing?

Ans: Online wire size calculation tools simplify the process by considering factors like voltage drop in cables, current rating, and load factor. However, it's essential to cross-check results with standard electrical installation guidelines.

Q4. What happens if I choose an undersized cable?

Ans: Usage of an undersized cable results in overheating, excessive voltage drop, and reduced efficiency. This can lead to premature failure of electrical devices and pose significant safety risks.

Q5. What is the significance of diversity factor in installations?

Ans: The diversity factor accounts for the probability that not all electrical devices will be operating simultaneously. It helps in optimizing cable size selection, reducing costs, and preventing unnecessary oversizing of cables.

Older posts Newer posts