How to Convert Normal Lights to Smart Lights?

Smart lights have gained incredible popularity over the past years, making them some of the most frequently purchased units. And given the amazing advantages they bring into your household; it is no surprise that most modern homeowners have started to prefer smart lights to traditional incandescent lights. This article discusses the incredible benefits of smart lights and how to make normal lights smart.

Converting to Smart Lights

When it comes to how to make normal lights smart, adopting a completely new lighting system for your house might seem like a challenge, but there is no need to worry. Smart lights are extremely easy and intuitive to use and can be operated efficiently without a hassle. Mentioned below are some of the tips that can get you ready for these futuristic smart lights in your home:

  • Smart lights are exceptionally easy to install and maintain and do not necessarily require expensive investments and rewiring. However, getting your house future-ready with smart lights might need you to get the wiring in your house checked by a professional against damages, as well as to avoid any electrical accidents in the future.
  • Installing smart lights in your house can also need you to install smart switches for efficient control. Smart switches are programmable modules that can seamlessly connect with your household electricity lines and home automation system without the need for any complicated electrical rework.
  • If you are looking for a budget-friendly alternative to new smart lights, you can always look into smart light bulb adapters and smart switch converters, that can be used to remodel existing lightbulbs so they can be remotely accessed using home automation systems and smartphone devices. These adapters and smart switch converters are equally efficient and easy to install as they do not require any additional hubs or wiring.
  • And if your smart home lighting system is already in place, it might be a good time for you to invest in a home automation system or smart AI assistants for seamless access. Smart lights can be efficiently synchronized with home automation systems, granting you complete control from the smartphone app. AI assistants like Google, Siri and Alexa can also allow you to access the control module of your smart lights with voice commands.

Advantages of Smart Lights

On the surface, upgrading from normal lights to smart lights might not sound like a lot, since both serve the primary function of illuminating an area. However, if you consider the exciting new advantages that smart lights bring to your household, you might want to give smart lights a shot. So, mentioned below are some of the amazing benefits of having smart lights in your household:

  • User Convenience

    Smart lights are a game-changer in any modern home. And when you consider their limitless potential, especially in terms of the convenience it adds to the household, it is undoubtedly one of the finest electrical products of present times. Operating a light switch is not complicated, but to be able to control the lighting system of your house with just a simple gesture of the hand does take things to a greater level altogether! In addition to the amazingly convenient hand gestures to control your lighting system, smart lights can also be effectively operated using your smartphone, and even virtual assistants like Alexa, Google Assistant, or Siri. To make things even better, smart lights can be conveniently connected to home automation systems for remote access, with extensive features like ambient lighting, group control, and more. With group control, you can easily toggle between operating your smart lights individually, as well as collectively as a unit.

  • Wide Colour Palette

    One of the biggest advantages to buying smart lights for your home is the wide colour palette they appear in, serving as ambient and accent lighting as well. With a wide range of colour setups to choose from, smart lighting can add a new dimension to your household, creating a sense of depth and wonder like never before. Smart lights are designed with colour-changing LEDs, which can be programmed to set the ambience with a colourful palette to choose from.

    In addition to adding a touch of colour and excitement to your household, colour-changing smart lights also have more subtle advantages that give them the edge. These smart lights can be programmed to switch between a warmer and a cooler colour setup depending on the weather and the time of day, which can have a profound influence on your mind. Whatever the weather outside might be, smart lights ensure you are coming back to a warm, welcoming home at the end of the day. In recent years, smart lights have grown amazingly popular among modern homeowners because of their ability to change colours and their intensity on command.

  • Setting Schedules

    Since smart lights can be connected to a home automation module, they can also be personalized to set up routines and schedules directly from your smartphone. You can also program the smart lighting in your house to respond on the basis of the time of day, such as switching on lights at sunset, and turning them off when the sun rises. Using an intuitive home automation system can also help you automate such functions without having to manually operate them.

    Smart lights are also beneficial in setting schedules. You can automate the smart lighting system to alter the intensity of light at specified hours, such as putting on dimmer lights after midnight, and more without having to manually alter them every time. Synchronizing your smart lights with your everyday schedule also allows lights to automatically turn off when you are not at home, and help conserve energy.

  • Energy Conservation

    There has been an increasing need for energy conservation in recent years, and with most industries switching to greener, eco-friendly modes of operating, the growing popularity of smart lights is another step towards a sustainable future. Taking the shift from normal lights to smart lights can also be a wise choice given the fact that traditional incandescent light systems require a higher energy input to operate. Smart lighting system which mostly uses LED lamps is considered environmentally friendly and secure, with improved power conservation and low energy requirements. Since LEDs can further cut down unnecessary energy usage, smart lighting systems are helpful in minimizing any wastage of energy.

    In addition to consuming significantly less electricity, smart lamps can be efficiently controlled through the home automation system, which can schedule lighting modes, and automatically turn off lighting systems when not required. This also contributes to improved energy conservation, which is reflected in the reduction in your monthly energy consumption.

  • Easy Installation and Maintenance

    In addition to the amazing conveniences and reduced power consumption of smart lights, they are also exceptionally easy to install and maintain. Since smart lights do not require complex wiring, they can be seamlessly installed in any household without the need for additional expenditures on renovation and rewiring. The ergonomic design of smart lights also makes them significantly durable against physical damage, and last longer. Smart lights are also available as decorative units like ceiling pendants, which can contribute to the general aesthetics of your house, enhancing its elegance.

  • Easy Synchronization

    Smart lights are extremely popular among modern homeowners given their amazing ability to adapt and synchronize to their environment. Not only can advanced models of smart lights change the colour and warmth of the light on command, but they can also offer added functionalities such as seamlessly synchronizing with the television or audio system. Smart lights can track the video signal of the television screen to mimic the atmosphere, allowing you to associate with the dominant colours on the screen and provide you with a uniquely immersive experience. You can also pair your smart lights with music applications like Spotify for an added bonus to your musical experience.

  • Added Security

    The latest smart lights models come with a dedicated away mode and motion triggers that can be remotely operated while you are away from home. The away mode is a clever addition to make your home secure, as it randomly switches the lights in your home on, keeping any unwelcome guests away. When paired with the home automation system, these smart lights can also send out automated alerts to keep you updated on the security of your house.

Read Also: Eco-Friendly Lighting: Everything You Need to Know