How to Choose Modular Switches for Your Home - Buying Guide

Electrical switches are an important aspect of your environment. Regardless of how tiny or large your place is, switches are required everywhere. In today's world, modular electrical switches not only alleviate the problem of turning on/off electrical equipment, but they also improve the appearance of your space. As a result, it is critical to grasp the fundamentals before making the appropriate move.

Modular switches function similarly to standard electrical switches, but with enhanced appearance. Each switch/socket in a non-modular switch is kept in place by a pair of screws. These screws detract from the appearance of the switchboard/wall since their color and form never match the rest of the board. Modular switches are held in place by sturdy plastic latches. Modular switches are now favored over traditional non-modular switches.

They are common in both residential and business locations. They are often more costly than non-modular switches, but they are well worth the cost. They are an essential component of interior design and may significantly alter their look. Conventional non-modular switches are no longer fashionable, thanks to the new variety of modular switches. Previously, you had to take care of the screws that came with the switches.

Modular switches have rapidly acquired popularity for obvious reasons:

Why should you install modular switches in your homes?

1. Elegance

Modular switches are undeniably attractive and stylish. These switches are available in a variety of patterns, forms, textures, and colors to complement the newly renovated interiors of your home or apartment.

Modular switches, as opposed to ordinary switches, exist in a variety of colors, finishes, and styles. Because of their adaptability, you may experiment with various options such as designer switch plates, glass switch plates, color-darkened switch plates, and more.

2. Safety

This is one of the primary reasons for the success of modular switches. The most important consideration while utilizing any technological equipment is safety. Traditional switches contained exposed metal screws that might cause a malfunction or a shock.

Because modular switches have no metal components on their sides, there is no risk of electric shock. If you have children, installing modular switches is a smart option since they are constructed of high-quality plastic and have no metal pieces on the front.

Also Read: Know Everything About Modular Switch Box

3. Versatile and Multi-Functional

Modular switches are distinguished by their adaptability. These switches may be used for automation, communication, safety, and data transmission. Various kinds of switches for various technologies may be put in various places of the building.

Because modular switches are available in a variety of capacities, they may also be employed for specialized applications. These switches are very versatile since they may be swiftly connected to or disengaged from switch plates to satisfy a variety of requirements.

4. Efficient and Ergonomic

Modular switches are quite economical. Companies that manufacture such high-end switches often subject them to thorough testing to assure their lifetime. Their inside wiring is energy efficient, allowing them to be utilized year after year.

The new modular switches have also been ergonomically designed to give a gentle touch and silent service.

With all of the advantages in mind, modular switches are the ideal choice. These switches include hidden bolts, anti-weld design, efficient operation, shuttered ports, and other enticing characteristics. Modular switches are also easy to install, activate, and utilize. Furthermore, unlike ordinary switches, these switches have serious safety concerns.

Do’s and don'ts for modular switches when renovating your own house?

Because of its aesthetic advantages over traditional switches, modular switches have dominated the electrical switch industry. They increase the value of any property.

We realize how important the electrical component of your house is to you, so we've included a few recommendations to assist you discover the best modular electrical switches.

Do's for modular switches when renovating your own house

1. Heat-Resistant Materials

One of the key considerations while searching for a functional switch device is the safety of the living area. Electrical circuits are often prone to overcurrent and arc flashes, which may result in a fire. So the goal is to limit the damage, and the first step is to purchase flame retardant (FR) grade materials that resist fire spread.

FR-grade polycarbonate, a thermoplastic used for switches and cover plates, is one of the most used materials. For a more exquisite appearance, you may also use specialist glass.

Also Read: Best Value Modular Switches from Schneider Electric Online

2. Broad Customization Options

The goal of looking for modular switches is to establish a harmonious balance between the electrical switches and the furnishings of your area. Design sensibility adds a refined visual sense to every living area.

When the switches and their various components are designed to conceal screw holes and have varied finishes that match in with the surrounding walls, the whole design seems high-end. To complement your décor, opt for matte, glossy, wood, or metallic finishes.

3. Broad Technological Options

Switches operate using a variety of technologies. Because of its adaptability, two-way switches are common in today's world. They let users to turn on lights from numerous locations in a living area. These are especially useful in big commercial environments where numerous persons may need to manage a single device from a distance.

4. Adaptable Pin-Type Sockets

One of the most serious concerns with the use of switches and socket boards is that overseas visitors' gadgets are often incompatible with local pin types. As a result, it is important to note that your building's switchboards and sockets should be adaptable to multiple pin types to facilitate utilization. When you can afford it, don't skimp on presenting various alternatives.

5. Clean and Durable Design

Because to their orthogonal design, conventional switches can seem filthy. Curved mounting plates are used in some modular switch designs to prevent dust from gathering between the wall and the plate. Some of these modular switches and plugs are also UV-resistant, reducing discoloration caused by UV light rays.

6. Child Safety

Modular switches have a more compact design, which avoids dangerous situations from emerging in the living environment while children are present. Look for shuttered sockets and fastening plates with arc flash protection. Look for microbe-resistant surfaces that cleanse with ions.

7. Maintenance & Repair

It is critical to discover modular switches that can be easily removed. When faceplates must be removed, the surrounding paint and wall might be damaged, so search for a modular switch series with a front-loading mechanism that permits fast disconnection of a broken switch or socket.

Many modular switch manufacturers provide a variety of switch ranges and series to accommodate the many design possibilities in residential and commercial environments.

Don'ts for modular switches when renovating your own house

When you are planning to renovate your house, there are a lot of things that you need to consider. From the budget to the timeline, every decision you make will have an impact on the outcome of the renovation.

One of the most important decisions you will make is choosing the right modular switches. With so many options on the market, it can be difficult to know which ones are right for your home.

Here are five things that you should NOT consider when choosing modular switches for your home renovation:

1. The price

While it is important to stay within your budget, you should not choose your switches based solely on price. There are a lot of factors that go into determining the quality of a switch, and the price is only one of them.

2. The brand

There are a lot of different brands of modular switches on the market, and they all have their own strengths and weaknesses. Instead of focusing on the brand, focus on finding the right switch for your needs.

Also Read: 5 Tips for Selecting The Best Electrical Switches And Sockets

3. The style

There are a lot of different styles of modular switches, and it can be tempting to choose the one that looks the best. However, the style of the switch should be the last thing you consider. The most important thing is that the switch is functional and safe.

4. The reviews

While it is important to do your research, you should not base your decision entirely on online reviews. Everyone has different needs, and what works for one person may not work for another.

5. Your gut feeling

It is important to trust your instincts, but you should not make your decision based solely on your gut feeling. There is a lot of information to consider when choosing modular switches, and you should take the time to weigh all of your options before making a decision.

Wrapping It Up

If you are planning a smart home renovation, you may be considering updating your old light switches to new, modern modular switches. There are many benefits to choosing modular switches over traditional switches, including safety, durability, and cost savings.

When choosing modular switches for your home renovation, be sure to select a product that is compatible with the circuit where it will be installed. You can determine the type of switch you need by removing the old switch and inspecting the wires connected to it.

Proper installation is important for the safety of your family and the longevity of your new switches. Be sure to follow the manufacturer's instructions and consult a professional electrician if needed. With proper installation and care, your modular switches will provide years of safe, reliable service.