Electrical Isolator- Types, Working & Its Applications

An electrical isolator is an essential switching device used to disconnect a part of an electrical circuit for safety, maintenance, or fault isolation. It plays a critical role in power distribution systems by ensuring that equipment and personnel remain safe during inspection or repair work.
Table of Contents
- What Is an Electrical Isolator?
- Function of an Electrical Isolator
- Types of Electrical Isolators
- Working Principle of an Electrical Isolator
- Uses of Electrical Isolators
- Applications of Electrical Isolators
- Advantages of Using Isolator Switches
- Electrical Isolator Symbol
- Maintenance Tips For Isolators
- In Conclusion
- Frequently Asked Questions
This article explains what an electrical isolator is, how it works, its types, applications, advantages, and maintenance tips.
What Is an Electrical Isolator?
In simple words, an electrical isolator is a kind of mechanical switch that isolates a part of a particular circuit when required. Typically, these switching devices are utilized to open a circuit in no-load condition and not when the current is flowing through the circuit. In a circuit, electrical isolators are placed at both ends of a circuit breaker to make it safe and easier to repair the breaker. These switches never work in full-load conditions.
With brief information about what an isolator is, move on to the following section of this blog that will introduce you to the working mechanism of electrical isolators.
Function of an Electrical Isolator
The main function of an isolator is to separate a circuit from its power supply. It ensures the safety of workers and prevents electric shock during maintenance. Isolators are not meant for switching loads, but work as safety devices to isolate parts of electrical systems when switched off.
Disconnect Power Safely
An isolator is used to safely cut off the power supply in a circuit. This helps during maintenance or inspection. The function of an isolator is not to interrupt load current but to disconnect once power is off.
Prevent Unwanted Currents
By creating a visible air gap, isolators ensure no current leaks into equipment. It is crucial in preventing electrical fires or faults. The air break design makes the system secure during shutdown.
Assist During Faults
In case of a short circuit or overload, isolators allow part of the network to be separated. This helps technicians locate faults quickly. Once the fault is fixed, the system can be restored section by section.
Enable Safe Repairs
When equipment needs to be checked or replaced, isolators make sure there is no live current. It helps engineers work without the risk of electric shock. It’s an essential part of routine repair systems.
Improve Network Control
Operators can isolate sections to manage loads better during high-demand periods. This helps prevent overload in grids. Using isolators this way supports better power distribution planning.
Types of Electrical Isolators
Electrical isolators are classified based on construction and installation location.
Types Based on Construction
Double Break Type Isolators
The Double break type isolators have three loads of post insulators. Among these three, the middle insulator has a tubular contact or flat male that is turned straight through spinning the middle post insulator. At the bottom of the post insulator, a lever method is used for the middle post insulator’s rotation.
Single Break Type Isolators
Another type of isolator is the Single break type, which has its arm contact broken into two components. One of these arm contacts is responsible for holding the male contact, and the other one for holding the female contact. A shift is observed in the arm contact due to the rotation of the post-insulator upon which they are fixed. This rotation of the post-insulator is reversed to each other, resulting in shutting the isolator by the arm contact. The counter rotation opens the isolator as well as the arm contact. In cases of emergency, these isolators can also be operated manually.
Pantograph Type Isolators
Pantograph isolators require less horizontal space and are mainly used in high-voltage switchyards. Their vertical movement allows efficient operation in compact substations.
Types Based on Power System Location
Bus Side Isolator
Bus-side isolators are linked directly to the main bus system. They are placed between the bus and the incoming or outgoing feeder. Their role is to disconnect the bus during maintenance without touching the full circuit. This is one of the key electrical isolator types used in medium to high voltage systems.
Line Side Isolator
Line-side isolators stay connected through the feeder line. These help isolate the line during maintenance or faults without disturbing the whole bus. They often act as an interface between substation equipment and external transmission. The isolator's working principle is clearly visible in this configuration.
Transfer Bus Side Isolator
Transfer bus side isolators are placed between the transfer bus and the main circuit. These isolators allow power to be rerouted when the main bus is under repair. This setup helps in reducing downtime. They are critical in large substations where backup is always needed for the smooth functioning of the electrical isolator.
Working Principle of an Electrical Isolator
The working principle of an electrical isolator is based on physical disconnection of conductive parts to stop current flow completely.
Isolators are operated only after the circuit breaker opens, ensuring zero current during operation.
Modes of Operation
Manual Operation of Isolator
Manual isolators are operated by hand and are often used during maintenance. They are installed in locations where automatic systems are not needed. Operators physically open or close the isolator to stop or allow the current. These are reliable when human control is preferred over automation. Such devices explain well how an isolator works in older or simpler systems.
Semi-Automatic Operation
Semi-automatic isolators mix both manual and motorised functions. The control panel can operate them with minimum effort. However, in case of a power failure, these isolators can be handled manually. Their design ensures safety while allowing faster operations during emergencies. The function of the isolator becomes more visible in this flexible operation mode.
Fully Automatic Operation
Fully automatic isolators are common in large substations and grid systems. These work based on control commands or sensors. They don’t need human interaction and respond fast to load changes or faults. They make the electrical isolator symbol come alive in modern smart systems.
Fixed Position in Circuits
Isolators are fixed in one location in the circuit. They do not move or shift once installed. Their job is to isolate parts like transformers or feeders when required. These are not like mobile switches but rather form a stable point of disconnection. This makes them essential in every isolator in an electrical circuit setup.
Safety Features
• Visible air gap for confirmation
• Mechanical interlocking with circuit breakers
• Earthing switch to discharge trapped electrical charges
Uses of Electrical Isolators
Isolators are commonly used in electrical systems to disconnect a part of the circuit when needed. They are used during maintenance or repairs to cut off power flow and reduce risks. These switches are also seen in substations and power grids to keep equipment safe from overload or faults.
In Power Plants
Isolators are used in power plants to disconnect specific sections during inspections or fault conditions. It ensures safety when workers perform maintenance. Since the isolator in the electrical circuit is manually operated, the system stays secure when turned off.
In Substations
Substations make use of isolators to disconnect transformers or feeders when they need to be serviced. This helps reduce downtime and prevents accidental energization of equipment. Workers rely on it to work safely without power running through the system.
In Industrial Units
Heavy industries depend on isolators to cut off power to machines during an emergency. It prevents electrical shocks and damage to machinery. Isolators installed in control panels also reduce the risk of accidents.
In Residential Wiring
Homes with rooftop solar or generator systems use isolators to stop backfeeding into the main grid. It’s a vital part of safety for electricians and maintenance crews during service. It avoids energy flowing into inactive circuits.
In Railway Systems
Electric trains and tracks often use isolators to control sections of live wires. When needed, a section can be disconnected while keeping the rest of the system active. This keeps services running without a full shutdown.
Applications of Electrical Isolators
• Power Plants: Used to isolate generators, transformers, and feeders during inspection or faults.
• Substations: Essential for disconnecting transformers, busbars, and transmission lines safely.
• Industrial Units: Installed in control panels and machinery to ensure safe shutdown during repairs.
• Residential Systems: Used in solar installations and generator connections to prevent reverse power flow.
• Railway Systems: Help isolate sections of overhead lines while keeping other parts operational.
Advantages of Using Isolator Switches
Isolator switches improve safety by clearly separating the circuit during shutdown. They help avoid accidents, especially during repair work. Another benefit is their low maintenance. They are easy to operate and provide a reliable way to cut power without complex systems, making them a practical choice for electrical setups.
Safety from Electric Shock
One of the biggest advantages is safety. Isolator switches ensure no electrical energy remains during service. So, engineers can handle lines and equipment with peace of mind.
Clear Isolation
Unlike circuit breakers, isolators show a clear disconnection with open contacts. This gives visual assurance to operators. Such confirmation is especially important during emergency disconnection.
Simple Construction
Isolators have fewer parts and a simpler design compared to other switching devices. This makes maintenance easy. The electrical isolator types vary in build, but most share a basic framework.
Cost-effective Solution
Since isolators are not meant to handle current breaking, their build cost is low. This makes them a suitable addition in all medium and high voltage networks. Also, it cuts maintenance expenses.
Useful During Routine Maintenance
It becomes easy to service machines without disconnecting the entire system. Using isolators this way avoids a full blackout. It keeps some systems alive while repairs continue.
Electrical Isolator Symbol
The electrical isolator symbol is a simple straight line with a small break or gap in the middle, indicating disconnection. It’s widely used in electrical drawings to mark a point of safe isolation. This symbol helps electricians identify isolators in circuit diagrams easily.
Maintenance Tips For Isolators
Being a mechanical device, faults are natural to occur in electrical isolators. However, if they receive proper maintenance, these faults can be minimized. Below are some maintenance tips that must be followed to ensure their smooth operation.
• Electrical isolators must be kept clean. They must be clean from salt cement and acid fumes.
• Isolators must be replaced with new ones as soon as a defect is observed to prevent the entire circuit.
• The arrangement of contact rods should always be appropriate.
• The connections of isolators must be tight, and regular inspection must be done to ensure these connections are in place.
• Once the isolator is closed, the earth switch must be closed to check the mechanical interlock of the isolators.
Several other maintenance steps must be taken to ensure appropriate maintenance for the electrical isolators. However, one key point to remember here is that safety measures must be followed when maintaining isolators, and if you do not know much about them, always rely on a professional to help you with the maintenance.
Read Also - Difference between Circuit Breaker and Isolator / Disconnector
In Conclusion
Isolators are widely used to separate a faulty section of an electrical circuit from a healthy one to prevent further damage and efficient repair. These switching devices play a crucial role in the overall operation of a circuit. As a result, it is essential to ensure they are of premium quality. If you are looking to buy any type of electrical isolator, the online store of Schneider Electric India is just the place for you.
Frequently Asked Questions
Q1. Where are electrical isolators commonly used?
Ans. Electrical isolators are used in power plants, substations, transformers, and household equipment. In kitchens, they are part of heavy appliances like ovens. In industrial settings, they protect machines during servicing. You can spot them where power isolation is a regular need. They are a core part of the uses of isolators in daily life.
Q2. Is an isolator the same as a circuit breaker?
Ans. No, they are not the same. A circuit breaker can open under load, interrupting current flow safely. An isolator cannot interrupt load current and is used only when the current is already zero. The function of the isolator is focused more on safe disconnection than fault handling.
Q3. Why is an isolator installed on both sides of a circuit breaker?
Ans. It is to ensure complete isolation of the circuit breaker during servicing. Isolators on both ends cut off the supply from both sides. This ensures safe maintenance and avoids backfeeding. It's a basic practice in every isolator in electrical circuit layout.
Q4. What safety precautions should be taken when operating an isolator?
Ans. Always turn off the load before using an isolator. Use gloves, wear safety gear, and ensure there's no current flow. Operators should follow lockout-tagout steps and inspect visually. The isolator's working principle depends on safe handling during operation.
Q5. What is the voltage rating of a typical electrical isolator?
Ans. Voltage ratings vary from 11 kV to 765 kV, depending on application. Smaller ones in homes may range from 240V to 415V. The electrical isolator symbol can be found in manuals with such technical ratings mentioned clearly.
Q6. What is a fused isolator?
Ans. A fused isolator combines a fuse and an isolator in one unit. It cuts off both current and provides protection against overcurrent. This setup prevents faults and keeps connected devices safe. It is often used in domestic areas for better function of the isolator and fault response.
Q7. How is an isolator different from an MCB?
Ans. An isolator is a disconnector used during maintenance. An MCB (Miniature Circuit Breaker) trips on overload or short circuit automatically. Isolators lack sensing elements. They are manually operated. That makes the electrical isolator types different from standard breakers and protective devices.
Q8. What is the typical lifespan of an isolator switch?
Ans. A typical isolator switch lasts around 15–25 years based on usage and environment. Regular maintenance helps. Dust, heat, or humidity can reduce life. In protected indoor panels, life goes longer. The how isolator works part does not change, but its quality might drop with time.
Comments