Wireless auxiliary contact NSX

LV429454
Be the first one to review this.

Excl. Tax

login_green To View the best prices please Sign in / Register.
loader
Loading...

Description

This is a wireless auxiliary contact that provides remote indications of the circuit breaker status. It is used on ComPacT NSX 100 to 630 and ComPacT NS 630 to 3200 new generations. This wireless auxiliary contact provides OF information (ON/OFF), that indicates the position of the circuit breaker power contacts. It provides SD information (trip indication), that indicates that the circuit breaker as tripped due to an electrical fault, operation of a voltage release or push to trip button. It provides SDE information (fault trip indication), that indicates that the circuit breaker as tripped due to an electrical fault (overload, short-circuit, ground fault, earth fault). This wireless auxiliary contact works with Zigbee wireless communication protocol (IEEE 802.15.4) within the frequency range 2405-2480MHz . It is a plug & play technology for clear connection status. This wireless auxiliary contact is placed in the same position as the wired version. A LED light is integrated and gives an indication in case of tripping. Communication architecture is fully EcoStruxure Power validated, with any application.

Product Details

Product Name Wireless auxiliary contact NSX
Range Name ComPact NSX
Tax Class GST-18

No Related Posts

Seller Information

Documents

Extended Warranty

Reviews

Write Your Own Review
Only registered users can write reviews. Please Sign in or create an account