PLC Controllers

120 results

Sort By arrow-down
Module TM3 - 4 AI 2 AO
TM3AM6
Price starting from
₹ 45,308.00
₹ 28,090.96
Ethernet TM3 Bus Coupler Module
TM3BCEIP
Price starting from
₹ 26,920.00
₹ 16,690.40
MODULE TM3-24 IO RELAYS
TM3DM24R
Price starting from
₹ 30,762.00
₹ 19,072.44
MODULE TM3-16 OUT RELAYS SPRING
TM3DQ16RG
Price starting from
₹ 25,153.00
₹ 15,594.86
MODULE TM3-8 OUT RELAYS SPRING
TM3DQ8RG
Price starting from
₹ 18,059.00
₹ 11,196.58
MODULE TM3-4 INPUTS TEMPERATURE
TM3TI4
Price starting from
₹ 43,680.00
₹ 27,081.60
MODULE TM3-24 IO RELAYS SPRING
TM3DM24RG
Price starting from
₹ 32,583.00
₹ 20,201.46
MODULE TM3-BUS RECEIVER
TM3XREC1
Price starting from
₹ 34,386.00
₹ 21,319.32
MODULE TM3-BUS TRANSMITTER
TM3XTRA1
Price starting from
₹ 23,775.00
₹ 14,740.50
MODULE TM3-16 INPUTS
TM3DI16
Price starting from
₹ 22,726.00
₹ 14,090.12
MODULE TM3-8 OUT RELAYS
TM3DQ8R
Price starting from
₹ 18,073.00
₹ 11,205.26
MODULE TM3-8 INPUTS
TM3DI8
Price starting from
₹ 14,896.00
₹ 9,235.52

Buy PLC and PAC Controllers

A PLC (Programmable Logic Controller) and a PAC (Programmable Automation Controller) are both industrial control systems used to automate machinery and processes. PLCs are typically used for discrete control applications, while PACs offer more advanced capabilities and are suitable for both discrete and process control applications. PACs often feature greater processing power, more memory, and built-in support for communication protocols, making them versatile solutions for complex automation tasks. PLCs are well-suited for discrete control tasks and PACs offer greater versatility, performance, and flexibility, making them ideal for a wide range of industrial automation applications. The choice between PLCs and PACs depends on factors such as the complexity of the application, integration requirements, and scalability needs. Both of them are types of industrial control systems used to automate machinery and processes in manufacturing, infrastructure, and other industries.

PLC (Programmable Logic Controller):

PAC (Programmable Automation Controller):

FAQ:

Are PAC better than PLC?

Whether PACs are better than PLCs depends on the specific requirements of the application. PACs offer more advanced capabilities and flexibility, making them suitable for complex automation tasks and integrating with other systems. However, PLCs are often more cost-effective and simpler to implement for smaller-scale applications. The choice between PACs and PLCs ultimately depends on factors such as functionality, scalability, and budget.

How much does a PLC system cost?

The cost of a PLC system can vary widely depending on factors such as the brand, model, features, and complexity of the application. Basic PLC systems for small-scale applications can start at a few hundred dollars, while more advanced systems for large-scale industrial automation projects can cost several thousand dollars or more. Additionally, costs may include expenses for software, programming, installation, and maintenance, so it's essential to consider the overall investment when budgeting for a PLC system.

Which PLC is most used?

The most used PLCs vary depending on industry and application requirements. Schneider Electric and various other manufacturers offer a range of PLC models with different features, performance levels, and capabilities to meet the diverse needs of industrial automation applications. The choice of the most suitable PLC depends on factors such as functionality, reliability, and support.