Product availability may vary based on your location.
Control stations are devices used in industrial and commercial settings in lieu to control machinery, equipment and processes. They typically consist of push buttons, switches, indicator lights, and other control elements mounted on a panel or enclosure. Control stations allow operators to start, stop, and monitor machinery, as well as control various functions and operations within a facility. You can buy a control station, push button station, pendant station and local control switch from our eShop.
Push button control stations are essential components in industrial and commercial settings, providing operators with a convenient and intuitive interface to control machinery and processes. Know all about them in the points stated below.
A push button control station is a device used in industrial and commercial settings to control machinery, equipment, and processes. It typically consists of push buttons, selector switches, indicator lights, emergency stop buttons, and other control elements mounted on a panel or enclosure. Operators use push button control stations to start, stop, and monitor machinery, as well as control various functions and operations within a facility.
No, a push button is not a sensor. A push button is a manually operated mechanical switch that requires physical actuation by pressing it with a finger or object. It does not detect or respond to changes in its environment like a sensor does. Instead, a push button initiates a specific action or control function when pressed, such as starting or stopping machinery, activating a device, or signaling an event.
Various advantages of push buttons are: