AUTOMATION RELAY

An automation relay, also known as a control relay, is an electromechanical device used in automated control systems to switch electrical circuits on or off based on predetermined conditions. Automation relays can be used in various applications, such as industrial machinery, HVAC systems, and home automation, to control motors, lights, valves, and other devices. Relays in home automation are used to control various electrical devices and systems, such as lights, fans, heating systems, and security systems. They enable remote or automated operation by switching these devices on or off based on user inputs, preset schedules, or sensor readings.

Automation Relay

Showing 151-171 out of 171 products

Set Descending Direction
  1. SIMPLE SOCKET 22,5MM / MIXED TERMINATION
    In stock
    Rating:
    100%
    Regular Price ₹ 214 Special Price ₹ 131

Automation Relay

Showing 151-171 out of 171 products

Set Descending Direction
Page

The components of an automation relay typically include:

When an electrical current passes through the coil, it generates a magnetic field that attracts or repels the contacts, causing them to open or close. This action controls the flow of electricity in the circuit connected to the relay.

The various benefits of using an automation relay include:

FAQs