Home UPS

1 Item

arrow-down
1 Year Renewal Extended Warranty for (1) Smart-UPS 20K
WEXT1YR-SU-08

Explore Premium Schneider Electric Home UPS & Inverters

Schneider Electric eShop offers home UPS and inverter solutions designed for residential and small-office power backup.

Reliable Power Backup

A home UPS supplies backup power when the main electricity supply is interrupted. This helps keep essential devices operational during short outages and power interruptions. 

UPS and Inverter Functionality

UPS and inverter systems convert stored battery energy into usable electrical power for connected equipment. Depending on the design, they can provide backup during outages and support the operation of selected household appliances. 

Residential Power Requirements

Homes have different backup requirements depending on the appliances and electronics being used. A system supporting a router and computer will have different requirements from one powering several household appliances. 

Small-Office Applications

A home UPS can also support small-office equipment such as computers, monitors, routers and networking devices. Reliable backup can help reduce interruptions during work and protect ongoing tasks from sudden power loss. 

Key Features of Schneider Electric Home UPS & Inverters

A home UPS combines backup power with features designed for convenient residential use. Important specifications include output capacity, battery configuration, backup duration, protection functions and compatibility with connected equipment. 

Backup Capacity

UPS capacity determines the amount of electrical load that can be supported. It should be selected according to the combined power requirements of the appliances and electronics that need backup. 

Battery Performance

The battery stores energy that is used when the main power supply fails. Backup duration depends on battery capacity, connected load, battery condition and operating conditions. 

Surge Protection

Certain UPS systems provide protection against power disturbances such as voltage fluctuations and surges. This can be useful for sensitive electronics including computers, networking equipment and entertainment devices.

Automatic Power Switching

A UPS can automatically transfer connected equipment to battery backup when the main power supply fails. This reduces the need for manual intervention during an outage.

Why Choose Schneider Electric Home UPS for Your Home?

A suitable home UPS can provide dependable backup power for essential electronics and help reduce disruption during outages. Schneider Electric eShop solutions can be selected according to household and small-office requirements.

Uninterrupted Backup

A home UPS provides temporary power when the main electricity supply is unavailable. This is useful for devices that should remain operational during short interruptions, including routers, computers and other essential electronics. 

Protection for Electronics

Power disturbances can affect sensitive electronic equipment. Depending on the model, a UPS may provide protection against certain voltage fluctuations and surges. 

Convenient Operation

Automatic switching allows the UPS to respond to power interruptions without requiring users to manually start backup operation. This makes the system practical for everyday residential use. 

Flexible Usage

Home UPS systems can support different combinations of electrical equipment depending on their capacity. A user may prioritise computers and networking devices, while another may require backup for selected household electronics.

Applications of Home UPS in Residential & Small Office Settings

Home UPS systems are useful wherever power interruptions can disrupt daily activities or work. They can provide backup for computers, routers, monitors, televisions and other compatible electronics. 

Work-from-Home Setups

A home UPS can support computers, monitors and networking equipment used for remote work. Backup power helps reduce disruption during outages and allows users to continue essential tasks. 

Computers and Networking

Computers and networking devices can benefit from backup power because sudden outages may interrupt active work or internet connectivity. A suitable UPS can keep these devices operating temporarily. 

Home Entertainment

Televisions, streaming devices and other entertainment electronics can be connected to suitable UPS systems when their power requirements fall within the rated capacity. Backup power can prevent sudden shutdowns during interruptions.

Essential Household Electronics

Selected household electronics may require backup during short power interruptions. The suitable load depends on the UPS output capacity and appliance requirements. 

How to Choose the Right Home UPS or Inverter

Choosing a home UPS requires assessment of the equipment that needs backup, total power consumption and desired runtime. Users should compare output capacity, battery specifications, protection features and installation requirements. 

Calculate Connected Load

Start by identifying the appliances and electronics that require backup and determine their combined power consumption. The UPS should have sufficient capacity to support the expected load. 

Determine Backup Time

Required backup duration depends on how long users need connected equipment to remain operational during an outage. A system intended for short interruptions may require less battery capacity than one designed for longer backup periods. 

Check Appliance Compatibility

Not every appliance is suitable for every UPS. Users should check power requirements, starting loads and the UPS output characteristics before connection. 

Compare UPS Specifications

When comparing home UPS cost, users should also evaluate capacity, battery performance, protection features and warranty or service provisions. Looking only at purchase price can result in selecting an unsuitable system. 

Benefits of Installing a Home UPS

Installing a home UPS can provide backup power for essential electronics and reduce interruptions caused by outages. It can also support convenient automatic switching and, depending on the model, provide protection against certain electrical disturbances.

Power Continuity

A UPS keeps selected equipment running when the primary electricity supply fails. This is particularly useful for computers, routers and other devices where sudden shutdowns can interrupt work or connectivity.

Reduced Work Disruption

Power interruptions can cause unsaved work to be lost or disconnect networking equipment. Backup power gives users additional time to continue working or safely shut down equipment.

Equipment Protection

Some UPS systems provide protection against specific power disturbances. This can help reduce exposure of connected electronics to certain voltage-related events.

Greater Convenience

Automatic backup operation means users do not need to manually activate the system when electricity fails. Once correctly installed and configured, the UPS can switch connected equipment to battery operation.

Installation & Maintenance Tips for Home UPS

Correct installation and regular maintenance are important for safe and reliable UPS operation. The system should be installed according to manufacturer instructions, with appropriate ventilation and electrical connections.

Choose a Suitable Location

Place the UPS in a clean, dry and adequately ventilated area. Avoid locations exposed to excessive heat, moisture or restricted airflow.

Avoid Overloading

Connected equipment should remain within the UPS's rated output capacity. Overloading can affect performance and may cause the system to shut down or trigger protective functions.

Maintain the Battery

Battery condition directly affects backup performance. Follow the manufacturer's maintenance and replacement recommendations and monitor for signs of deterioration.

Follow Safety Procedures

UPS systems contain electrical components and batteries that require appropriate handling. Installation, electrical connections and servicing should follow the manufacturer's instructions and applicable safety requirements.

Home UPS Price List in India

Home UPS price in India varies according to capacity, battery configuration, backup requirements, features and application. A higher capacity can affect the overall home UPS cost, but price should not be the only selection factor.

Factors Affecting Home UPS Price

Home UPS price depends on factors such as output capacity, battery configuration, technology and protection features. Systems designed for higher loads or longer backup durations may have different costs.

Compare Capacity and Features

When evaluating price, compare output capacity, battery performance, protection functions and intended application. A lower-cost UPS may not provide adequate capacity for the required load.

Check Current Availability

Online pricing and product availability can change depending on the product configuration and supply conditions. Buyers should check the latest product information before ordering.

Best UPS for Home Office

The best UPS for a home office should provide sufficient capacity for the computer, monitor, router and other essential equipment. Users should consider total load, required runtime and output compatibility.

FAQs About Home UPS

Q. What is a home UPS?

A home UPS is a backup power system that supplies electricity to selected connected devices when the main power supply fails. It typically uses a battery to provide temporary power and may also offer protection against certain power disturbances, depending on the model.

Q. Which appliances can I run on a home UPS?

A home UPS can support compatible electronics such as computers, routers, monitors, televisions and other devices within its rated capacity. The connected load must remain within the UPS output specifications. High-power appliances should only be connected when specifically supported by the selected system.

Q. How much backup time does a home UPS provide?

Backup time depends on battery capacity, UPS efficiency and the total connected load. Lower loads generally allow longer runtime, while higher loads reduce available backup time. Check the product specifications and expected load to estimate whether the system provides sufficient backup for your requirements.

Q. What UPS capacity is suitable for a home?

Suitable UPS capacity depends on the appliances and electronics requiring backup and their combined power consumption. Users should calculate the expected load and select a system with sufficient output capacity. A suitable capacity margin can help prevent continuous operation at the maximum rated load.

Q. Can a home UPS protect my electronic devices from power fluctuations?

Some home UPS systems provide protection against certain voltage fluctuations, surges or other electrical disturbances. Protection features vary by model, so users should check the product specifications before purchase. A UPS should not be assumed to provide identical protection for every type of electrical disturbance.

Q. Can I use a home UPS for computers and networking devices?

Yes, a suitable home UPS can support computers, monitors, routers and networking equipment when their combined power requirements remain within the UPS rating. Backup power can help prevent sudden shutdowns and maintain connectivity during outages, making UPS systems useful for home-office and remote-working environments.

Q. How often should I maintain my home UPS?

Maintenance requirements vary by UPS model and battery type. Users should follow the manufacturer's recommended inspection and battery maintenance schedule. Monitoring backup performance, keeping ventilation clear and checking for signs of battery deterioration can help maintain reliable operation and identify issues early.

Q. Is a home UPS suitable for work-from-home setups?

Yes, a suitably sized home UPS can support work-from-home equipment such as computers, monitors and routers. It can provide temporary backup during outages and reduce disruption to work. The UPS should be selected according to the combined load and required backup duration of the setup.

Q. Where can I buy Schneider Electric Home UPS and Inverters online in India?

You can buy Schneider Electric Home UPS and Inverters online through Schneider Electric eShop in India. Before purchasing, check the output capacity, battery specifications, connected load requirements and other technical details to select a solution suitable for your home's or small office's backup requirements.



Best-Selling Schneider Electric India - Home UPS Price List (2026-2027)

Updated Date: 17 November, 2026

Top Popular Best-Selling Schneider Electric India - Home UPS Price List (2026-2027) Latest Price
1 Year Renewal Extended Warranty for (1) Smart-UPS 20K ₹ 0.00