Sensor case
Education test kit helps to learn assemble the Sensor case kit
Kit helps students to understand and learn various sensor technologies, detections principles, setup sensors & components, interconnections in Sensor case during installation
Training experiments that can be run on the kit
- Finding out about the various technologies used in industrial detection:
- Photoelectric detectors (barrier, reflex, fiber optics, background obliteration, etc.)
- Inductive and capacitive sensors for detection of various materials,
- Detection of rectilinear or angular movement via position switches.
- Implementing sensors.
- Making adjustments.
- Setting up a detection chain
Components of the kit:
Components |
Qty. |
Limit switch Plastic |
1 No. |
Limit switch metal end Plunger with elastomer boot 1 NO + 1 NC PG11 |
1 No. |
Limit switch plastic thermoplastic roller lever 1 NO + 1 NC PG-11 cable |
1 No. |
Limit switch thermoplastic roller lever plunger Horizontal action in 1direction 1 NO + 1 NC PG-11 cable |
1 No. |
Inductive sensor M18 sensing distances 8 mm 1 NO length 62 mm |
1 No. |
Inductive sensor M18 sensing distances 8 mm PNP length 62 mm |
1 No. |
Inductive sensor M18 sensing distances 8 mm |
1 No. |
Capacitive Proximity sensor M18 sensing distances 5 mm |
1 No. |
Photo Electric sensor sensing distance 30 m thru beam need a transmitter |
1 No. |
Photo Electric sensor sensing distance 30 m thru beam need a transmitter |
1 No. |
Photo electric sensor nominal sensing distances 1 m defuse |
1 No. |
Photo electric fiber amplifier |
1 No. |
Plastic fiber optic for sensor 3 m long |
1 No. |
Fiber optic Amplifier |
1 No. |
Product Name | Sensor case |
---|---|
Tax Class | GST-18 |
* Required Field