closed toroid A type, for Vigirex and Vigilhom, GA300

50442
Be the first one to review this.

Excl. Tax

login_green To View the best prices please Sign in / Register.
loader
Loading...

Description

This toroid is dedicated to Vigilohm Insulation Fault locators, and to VigiPacT type A residual current protection and monitoring relays. It allows the monitoring of the injected component from Vigilohm Insulation Monitor, and the measurement of a current rating up to 630A for VigiPacT monitoring and protection relays. The transformer ratio is 1/1000. The inner diameter of the toroid is 300mm and the weight is 2.280kg. The cables must be centered within the toroid and the diameter represented by all these cables should not exceed 150 millimetres. The maximum cross section per phase (R, S, T, N) is 2 cables of 240mm² for a copper conductor.

Product Details

Product Name closed toroid A type, for Vigirex and Vigilhom, GA300
Range Name VigiPacT
Tax Class GST-18

No Related Posts

Seller Information

Documents

Extended Warranty

Reviews

Write Your Own Review
Only registered users can write reviews. Please Sign in or create an account