Which Type of Power Backup Is Best for You? Servo UPS vs Stabilizer

An uninterrupted power supply is a basic need for everyone. Be it in-house or business, we require an ample amount of power supply to keep the operations running. If the power faces obstacles, it can hinder our work and often damage various electronic devices. 

To get an uninterrupted supply of electricity and save our devices, there are two popular power backups: stabilizers and servo UPS. But which one is the best power backup? UPS vs stabilizers can be a prolonged debating topic, so compare the products and see which one works out for you. 

What is a Stabilizer?

Stabilizers are a type of power backup that regulates voltage fluctuations in the power supply. The stabilizer working principle includes providing a constant voltage output by acting as an insulation between the primary power supply and the connected devices. This device safeguards household appliances like televisions, refrigerators, and air conditioners against voltage surges, spikes, and sags. In factories and industries, stabilizers are used for furnaces, machinery, and other equipment. These provide quick voltage adjustments and may accommodate a wide variety of input voltages.

Read Also - GET ALL THE KNOWLEDGE ABOUT SCHNEIDER ELECTRIC'S STABILIZER

What are the Benefits of Using a Stabilizer?

Stabilizers offer multiple benefits, which are discussed in this section.

Cost-Effective

Voltage stabilizers are costly; it is a myth. Investing in one will save you from expenditures on prospective repair and repurchase charges for electrical gadgets. Without a stabilizer, your electronics are more vulnerable to voltage fluctuations. Since voltage stabilizers help maintain electric gadgets in excellent working order, they are a worthwhile purchase. 

Protects Electric Equipment from Damage

Electrical equipment has a safe working limit above or below which the entire operation can be affected. A continuous unusual voltage supply to an electric appliance destroys the insulation, resulting in low efficiency and performance. A voltage stabilizer safeguards the device against such risks.

Makes Appliances Long-lasting

If the appliances are in good condition, they can last longer. A voltage stabilizer prevents power surges from affecting electrical equipment. Individuals can get the most of them when they have a steady current flow, which is an important factor in determining the health and longevity of the electric appliance. 

Customizable

Stabilizers allow people to easily customize specifications. This device can adjust to different voltage requirements, capabilities, and sizes. For instance, an air conditioner's power needs differ from a refrigerator's. So, how to choose a stabilizer for an AC or finding the right stabilizer for a refrigerator would necessitate various product specifications. Thus, it may be readily manufactured for practical purposes. 

Read Also - SCHNEIDER ELECTRIC STABILIZERS: WHY AND WHERE DO YOU NEED THEM

What is a UPS?

Also known as an uninterrupted power supply, UPS is a device that serves as a power backup option. A UPS not only maintains the voltage but also acts as a source of power during outrages. This power backup option has a battery that is constantly charged, and the main power supply is operational. UPS working principle differs from that of a stabilizer. When the power source is turned off, the UPS operates as a backup power supply. This keeps linked gadgets from shutting off and ensures a constant power supply.

Benefits of using a UPS

The following are the benefits of using a UPS.

Constant Power Supply

UPS provides a constant power supply. UPS delivers power from its internal battery when the primary power supply fails. The uninterrupted power supply guarantees that the electrical appliances, such as servers, computers, and other vital equipment, continue to operate normally.

Business Continuity

Downtime can have a negative impact on corporate operations. This can lead to wasted income, damaged customer trust, and reduced productivity. A reliable UPS helps in corporate continuity during power outrages. Businesses with an uninterrupted power supply may continue to operate smoothly, provide continuous client service, and avoid any negative influence on their bottom line.

Restoration of Data

For both individuals and businesses, data loss can have serious ramifications. Suppose you’re running an online business or working on a project, and the power goes out. Your unsaved work and vital data will be lost permanently if you don’t have a UPS. However, with a dependable UPS, you can avoid such disasters. The UPS allows users to save work and safely shut down appliances, ensuring data safety from power outrages. 

Offers Peace of Mind 

A UPS provides peace of mind. Knowing you have a reliable power backup option reduces the worry and anxiety associated with power outrages. Whether it is an online gaming session, working on a critical business presentation, or simply surfing the internet, the UPS serves as a safety net, enabling you to focus on the work at hand without worrying about unexpected power outages.

Read Also - HOW TO PICK THE RIGHT UPS FOR YOUR DESKTOP COMPUTER

Comparison Between Stabilizers and UPS

The following table will provide a brief comparison between Stabilizers and UPS based on important factors. 

Factors

Stabilizers

UPS

Backup Capacity

Stabilizers only maintain the voltage fluctuations in the power supply.

UPS not only maintains voltage fluctuations but also provides power from its battery during power outrages. 

Cost

These devices are durable and very cost-effective.

Since UPS supplies power during outrages, they require batteries, which makes them costly. 

Maintenance

Stabilizers only need to be checked to see if the connections are okay, making the maintenance cost low. 

For optimal performance, UPS batteries need to be removed and replaced from time to time. Hence, the maintenance cost is higher. 

Application

Stabilizers safeguard residential and industrial equipment from damage caused by voltage fluctuations.

This power backup option is used for devices that require power during emergencies, such as medical equipment, computers, and servers. 

Final Thoughts

For varied reasons, both Stabilizers and UPS are great power backup options. To maintain voltage fluctuations, you may require a stabilizer to safeguard your home and industrial appliances. These are affordable and simple to maintain on a limited budget. However, UPS systems are used only during emergencies. Not only do they maintain voltage fluctuations, but they also provide power during outrages. It is important to evaluate your requirements while choosing a power backup option. 

Find Top-Notch UPS and Stabilizer Options at Schneider eShop

For a constant and stable power supply, Schneider eShop provides robust UPS inverters and stabilizers. This is an extremely useful power backup option used at homes that operate without an external frequency reference. Our UPS systems have protection mechanisms to safeguard computer systems and prevent damage caused by overvoltage, transients and power dips. Our stabilizers are also recommended by many satisfied customers. Designed to withstand Indian weather conditions, our voltage stabilizers are the perfect option to prevent voltage quality and surges. We offer stabilizers for various electrical appliances, including TVs, fridges, washing machines, ACs, electrical treadmills, and more. Visit our e-Shop and enjoy the convenience of free installation and delivery.