What is a Varactor Diode? Working, Characteristics and Applications

What is a Varactor Diode? Working, Characteristics and Applications

Summary

What is varactor diode technology, and why does every tunable radio circuit depend on it? This guide explains varactor diode working through the voltage-controlled depletion region, covers the main varactor diode characteristics such as capacitance ratio and quality factor, and reviews the varactor diode symbol used in circuit drawings. It also examines construction, doping profiles and typical applications in oscillators, filters and phase-locked loops. Capacitance values, voltage ranges and tuning ratios support each point.

Key Takeaways

  • Varactor diodes use reverse-biased semiconductor junctions to provide voltage-controlled capacitance for electronic tuning applications.
  • Increasing reverse voltage widens the depletion region, reducing capacitance and changing the resonant frequency of circuits.
  • Capacitance ratio, quality factor, leakage current, and breakdown voltage determine tuning range, signal quality, and operating limits.
  • Silicon varactors suit common radio-frequency circuits, while gallium arsenide devices support high-frequency microwave applications requiring lower resistance.
  • Varactor diode applications include voltage-controlled oscillators, phase-locked loops, tunable filters, frequency multipliers, and wireless receivers.
  • Proper selection requires evaluating capacitance range, doping profile, temperature stability, package parasitics, and reverse-voltage limits.

Introduction

Previously, adjusting a radio involved turning a knob that was connected to a large air-gap capacitor. Now, the same thing is achieved using a small semiconductor chip and a control voltage. This chip is known as the varactor diode, also referred to as a varicap or tuning diode. If anyone asks what is varactor diode, they will discover one fundamental idea: a junction that acts like a capacitor whose value can be altered electronically. Owing to this feature, television sets, mobile phones, satellite receivers and radar systems are able to change frequency without the need for any moving parts. The sections that follow deal with the physics, the varactor diode construction, the key parameters and the circuits in which the device proves its value.

What is Varactor Diode

A varactor is a semiconductor junction diode which has been designed to make use of the capacitance of a reverse-biased PN junction that varies with voltage. When reverse bias is applied, the mobile carriers move away from the junction and a depletion region is left behind which functions as an insulating dielectric between two conductive areas. Increasing the width of this region by raising the reverse voltage reduces the capacitance, just as does moving the plates of a capacitor further apart. Typical devices provide a capacitance in the range of 1 pF to 500 pF at low bias and have tuning voltages from 0 V to 30 V. In practice, however, the diode is used almost entirely in reverse bias because forward conduction would destroy the useful capacitive characteristics.

Varactor Diode Characteristics

The varactor diode characteristics are based on a limited number of parameters, these values determining the frequency range which a circuit can cover, the degree to which the signal remains clean and the amount of control voltage required; three features are most important in practice.

Capacitance Versus Reverse Voltage

The main characteristics of a varactor diode are given by the formula C = C0 ÷ (1 + V ÷ Vbi)^n, where C0 represents the capacitance at zero bias, Vbi is the built-in potential which is approximately 0.7 V for silicon, and n is the grading exponent; for an abrupt junction the value of n is 0.5, whereas for a hyperabrupt junction it is 1 or higher. A diode that has a capacitance of 40 pF at 1 V can drop to 8 pF at 20 V, resulting in a ratio of 5:1.

Quality Factor and Series Resistance

The quality factor, denoted by Q, is equal to the capacitive reactance divided by the series resistance, which means that the higher the resistance the lower the Q value. Silicon varactors usually have Q values in the range of 100 to 400 at a frequency of 50 MHz, while gallium arsenide varieties go above 1,000 at microwave frequencies. Since a low Q results in greater loss and an increased oscillator phase noise, high-frequency designs prefer GaAs devices even though they are more expensive.

Breakdown Voltage and Leakage Current

The maximum value that the tuning range can reach is determined by the reverse breakdown voltage, with typical figures ranging from 12 volts to 60 volts. Leakage current is generally in the nanoampere range, although it increases with temperature and has the effect of shifting the bias point. The capacitance temperature coefficient is usually between 300 and 600 ppm/°C. For this reason, designers ensure that the bias remains below the breakdown level and make allowance for drift in precision oscillators.

Varactor Diode Construction

The way in which components are manufactured determines the form of the capacitance curve and the maximum frequency; the semiconductor material, the doping profile, and the package all have an effect on performance. Only by understanding how a varactor diode is constructed can one explain why two parts which have the same capacitance at one voltage can behave in a very different way over the tuning range.

Semiconductor Materials and Junction Types

Most devices make use of silicon, which is obtained through diffusion or by means of epitaxial growth on a heavily doped substrate. Gallium arsenide is used in microwave applications since it has a higher electron mobility and lower series resistance. Abrupt junctions feature a uniform change in doping, while hyperabrupt junctions employ doping that increases as one approaches the junction. The second type gives rise to a steeper curve, a characteristic that is suitable for wide-range tuning such as that required by television and FM tuners.

Doping Profile and Epitaxial Layer

The concentration of dopants determines the width of the depletion region and thus the change in capacitance. Above the heavily doped substrate there is a lightly doped epitaxial layer, which ensures that the series resistance remains low while at the same time maintaining a broad depletion region. The thickness of the layer is usually between 1 µm and 10 µm. Hyperabrupt profiles are obtained through ion implantation or by using controlled epitaxy, and the capacitance ratio that results can reach 10:1 or higher within the defined bias range.

Packaging and the Circuit Symbol

The components are available in surface-mount packages including SOD-323 and SOT-23, as well as in axial leaded and microwave chip types. The varactor diode symbol is the standard diode symbol, which consists of a triangle and a bar, together with a capacitor plate placed next to the cathode bar to show that the capacitance is variable. Dual common-cathode packages are widely used since they enable balanced tuning. At high frequencies, package parasitics, ranging from 0.2 pF to 0.5 pF, become important.

Understanding Varactor Diode Working

The varactor diode working is based on a simple physical scenario in which a reverse voltage alters the depletion region and this change in width results in a change of capacitance; the device thus functions as a capacitor controlled by voltage and draws only a negligible control current, a property that renders it suitable for use in tuning circuits.

Depletion Region and Reverse Bias

As the reverse voltage increases, the holes in the P region and the electrons in the N region move away from the junction. The depletion layer therefore becomes wider and the capacitance is given by C = εA ÷ W, in which W stands for the width, A for the area and ε for the permittivity. If the width is doubled the capacitance is roughly halved. Since the diode in this state permits only a very small leakage current, the DC control source is not heavily loaded.

Tuning an LC Resonant Circuit

When a diode is connected in parallel with an inductor, a resonant circuit is obtained having a frequency given by f = 1 ÷ (2π√LC). Because the capacitance varies with the bias voltage, the resonant frequency can be altered electronically. For instance, a 100 nH inductor together with a varactor whose capacitance changes from 40 pF to 8 pF causes the circuit to tune from approximately 80 MHz to 178 MHz. Capacitors that block direct current keep the control voltage isolated from the remainder of the circuit.

Signal Level and Distortion Limits

A big RF signal can cause the diode to move through part of its bias range, leading to distortion and the generation of harmonics. When diodes are connected back to back, the even-order products are cancelled out, and as long as the signal amplitude is small, usually under 100 mV, the response remains linear. Components operated above this level require a higher bias and a smaller value of C0. It is for these reasons that designers carefully select the configuration and the bias point well before deciding on any specific package.

Varactor Diode Applications

Most of the demand is for wireless equipment, since tuning, modulation and frequency synthesis all rely on voltage-controlled capacitance. Varactor diodes applications are majorly found in test instruments, radar and consumer electronics; the three areas mentioned below are the most common.

Voltage-Controlled Oscillators and Phase-Locked Loops

A voltage-controlled oscillator includes a varactor in its resonant circuit so that the output frequency is determined by the control voltage. Within a phase-locked loop, the output of the loop filter controls the varactor and thus locks the oscillator to a stable reference. This setup makes up the fundamental part of the frequency synthesizers used in mobile phones, Wi-Fi radios and satellite receivers, the tuning ranges extending from a few per cent to more than an octave.

Tunable Filters and Receiver Front Ends

Varactor-tuned bandpass filters keep up with a desired channel by electronically adjusting their resonant frequency. In the past, FM broadcast receivers and television tuners used them for selecting a station, replacing mechanical capacitors. Today, software-defined radios employ them for preselector filtering in order to reject out-of-band interference. Since only a voltage is required for tuning, a microcontroller together with a digital-to-analogue converter can control the whole front end.

Frequency Multipliers and Modulation

When a large-signal drive is applied, the nonlinear capacitance causes harmonics to be produced, which is why a varactor can be used as a frequency multiplier in microwave transmitters. In the case of frequency modulation, the audio signal is added to the bias voltage so that the oscillator frequency changes in accordance with the amplitude. Parametric amplifiers had previously made use of this effect for low-noise amplification. In control panels, electric switches are used for switching the supply on and off as well as for isolation, while semiconductor tuning devices are responsible for adjusting the signal level.

Conclusion

A varactor diode is able to convert a control voltage into a variable capacitance, and this one function forms the basis of tunable filters, oscillators and synthesizers in modern electronics. The right choice will depend on the capacitance range, the Q factor, the breakdown voltage and the doping profile. Silicon is suitable for most radio frequency applications, whereas GaAs is used for microwave applications. For power distribution, control equipment and protective devices which support electronic equipment, Schneider Electric eShop provides a wide variety of electrical products for use in industrial and commercial installations.

FAQs

1. What is the difference between a varactor and a Zener diode?

A Zener diode is designed for stable voltage regulation in reverse breakdown, whereas a varactor is operated well below breakdown for its capacitance. The doping and geometry are optimised for different purposes.

2. Which parameter indicates the tuning range?

The tuning ratio, the ratio of maximum to minimum capacitance over the specified voltage range, shows how far a circuit can tune. Datasheets quote it between two stated bias points, such as 1 V and 25 V.

3. Why does temperature affect a tuning diode?

Capacitance and leakage both drift with temperature, and the built-in junction potential changes at about −2 mV/°C. Oscillators therefore use temperature-compensated bias circuits or crystal references.

4. Can a varactor replace a mechanical variable capacitor?

In most small-signal radio circuits, yes. Mechanical capacitors still suit very high-power transmitters, where RF voltage would exceed the diode’s linear range.

5. How are varactors tested?

A capacitance-voltage (C-V) meter or LCR meter measures capacitance at specified bias points, typically at 1 MHz or 100 kHz. Results are compared with datasheet curves.

Older posts Newer posts