Schneider Electric & Contactor Relay

As vital electricity is in sustaining our everyday life, it has its fair share of risks. One of the biggest threats posed by electricity is the risk of permanent electrical damage to connected devices. Certain electrical devices or motors require high voltage to function properly. So, while high voltage current does not affect these devices adversely, problems can arise when the amount of current passing through the electrical circuit is unprecedently high or is not stable.

What are contactor relays?

There is no failsafe way of preventing the sudden surges or dips of voltage in an electrical motor. The electrical input can soar to dangerously high levels during power anomalies, which is harmful to electrical appliances connected to the circuit. In order to avoid any permanent damage, necessary precautions must be taken. One of the precautions usually taken in order to avoid device burnouts is by installing contactor relays that have multiple contacts. A different motor can be connected to each of them. Thus, any amount of voltage can pass through the electric motor without causing any harm to the main circuit.

How do contactor relays work?

There are three main components of a power contactor and each of them plays an important role in the working procedure. They form the core of the contactor which is electromagnetic in nature. Current passes through the contactor which is responsible for exciting the electromagnetic core. Due to this flow of electricity, a magnetic field is created, which affects the electrical contacts.

Contacts are of different types, but they primarily have a common quality of high welding resistance and stable arc resistance. These contacts are also durable against erosion and mechanical stress for longer performance and durability. A contactor usually has a movable contact and a fixed one. The magnetic field causes them to form a normal, closed circuit which is responsible for switching on the motor. The enclosure binds the sensitive components of a contactor and its function is simply protection. As soon as the flow of current is stopped, the electromagnetic core loses its energy and returns to its neutral state, resulting in an open circuit. This, in turn, switches the electric motor off.

Advantages of using contactor relays at home –

An alternative to using a contactor relay at home is constructing special switches or rewiring your entire home to accommodate electrical motors that have unstable power. This is not just extremely complicated, but also very expensive. Instead, purchasing contractor relays is much more budget-friendly and less of a hassle. Moreover, it can adjust well with both AC and DC devices. All it does is take up a fair amount of space and make sure that the power surges in an electric motor have no negative influence on the other electrical devices at home. Installing a contactor guarantees less power consumption and does not even require much maintenance. Most modern homes have switched to contactor relays for electrical support and device efficiency.

Contactor relays from Schneider Electric

Schneider Electric features some of the best contactors electrical that are available in the market. While each of them has distinct features, you can choose the one that suits your needs the most.

- TeSys Giga Control Relay

The feature that sets the TeSys Giga Control Relay apart is its ability to self-diagnose in case of any issue. It is equipped with an overload alarm that goes off as soon as the amount of power crosses the threshold value. It has a wide voltage control and is dustproof, which reduces the risk of coil burning.

- TeSys Thermal Overload

The TeSys Thermal Overload relay contactors have an extremely appealing design. The modern and stylish look will suit the aesthetics of any home. Moreover, it is equipped to support Electro domestic and HVAC applications. The maintenance cost is pretty low making the TeSys Thermal Overload relay contactors an extremely wise purchase in the long run.

- EasyPact TVS

The TeSys LR9 series has a wide product range to choose from. Thus, you can find the most appropriate product for your electric motor at Schneider Electric. It sports a high level of accuracy because of thermal modelling which is why it can adjust well even with extremely demanding applications.

- TeSys LR9 – LR9D / LR9D –

If you are looking for a contactor that is simple yet effective, then the EasyPact TVS contactors will be perfect for you. Their designs are fairly uncomplicated and do not take up much space in your home. The performance provided by the contactor from the EasyPact TVS series is exactly what you need to ensure a stable electrical line.

Buy the best contactor relays at Schneider Electric’s online store

Contactor relays are extremely essential if you want to ensure the smooth running of your electrical devices. And, you can find the best range of contactor relays at Schneider Electric online store with guarantees of long-lasting, top-quality performance. You can also visit the online Schneider Electric store for amazing deals on electrical products and components that are bound to ensure maximum electrical safety and efficiency in your household.

Read More:- All You Need To Know About Contactors