Know All About Smart Fan Regulator

The summer season is fast approaching over the Indian subcontinent. And to beat the torrid summer heat, what can be better than sitting down to cool off under the relaxing breeze of a ceiling fan? However, getting up to adjust the regulator every time you want to change the fan speed can be cumbersome, especially when you’re trying to relax. Therefore, it might be a wise idea to equip your household with the best smart fan regulators from Schneider Electric and upgrade your home with a more comfortable, convenient, and smarter option than conventional fan regulators.

What are smart fan regulators?

As implied by its name, a fan speed regulator is responsible for operating and adjusting the speed of ceiling fans. However, with improvements in technology, modern homes have replaced the traditional fan speed regulator models with newer ones. The latest smart fan speed regulators, in this regard, has grown extremely popular over the past years due to their very convenient functioning.

The smart fan speed regulator does not require any manual control and can be adjusted remotely through voice commands or smartphone applications. Not only are these smart fan regulators immensely convenient, but they also come with several other benefits, including:

- They are easy to install and control

- Their stylish, modular design goes well with the aesthetic of modern homes

- Benefits like cloud-based operation, scheduling, and more

- Requires little maintenance and less servicing

- Incredibly durable and long-lasting

Smart fan regulators from Schneider Electric

The Schneider Electric online store has your back this summer with these carefully crafted models of smart fan speed regulators for maximum convenience and comfort:

  • Wiser - Fan Speed Controller
  • Wiser is among the biggest brands of home automation systems in India. And since the launch of the Wiser fan speed regulator, Wiser has become yet more popular. The fan speed regulator from Wiser is extremely convenient due to its small size, making it easy to maintain and manage. The small size of the Wiser fan speed controller makes it possible to fit behind existing switches without having to change the wiring or other components. Furthermore, it comes with noiseless performance and can be used to control ceiling fans without any humming noise. In addition to convenient remote operation via the Wiser smartphone app, the Wiser fan speed controller can also be manually controlled via a bell switch to increase or decrease the fan speed. The Wiser fan speed controller can also be controlled through commands over IoT Aggregator and can be integrated with other Z-Wave devices for event-based operations.

  • Wiser - Two-Channel Dimmer Controller
  • The Wiser Two-Channel Dimmer Controller is another popular choice for those wishing to upgrade their modern home with a smart fan controller. The Wiser Two-Channel Dimmer controller does not just convert mechanical switches into smart switches, but it also supports analogue and direct dimmer functions simultaneously. Supported by cutting-edge operation technology, the Wiser Two-Channel Dimmer Controller can be operated remotely either by the Wiser app or over voice commands. Furthermore, it has been equipped with bell switches to raise or lower the fan speed, as well as regulate the light intensity manually. This Two-Channel Dimmer Controller from Wiser is convenient to install and manage due to its smaller size and is a great option for the approaching summer because of its comfortable price range.

  • Opale - 1200W Electronic Dimmer
  • Opale is one of the most favoured brands of household electrical components in India, known for its efficiency and economical price. The 1200W Electronic Dimmer from Opale is an exquisite fan speed regulator. It comes with an attractive look that significantly improves your home decor with its unique patented satin finish and modern designer look. The satin finish also lends to the Opale 1200W Electronic Dimmer’s durability, making it resistant to scratches and most physical damages. In addition, they are easy to install and manage, with an anti-glare coating which also minimizes the accumulation of dust over time. The Opale 1200W Electronic dimmer has been constructed with a high-grade flame-resistant material, which greatly eliminates the risks of accidents like electrical fires and short circuits. The convenient operation and easy, noiseless function make the Opale 1200W Electronic Dimmer a popular fan speed regulator across India. The Opale 1200W Electronic Dimmer comes in several colour options, including dark grey and white, making it incredibly adaptive to the aesthetic of any modern home.

  • Are you ready for the summer?
  • Be ready for the sizzling summer with smart fan regulators. You can conveniently choose from the wide range of products from the online Schneider Electric store and purchase a smart fan dimmer switch from the comfort of your home. You can also look for other manual fan speed regulator models that will complement the aesthetics of your home. In addition to fan speed regulators, the Schneider Electric online store brings together all electrical components and solutions under one roof for you to compare and choose from. This summer, bring home comfort and convenience with a new smart fan regulator from Schneider Electric.

Read More: - Why Anti-Bacterial Switches Are A Good Choice For Home