What is Hydroelectric Power? Working, Types, Uses and Benefits

What is Hydroelectric Power? Working, Types, Uses and Benefits

Summary

What is hydroelectric power? Mainly, it is power derived from moving water. The article discusses the hydroelectric energy meaning, the different types of power plants, and their everyday applications. It also explains how hydroelectric power works, beginning with the lake located behind a dam and ending with the wires on a pole. It then compares the advantages with the limitations.

Key Takeaways

  • Hydroelectric power converts moving or falling water into electricity using turbines, generators, and transformers.
  • Electricity production depends on water flow, head, and turbine efficiency, which varies according to site conditions.
  • Impoundment, run-of-river, and pumped-storage plants serve different purposes based on water availability and electricity demand.
  • Hydropower provides renewable electricity, low operational emissions, flexible generation, grid stability, and long-term operating benefits.
  • High construction costs, ecological disruption, community displacement, and unpredictable rainfall create significant challenges for hydropower projects.
  • Careful site selection, environmental assessments, regular inspections, and effective water management improve hydropower project safety and reliability.

Introduction

For over two thousand years people have used water to carry out work. For instance, early mills made use of a wheel and a stream to grind grain. Nowadays the same principle is used to light entire cities; a single large dam can supply power for millions of homes. In fact, hydroelectricity provides about 14 percent of the world's power and therefore is the leading renewable energy source. Yet a great many people overlook the finer points. What is the importance of a dam lake? And what distinguishes a run-of-river plant from pumped storage? This article gives answers to both questions and also looks at the various parts, the different types, the advantages, and the trade-offs.

What is Hydroelectric Power

The hydroelectric energy meaning is simple. It is power generated by the force of water which is moving or falling. Rivers are filled by rain and by melting snow, and gravity causes the water to flow down hills. A power plant catches this force as the water goes downhill and then converts that force into power. Since nothing is burned, there is no smoke emitted from the site. Those who wish to obtain reliable hydroelectric energy information should look at three figures: head, flow, and efficiency. Today's turbines are able to turn 85 to 95 percent of the water's energy into power, whereas coal and gas plants seldom achieve such figures. In fact, hydroelectric power is the oldest large renewable energy source that is still in regular use.

How Does Hydroelectric Power Work

The working of hydro power plant systems involves a series of steps. Initially, height is converted into speed; then, speed is transformed into spin; and lastly, spin is turned into power. There are four stages you must know about when learning how does hydroelectric power work.

Water Storage and Intake

A dam raises the level of the water and creates a reservoir. The water stored in the reservoir contains energy due to its height. The distance between the surface of the lake and the turbine is known as the head, and the greater the head, the more energy is obtained from each litre. At the intake there are gates and screens which prevent debris from passing through and regulate the flow. Because of this, the operators open or close the gates in order to meet demand, which is the reason why reservoir power stations are so flexible.

Penstock and Turbine

The water, as it comes in, flows down a large steel pipe known as the penstock. As it descends, pressure increases and the jet then strikes the turbine blades. The most suitable type of turbine varies according to the site; Pelton wheels are appropriate for a head above 300 metres, Francis turbines are used for medium head and Kaplan turbines work most efficiently at low head with a high flow. Each type of turbine performs well only within its own range.

Generator and Transformer

A shaft connects the turbine to the generator. The operation of generators in a hydroelectric power plant is based on one simple principle: when a magnet passes by a coil of copper, an electric current is produced. The magnets rotate within the coils and as a result alternating current flows out. The output is generally in the range of 11 kV to 25 kV. This voltage is then increased by a step-up transformer to 132 kV, 220 kV or even higher. The reason for using a higher voltage is that it results in a lower current, which in turn means less power is lost over long distances. At the same time, the water that has been used exits via the tailrace and then returns to the river.

Transmission and Distribution

The power lines carry the electricity to substations, where the transformers reduce it once more. From there, the local power grids pass it on to houses, factories, and shops. Within a building the power reaches a power distribution board, which then divides it into safe circuits for lighting, sockets, and machines. That final stage is essential if safe delivery is to be achieved. Many people are unaware that the matter of delivery is just as important as the generation of power.

Hydroelectric Power Plant Classification

Hydroelectric power plant classification generally depends on whether they have storage facilities, a certain head, or a particular size. The most frequently used approach is to consider how the station manages water; in addition, head and size provide two other useful perspectives. All of these methods together apply to almost every power plant in the world.

Impoundment Plants

Impoundment plants make use of a big dam and a reservoir; the best-known example is China's Three Gorges Dam, which has a generating capacity of 22,500 MW. The operators collect water during the wet months and then release it when demand is at its highest. Owing to this ability to control water levels, such plants are well suited to providing both base supply and peak supply, and they also assist in flood control and in meeting water demands. The drawback is that the costs of construction and the amount of land required are high.

Run-of-River Plants

Power stations of the run-of-river type channel a portion of the river through a canal or a pipe; they have either no storage or very little. The amount of electricity they produce therefore varies with the flow, reaching a peak during the monsoon and falling in the dry months. Less damage is done to the valley since there is no large reservoir causing flooding of the area. For instance, many of the projects in the Himalayas make use of this kind of design in order to take advantage of the steep slopes with only small diversion weirs.

Pumped Storage Plants

Pumped storage plants function like a huge battery: there are two lakes at different heights. While demand is low, excess electricity from the grid is used to pump the water uphill; when demand increases, the water flows back down through turbines. The efficiency for the whole process is generally between 70 and 80 percent. Nevertheless, pumped storage still contains the majority of the world's grid-level storage and its importance is increasing as the use of solar and wind energy expands.

Classification by Head and Capacity

Another method of classifying plants is according to the head. Schemes with a low head are those beneath 30 metres, medium-head schemes lie between 30 and 300 metres, and high-head schemes are above 300 metres. Size also provides a second classification. In India, micro plants have a capacity of up to 100 kW, mini plants up to 2 MW, and small plants up to 25 MW; anything larger is considered to be large. Different types of turbines and civil engineering work are required for each category.

Uses of Hydroelectric Power Plant

Hydroelectric stations all over the world provide electricity for cities, farms, factories, and isolated villages, and in many cases a single well-thought-out project meets all these needs. Some common uses of hydroelectric power plant are as follows.

Grid Electricity Supply

The primary function is to supply the national grid; hydroelectric units can start up within minutes, which is much quicker than coal or gas power stations. Because of this, grid operators make use of them to counter sudden changes in demand. Hydroelectric power also has the capability for black start, allowing the grid to be restarted following a blackout. Large stations usually operate at a capacity of between 40 and 60 percent and vary their output throughout the day.

Irrigation and Water Supply

During the dry season, reservoirs store water which has been collected during the monsoon. This water is then transported by canals to the farms and allows crops to be grown over large areas. For example, the Bhakra Nangal dam in India combines water for farming with its power generation. Cities also get their drinking water from such lakes. Since the income from power sales is used to finance the project, one dam provides water for both agricultural use and for the electrical grid.

Flood Control and Navigation

Dams retain the peak floodwater and release it gradually, thereby protecting towns and farms situated downstream. Consider the fact that a single controlled release can prevent damage that is worth much more than the amount earned from selling power for a whole season. Furthermore, the locks located next to large dams allow cargo boats to use the rivers, thus reducing freight costs. In addition to this, the lakes provide opportunities for fishing and leisure activities.

Industrial and Remote Power

Small plants supply electricity to villages and industries that are distant from the main power grid; aluminium smelters, paper mills, and mines usually get their power directly from local hydroelectric units. At these sites, a power distribution board divides the main supply into feeders for motors, drives, and lighting. On a smaller scale, micro hydro systems operate; in hilly areas a stream and a small turbine are sufficient to light a village with a few kilowatts.

Benefits of Hydroelectric Power

The advantages of hydroelectric power go beyond clean energy; fuel costs amount to nothing, the plants have a lifespan spanning generations, and the output can be quickly adjusted.

Renewable and Low Carbon

Water is replenished as a result of the rain cycle, which means that the fuel will never be used up. The median value for lifecycle emissions is around 24 grams of CO2 equivalent per kWh. In contrast, coal is about 820 grams. Since there is no burning, there is also no sulphur dioxide, soot, or ash at the plant. Hence, replacing coal with hydroelectric power reduces both greenhouse gases and local air pollution.

Low Operating Cost and Long Life

After it has been constructed, a hydroelectric power station does not have to pay for fuel. The costs of operating and carrying out repairs remain low, and a great many plants continue to function for between 50 and 100 years, with new components being installed at various times. Some of the stations that were built a hundred years ago are still in operation today.

Grid Flexibility and Reliability

Few sources react as quickly as hydro. A turbine can go from being stationary to full load within a matter of minutes. This is useful for keeping the grid stable when demand rises or when wind and solar power output falls. Moreover, reservoir stations store energy in the form of water, making it available at any time.

Multipurpose Value

One project is capable of providing power, water for farming, drinking water, protection against floods, and opportunities for leisure. This common benefit increases the total value of a dam. At the same time it promotes local development, as roads, jobs, and services move into remote areas with large projects.

Limitations of Hydroelectric Power

No power source is flawless, and hydroelectric power has actual limitations. The costs arise immediately, suitable locations are rare, and rivers alter once a dam has been built.

High Capital Cost and Long Build Time

Because a big dam requires a great deal of civil engineering work and construction can take between five and ten years, the costs usually lie between 1,500 and 5,000 US dollars per kW depending on the terrain. Delays and cost overruns are frequent on such large projects, so investors have to wait a long time before they start to see a return. As a result, it is more difficult to obtain funding for dams than it is for solar or wind farms.

Environmental and Ecological Impact

Dams alter the flow of rivers, prevent fish from reaching their usual habitats, and cause silt to be trapped. The silt stored behind the dam leads to the starved conditions of the river deltas and floodplains downstream. In warm areas, the lakes may also give off methane as a result of decaying plants. The effects can be lessened by the use of fish ladders, by scheduling water releases, and by choosing careful sites for the dams. However, they cannot eliminate these effects altogether.

Dependence on Rainfall and Geography

Output is dependent on water, and droughts, the shrinking of glaciers, or changes in the monsoons can all lead to a sharp reduction in output. Even if a site is good it still needs the correct balance of flow and head, and the most suitable sites are usually in remote areas or are already being used. The need to run long power lines increases both the cost and the losses.

Displacement and Safety Concerns

The construction of reservoirs causes land, villages, and farms to be flooded. Large-scale projects have led to the displacement of millions of people all over the world, raising serious issues regarding housing and compensation. Holy sites and forests can also be lost. There is also concern about dam safety since a failure could put the towns located downstream in danger.

Conclusion

Hydroelectric power works since gravity takes care of the heavy part of the process; water flows down through a penstock and causes a turbine to spin. The turbine's rotation is then converted into alternating current by a generator, after which a transformer increases the voltage for transmission. Once you understand how hydroelectric power works and the various stages of a hydroelectric power plant have been made clear, the rest is easy to grasp. If you would like to find out more about hydropower, get product recommendations, or need a power distribution board appropriate for a plant or site, the Schneider Electric eShop is a good place to begin. However, a site study carried out by a qualified engineer should still be the first step.

FAQs

Which country makes the most hydropower?

China leads by a wide margin, followed by Brazil, Canada, and the United States. China alone supplies close to 30 percent of global hydro output.

What is a surge tank and why does a hydro plant need one?

A surge tank is a tall chamber linked to the penstock. It soaks up sudden pressure jumps, known as water hammer, when turbine gates open or close fast. As a result, the pipe and gear stay safe.

How is hydropower different from tidal energy?

Hydropower uses river flow and gravity, while tidal energy uses the rise and fall of ocean tides. Tidal output is easy to predict but limited to coasts. Tidal capacity worldwide also remains small by comparison.

How much of India's power capacity comes from hydro?

Hydro supplies roughly one tenth of India's installed capacity. Much of the unused potential lies in the Himalayan states and the north-east, where steep land and heavy rain favour new projects.

Can an old hydro plant be upgraded?

Yes. Operators often replace runners, fit new governors, and add digital controls. These upgrades can lift efficiency and output by several points and add decades of life, usually at a cost well below that of a new dam.

Older posts Newer posts