What is the Difference between MCB, MCCB, RCB, RCD, RCCB, and RCBO?
Summary
Learn the differences between MCB, MCCB, RCD/RCCB, RCBO and RCB: MCBs protect low-power circuits (0.5–125 A), MCCBs handle high currents (up to 1000 A), RCD/RCCB detect earth leakage, and RCBO combines overcurrent + earth-fault protection — pick by load, fault type and application.
Key Takeaways
• MCB = miniature circuit breaker for low-power circuit overload/short-circuit protection.
• MCCB = moulded case breaker for higher current industrial loads (up to ~1000 A).
• RCD / RCCB = earth-leakage detectors that trip on residual current (safety from electric shock).
• RCBO = combines MCB (overcurrent) + RCD (earth-leakage) in one device.
• RCB (term used on site) refers to residual circuit protection devices — check specs for exact function.
• Choose by current rating, fault type (overload vs earth leakage), and application (domestic vs industrial).
Circuit breakers are protective devices that control the flow of electrical current within the circuits. They play a vital role in maintaining the safety and integrity of electrical systems by interrupting the current in cases of abnormal flow. Thus, by preventing excessive current flow and potential hazards, circuit breakers ensure the reliable operation of electrical installations. MCB, MCCB, RCB, RCD, RCCB, and RCBO are all different models of circuit breakers. They are used in homes and organizations to prevent potential electrical hazards.
Table of Contents
- Why Are Circuit Breakers Important for Electrical Safety?
- What are MCB and MCCB?
- What are the Similarities between MCB and MCCB?
- What are the Differences between MCBs and MCCBs?
- What is RCB, RCD, RCCB, or RCBO?
- What are the Similarities and Differences between RCD and RCBO?
- What are the Differences between an RCD and MCB?
- What are the Similarities Between MCB and RCCB
- Difference Between MCB VS RCCB
- What are the Similarities Between RCD and MCB?
- What are the Similarities Between RCCB and RCBO
- What are the Differences Between RCCB and RCBO
- Schneider Electric eShop - A One-Stop Solution for all your Electrical Requirements
- Frequently Asked Questions
These various terms in the realm of electrical circuits and protection devices may seem confusing, especially to the uninitiated. However, it is crucial for you to understand the essential differences among these devices in order to ensure the safety of electrical installations in your home and/or business as well as the safety of all the people in the vicinity and the premises.
Hence, in this article, we shall take you through the similarities and differences among MCCB circuit breakers, MCB, RCB, RCD, RCCB, and RCBO, shedding light on their specific applications and functionalities.
Why Are Circuit Breakers Important for Electrical Safety?
Electrical appliances used nowadays are protected by circuit breakers like RCB breaker, MCCB circuit breaker, and RCBO to secure circuits from overload, short circuit and ground fault. They instantly shut off power in the event of faults hence averting electric fires, possible equipment damage as well as protecting individual well-being. Thus they are able to enhance and maintain a standard and secure electrical system in the homes and businesses.
What are MCB and MCCB?
MCB
MCB stands for Miniature Circuit Breaker. They are widely used protective devices in electrical systems. MCBs are typically designed to meet the needs of low-power applications, generally ranging from 0.5A to 125A. They are most commonly used in residential and commercial installations to protect circuits against short-circuiting and power overload.
MCCB
The full form of MCCB is Molded Case Circuit Breaker. They are capable of handling extremely high currents, up to 1000A. They are extensively used in industrial applications where large electrical loads need to be safeguarded.
Understanding the Benefits of Using Moulded Case Circuit Breakers (Mccb)
What are the Similarities between MCB and MCCB?
MCBs and MCCBs share some similarities and some of the most common ones are as follows:
-
1. Both are protective devices designed to interrupt the flow of current in cases of overload or short-circuiting.
-
2. They provide a vital safety feature by preventing damage to the electrical system and minimizing the risk of electrical fires.
-
3. Both mainly find application in low-voltage or low-tension settings.
-
4. Both MCBs and MCCBs are available in the market with different current ratings.
-
5. Both types of devices can be manually operated, i.e., switched on or off for purposes of maintenance.
What are the Differences between MCBs and MCCBs?

Despite their similarities, MCBs and MCCBs have some clear differences as well, especially in terms of construction, application, and performance characteristics. Some of the most prominent differences between MCBs and MCCBs are as follows -
-
1. Current rating refers to the maximum current that MCBs and MCCBs can draw without getting damaged. While an MCB has a current rating of 100A, the current rating for an MCCB circuit breaker is between 10-200A.
-
2. Their interrupt rating is also a major area of difference between these two protective devices. Interrupt rating refers to the maximum current that a self-operating electrical switch can block without getting damaged. MCBs usually have an interrupt rating of up to 1800A while MCCBs come with a much higher interrupt rating ranging from 10KA-200KA. This makes MCCBs highly suited for industrial purposes including heavy-duty machinery and equipment. MCBs, on the other hand, are best suited for smaller appliances and limited electrical loads.
-
3. One of the most crucial components of self-operating switches is the tripping circuit. A tripping circuit leads to the breakage of the circuit in cases of abnormal current flow. While an MCB has a fixed tripping circuit, MCCBs come equipped with movable tripping circuits.
-
4. While an MCB can have up to 3 poles, MCCBs often have up to 4 poles. ‘Poles’ refers to the number of safety and switching phases the MCB or MCCB circuit breaker has to maximize safety.
-
5. In case of abnormal electrical conditions such as extremely high voltages or power surges, MCBs turn off automatically. This happens due to its operational mechanism wherein extremely high voltage conditions lead to disconnection in the circuit and stops the flow of electricity. Short circuits can also be expertly detected by this mechanism and in such cases too, the circuit is broken. This prevents damage to appliances and electrical equipment by safeguarding them from the potential hazards of voltage surges.
The role of MCCBs, on the other hand, is to avert electrical overload and consequent overheating of the electrical circuit. It has bimetallic components which expand and contract when they detect an overload in the circuit. An open flow of electricity is allowed by the MCCB under normal circumstances.
However, the MCCB gets heated up when the circuit is overloaded. This results in the prevention of electricity flow by the bimetallic components leading to the cooling down of the MCCB.
-
6. MCCBs allow for remote operation via shunt wires. This feature is not available for MCBs.
| Characteristic | MCB | MCCB |
|---|---|---|
| Full Form | Miniature Circuit Breaker | Moulded Case Circuit Breaker |
| Tripping Circuit | Fixed | Movable |
| Definition | A Miniature Circuit Breaker (MCB) is an electrical switch designed to protect an electrical circuit from damage caused by overload or short circuit. It automatically interrupts the flow of current. | A Moulded Case Circuit Breaker (MCCB) is an electrical device designed to protect electrical circuits from overcurrents and short circuits. It is enclosed in a molded case for enhanced safety. |
| Poles | Available in single, two, three versions | Available in single, two, three, four versions |
| Uses | For domestic purposes like home wiring | For commercial and industrial use |
| Rating current | 100 amps | 10-200 amps |
| Remote on/off | Not possible | Possible |
What is RCB, RCD, RCCB, or RCBO?
Now that we have a comprehensive idea about MCBs and MCCBs, let us move on to RCB, RCD, RCCB, and RCBO. All of these are protective devices widely used for personal and equipment protection against flaws in the current flow and electrical shocks.
RCB
RCB stands for Residual Current Breaker. It is a general term that encompasses both RCD (Residual Current Device) and RCCB (Residual Current Circuit Breaker). An RCD is designed to quickly disconnect the circuit when a residual current exceeds a certain value. Residual current refers to a current imbalance between the live and neutral conductors.
An RCCB combines the functions of an RCD electrical device and an MCB electrical device, providing protection against surcharge, residual currents, and short-circuiting.
RCD
An RCD (Residual Current Device) checks for any difference in current in live and neutral conductors which implies leakage currents. If there is a fault it isolates them from power thus no chance of one being electrocuted. The use of RCDs is important especially in regions with much moisture like the bathroom with regard to protecting the user from electrical faults.
RCCB
An RCCB – Residual Current Circuit Breaker, is an electric shock protective device which detects leakage currents. The main issue of RCCBs is that unlike other circuit breakers they are designed to protect from touching live wires and also provide earth fault protection which is essential for safety.
RCBO
An RCBO circuit breaker is an entity of an RCD and MCB in that it acts as a Residual Current Breaker with Overcurrent. It offers protection from overcurrent as well as earth leakage faults. They are employed in single circuits for providing overload protection as well as residual current detection, which demonstrates high flexibility of the RCBOs in electrical safety.
What are the Similarities and Differences between RCD and RCBO?

Both RCDs and RCBOs (Residual Current Breaker with Overcurrent) have a common goal of protecting against electric shock and minimizing the risk of fatal accidents. They both detect and interrupt the circuit when a residual current surpasses a specific threshold, ensuring the safety of individuals and preventing electrical hazards.
The principal difference between an RCD electrical device and an RCBO lies in its construction and functionality. An RCD is a standalone device that is typically installed at the origin of the electrical installation. It offers protection to a group of circuits or to the entire installation, detecting imbalances in the current flow. An RCBO, on the other hand, integrates the functionalities of both an RCD and an MCB or MCCB. It combines the features of circuit protection against surge currents, residual currents, and short-circuiting in a single device. An RCBO provides individual circuit protection, allowing for selective disconnection in the event of a fault, without affecting other circuits.
| Characteristic | RCD | RCBO |
|---|---|---|
| Full Form | Residual Circuit Device | Residual Current Circuit Breaker with Overcurrent protection |
| Protection Circuit | Protects at least 5 circuits | Protects 1 individual circuit |
| Definition | A Residual Current Device (RCD) is a safety device designed to quickly disconnect electrical circuits when it detects an imbalance in the electric current, helping prevent electrical shocks and fire hazards. | A Residual Current Circuit Breaker with Overcurrent Protection (RCBO) is an electrical device that combines the functions of a residual current device (RCD) and a circuit breaker. It provides both earth fault protection and overcurrent protection in a single unit, enhancing electrical safety. |
| Working | Monitors the current flowing through the circuit. If it detects an imbalance, it will trip. | Monitors the current flow same as RCD and it will trip if it detects an imbalance, just like an RCD. However, it adds additional protection against overcurrent, making it more comprehensive. |
| Uses | Prevents accidental fires and electrocution | Same as RCD and protect a circuit from overload and short circuit. |
| Versatility | Only be used to protect against shocks caused by ground faults. | Can be used to protect against shocks caused by ground faults but also selectively protects the circuit from overcurrent situations. |
What are the Differences between an RCD and MCB?

While an RCD and an MCB both offer protection in electrical installations, their primary functions differ significantly. An RCD is concerned with detecting and interpreting residual currents, which occur when there is a leakage of current due to faulty equipment or a breakdown of insulation. It provides personal protection against electric shock and is particularly important in areas where electrical equipment is in direct contact with humans, such as in kitchens and bathrooms.
On the other hand, an MCB primarily acts as a circuit breaker, protecting against overloads and short circuits. It is responsible for interrupting the current flow when it exceeds the rated capacity of the circuit or when a short circuit occurs. MCBs are commonly used in residential and commercial settings to protect individual circuits and appliances.
| Characteristic | RCD | MCB |
|---|---|---|
| Full Form | Residual Circuit Device | Miniature Circuit Breaker |
| Usage | Provides personal safety | Provides safety to the electrical equipment and avoid the risk of overcurrent and overheating. |
| Definition | A Residual Current Device (RCD) is a safety device designed to quickly disconnect electrical circuits when it detects an imbalance in the electric current, helping prevent electrical shocks and fire hazards. | A Miniature Circuit Breaker (MCB) is an electrical switch designed to protect an electrical circuit from damage caused by overload or short circuit. It automatically interrupts the flow of current. |
| Working | The residual current device operation is based on the difference in the current flowing through the live and neutral wires generating a magnetic field. | This works by sensing the current flowing through the circuit. When the current flowing through it exceeds a certain limit, it trips. |
| Triping point | Normally trips at 30mA | Trips at 10, 16 or 32A |
Read Also: Understanding The Difference Between Isolators, Rccbs, And Mcbs: A Comprehensive Guide
What are the Similarities Between MCB and RCCB
Though MCBs and RCCBs serve different purposes, both are essential for electrical safety. Here's how they are similar:
- Protection-Oriented: Both devices ensure protection. MCB protects against overload/short circuit. RCCB protects from earth leakage current.
- Circuit Disconnection: Automatically disconnect circuits upon fault detection to minimize risk of fire or electrocution.
- Compact Design: Installed within distribution boards. Modular in size.
- Manual Reset: Both can be reset after tripping.
- Mandatory for Safety Compliance: Required by electrical safety standards in most residential and commercial settings.
Difference Between MCB VS RCCB
The below comparison clears up the difference between MCB vs RCCB and answers MCB vs RCCB which is better- both are better together.
| Feature | MCB (Miniature Circuit Breaker) | RCCB (Residual Current Circuit Breaker) |
|---|---|---|
| Primary Function | Protects against overload & short circuit | Detects and interrupts earth leakage |
| Current Range | Typically 0.5A- 100A | Typically 25A- 125A |
| Trip Mechanism | Thermal & magnetic trip | Senses difference between live and neutral currents |
| Protection Type | Current overdraw protection | Earth leakage & shock protection |
| Use Case | Suitable for all circuits | Best for human protection in wet zones (kitchens, bathrooms) |
What are the Similarities Between RCD and MCB?
Both RCDs (Residual Current Devices) and MCBs serve vital roles in modern electrical systems:
- Automatic Disconnection: Trip circuits when irregularities are detected.
- Electrical Safety Compliance: Often required in residential and commercial installations.
- Compact & Modular: Designed for DIN rail mounting.
- No External Power Source Needed: Work passively within the circuit.
- User Resettable: Can be manually reset post-tripping.
What are the Similarities Between RCCB and RCBO
Understanding RCCB vs RCBO reveals overlapping functions:
- Earth Fault Protection: Both detect leakage current to prevent electric shocks.
- Quick Disconnection: Shut down power supply upon imbalance in current.
- Improved Electrical Safety: Prevents fire hazards and personal injury.
- DIN-Rail Mountable: Easily installable in most modern panels.
- Essential for Home & Industry: Used in both residential and industrial setups.
What are the Differences Between RCCB and RCBO
For installations needing comprehensive protection, RCBO is superior. That's why searches like RCCB vs RCBO Schneider Electric and difference between RCCB and RCBO are common when upgrading systems.
| Feature | RCCB | RCBO |
|---|---|---|
| Full Form | Residual Current Circuit Breaker | Residual Current Circuit Breaker with Overcurrent Protection |
| Functionality | Detects earth leakage | Earth leakage + overcurrent/short circuit |
| Protection Scope | Entire circuit group | Individual circuits |
| Application | Suitable for general protection zones | Ideal for selective & specific protection |
| Maintenance | Less complex | Slightly more maintenance due to multifunctionality |
Schneider Electric eShop - A One-Stop Solution for all your Electrical Requirements
Now that you know all about the various protective devices that can safeguard electrical systems, it is time to look for devices that best suit your requirements. While investing in protective electrical devices like MCBs, RCBs, RCCBs, or RCBOs, make sure that you always buy from a reliable and authentic place such as the Schneider Electric eShop. Schneider Electric eShop is the one-stop solution for all your electrical needs, including surge protectors, home automation, protective devices, and smart switches. Browse through the Schneider Electric eShop for the complete range of products available. If you have further queries or require assistance, do not hesitate to contact the customer service team. Visit the website for details.
FAQs About
Q1. Which is better, RCBO or RCCB?
Ans: RCBO is more preferable because in addition to the residual protection it also has the overcurrent protection while RCCB is just used in protection of leakage current only. In other words, as an extended form of RCCB, the RCBO is much more useful for an all-round security.
Q2. Why use RCBO instead of MCB?
Ans: While an RCB MCB protects against overcurrent, an RCBO offers both overcurrent and earth fault protection. This makes RCBO more effective in safeguarding both the circuit and individuals from potential electrical hazards.
Q3. Can I use RCCB at home?
Ans: Yes, an RCCB is suitable for home use, especially in areas prone to moisture or where there is a higher risk of electric shock. It ensures protection by cutting off the power in case of leakage, providing enhanced safety for the household.
Q4. Which MCB is used in the house?
Ans: Typically, single-pole MCBs are used for household circuits, as they protect against overcurrent and short circuits. For larger appliances, double-pole or triple-pole MCBs may be used to handle higher loads and ensure better safety.
Q5. Should I use RCD or RCBO?
Ans: An RCBO is a better option than an RCD since it offers dual protection, both from earth leakage (like an RCD) and overcurrent (like an MCB). This makes RCBOs more comprehensive in protecting both circuits and individuals.
Comments