Circuit Breaker - An Introduction

Our homes and commercial spaces are a hub for electrical consumption. We use a range of devices and equipment that are plugged into electrical units for a large part of our day. All these devices need protection from current overload or short-circuits since such events can permanently damage our appliances. It is to protect our devices from such malfunctions that circuit breakers are used. Circuit breakers cut off or suspend the electrical flow to the appliance when it detects any anomalies in the power supply. These come in many types and varieties, depending on your consumption needs.

It’s integral that every residential, commercial, and residential space be equipped with a high-quality and durable circuit breaker. These little devices offer a powerful function of protecting your devices and yourself from harm by reducing the breakout of electrical fires.

5 Common Circuit Breaker Issues You Should Know About

While installing a circuit breaker is important, it’s just as important to know the signs that indicate there is an issue with your circuit breaker. Identifying these signs will help you take immediate action on fixing the problems. If these circuit breaker problems remain unidentified, then they can cause damage to the breaker and reduce its functioning capacity. This will then impact the safety of your space. So, to best identify and resolve circuit breaker issues, look for these common signs.

1) Flickering Lights - When the lights in your house flicker or dim, it could indicate a problem with your circuit breaker. Many people, though, are unsure of whether this specific sign means an issue with the light fixture or the circuit breaker. A simple of way identifying includes noticing at what point the lights flicker. For instance, if you turn on a high-voltage appliance such as a room heater or AC, then you may see the lights dim. This indicates that the problem lies in the circuit breaker. To solve this problem, you can install an alternative circuit for high-voltage equipment.

2) Smells - If you smell burning plastic, sulfur, or the smell of rotten eggs, with no identifiable source, then the issue may very well lie in your circuit breaker. It’s important to call an electrician as soon you notice any strange smells since it indicates the circuit breaker is damaged. Rectifying this at the latest will protect your space from the risk of potential fires.

Read More: How Overload Conditions Occur and Why are circuit protection devices so important?

3) Heated Outlets - We often think it’s normal for appliances or outlets to warm up slightly while in use. On the contrary, this heating up of outlets and switch plates is a sign that something is wrong with the circuit breaker. If you at any time notice the heating of your electrical system, then turn off the power and contact an electrician immediately. A heated outlet should not be left unchecked for long periods.

4) Shocks - If you notice sparks and shocks when you touch your appliances or circuit boards, then this indicates an issue with the circuit board. For instance, if you feel tingling when turning on or off your lights or other switches, then immediately shut out the power supply. Such shocks and sparks can escalate into an electrical fire if not treated immediately.

5) Humming Noise - If you notice a humming noise from your circuit breaker, then it indicates an overload. In such cases, the circuit breaker is unable to shut down successfully and this can lead to sparking. In such situations, it is best to call an electrician and not use any equipment or appliances.

All the above are signs that there are issues within your circuit breaker. Knowledge of what to look for will help you take precautions against any accidents. If you experience any of the above issues, we recommend you immediately call a professional and not try to resolve them on your own.

Also Read: How Earth Leakage Circuit Breaker Work (ELCB) Explained

Circuit Breaker by Schneider Electric

Such circuit breaker issues can be mitigated and reduced by investing in a reliable and quality circuit breaker. Schneider Electric cares about the safety of your space and appliances and manufactures highly durable circuit breakers. These are tested thoroughly by the team of experts at Schneider Electric before being launched in the market. The circuit breakers by Schneider Electric come in a wide variety of specifications and prices, and you can choose one that best meets your needs. For the most durable, safe, and cost-effective circuit breakers, invest in Schneider Electric.