Best Electrical Safety Devices You Need to Have Installed in Your Home

The present world is heavily reliant on electricity for a variety of purposes - from running machinery and electrical appliances to charging devices, running servers, and more. Even at the household level, we use electricity as a readily available source of energy for lighting, cooking, heating, charging, and running electrical appliances like computers. Though electricity plays an important role in our everyday lives, electricity can often be a health hazard unless proper precautions are used.
In households, if left unchecked, electricity poses a significant threat to humans, especially children, and pets. Exposed wires or exposure to moisture can cause electrical accidents like electrocutions, fires, and short circuits. Moreover, in cases of electrical surges, the electricity flowing through live wires can suddenly rise to unprecedented levels, causing substantial damages to any connected device or appliance. During thunderstorms, a surge in electrical flow can cause permanent harm.
Therefore, to keep your loved ones secure or prevent your expensive appliances from burning out, installing safety devices and precautionary measures in your home is important. Electrical safety devices like the MCCB Switch can effectively keep the flow of electricity in check, and ensure the electrical flow is secure.
Let us discuss some of the best electrical safety devices from Schneider Electric that you need to have installed in your home.
- MCB and MCCB Switch
MCBs (Miniature Circuit Breaker) and MCCBs (Molded Case Circuit Breakers) are electrical safety measures frequently used across households. The MCCB electrical acts as a switch that maintains the voltage in the circuit at a fixed level and prevents excessive current flow. The fundamental purpose of the MCCB switch is to keep out unrestricted current from the connection which would otherwise cause damage to the connected appliance. During an electrical surge or an overload, the MCCB is triggered by higher voltages in the circuit. Once triggered, the MCCB causes the circuit to break, disrupting the flow of electricity to the connected device.
MCBs and MCCBs have a convenient design so they can be easily installed across the circuit. At usual conditions, they do not interfere with the flow of current, nor do they hamper the performance of any connected device. However, they have a lower tolerance to electricity, ranging from 10 to 125 amperes, so they can be triggered before the electricity becomes high enough to damage any connected electrical device. MCB and MCCBs are budget-friendly; the MCCB 125 amp 4 pole price is affordable and easily purchased from Schneider Electric.
- Surge Protection Devices
As the name indicates, Surge Protection Devices (SPDs) are used to ensure a safe voltage limit across circuits. During power anomalies like thunderstorms and utility issues, electrical appliances and components around the house face risks of burnout. To prevent such accidents, SPDs are used as restraints that limit the surge voltage up to desirable levels. They also discharge the overload current to distant grounds before it causes any harm to the electrical equipment around the house. Surge protectors are excellent electrical safety devices and are available as individuals, or as whole house surge protectors.
- Ground Fault Circuit Interrupters
Ground Fault Circuit interrupters, commonly known as GFCIs, are used to detect ground currents. They are solid-state trip units that are installed in the house as a protection for both humans and electrical appliances. GHCIs that provide people protection is designed to automatically detect residual electricity from ground faults. Upon sensing ground faults above 5 milliamperes, it triggers circuit breakers to restrict the flow of electricity immediately. It is popularly used across bathrooms and kitchens or around sources of water, preventing accidental electrocution. GFCIs designed for equipment protection are usually used to protect computers and heating equipment from electrical burnout or fires. They have circuit breakers that trip once the ground faults over 30 milliamperes.
In addition, self-closing outlet covers, safety plastic caps, cable management systems are superb measures to ensure electrical protection for your loved ones and expensive appliances around the household. Smoke detectors and alarms have grown popular over the recent years as well, as they are budget-friendly, and can issue warnings in case of smoldering and burning fires.
You can avail these effective electrical protection components and systems from Schneider Electric at great prices. Schneider Electric has a wide range of electrical products and components and offers attractive deals at the affordable MCCB 250 amp 4 pole price. Schneider Electric is a one-stop destination for all your electrical requirements and solutions. Visit our e-shop at https://shop.schneider-electric.co.in/.
Read Also: How Does The MCB Protect Your Home
Comments