Blog
Capacitor Bank Testing: Importance and Procedures Explained
A collection of capacitors of comparable ratings is known as a capacitor bank. These capacitors are arranged in parallel or series sequence to gather electrical energy. A capacitor bank is usually app...
Advantages of Circuit Breaker Test: Definition and Procedure Explained
Circuit breakers are essential electrical switches. The function of the circuit breaker is to prevent an electrical circuit from potential damage due to overflow of current through it, or overload or ...
Pick the Best 1.5 Ton AC Stabiliser: Essential Tips
Installing a stabiliser with your air conditioner is crucial. But why? Several factors make it essential to install a stabiliser with your AC. Continue reading this post by the Schneider Electric team...
Choosing the Right Capacitor Bank for Power Factor Correction!
What is capacitor bank? A capacitor bank consists of several capacitors. All these capacitors are of the same rating and are connected in series or parallel sequence. It stores electrical energy in an...
Why is the Transformer Rating in kVA Instead of kW?
Transformers play an important role in several industries. From manufacturing and electrical contracting to health care and higher education, several industries use them for their constant and efficie...
Optical Fibre: Definition, Structure, Propagation
Optical fibre has completely revolutionised the communications industry. Various industries use it for varying purposes. If you wish to understand its specifics, such as the structure of optical fibre...