Blog
Differential Relay: Working, Types, Advantage & Its Applications
Differential relays are basic components in power system protection, which play a vital protective role in transformers, generators, and other important apparatus against their internal faults.
DC Servo Motor: Construction, Working & Its Applications
Servo motors are among the most efficient and precise motor machines. Its torque to inertia ratio is high.
Different Types of Motor Starters Explained
Confusion regarding the varying types of motor starters is common in the electrical industry. We are here to help you get rid of this and keep yourself informed about all the types of motor starters. ...
Difference Between Single Phase and Three Phase Induction Motor
The induction motor is an AC motor that works on the grounds that electromagnetic induction recurs between the stator and the rotor of the motor.
How To Test A Capacitor? A Complete Guide!
Testing a capacitor might seem a challenging task. However, it is not as difficult as it seems, and this guide will help you learn about it.
Understanding Magnetic Contactors: Definition and Uses
If you are involved in the electrical world, you might have heard about magnetic contactors.
Understanding Servo Motors: Working Principles & Applications
Servo motors are a crucial component in the realm of automation, robotics, and control systems, offering precise control of angular or linear position, velocity, and acceleration.
Induction Motor: Working Principles, Basics & Types Explained
Induction motors are the workhorse of modern industry, playing a major role in one-third to one-half of the electrical apparatus used in industries nowadays, either as the prime mover or agent.
Working Principle of Electromagnetic Flow Meter Explained
Electromagnetic flow meters are also known as magmeters. They are widely used in various industries to measure the flow rate of conductive fluids.